module ti.sysbios.family.arm.MPU |
|
|
Memory Protection Unit (MPU) Manager
This module manages the Memory Protect Unit (MPU) present in many ARM
Cortex-R and Cortex-M devices. It enables the application to partition
the memory into different regions and set protection attributes for
each region.
[
more ... ]
#include <ti/sysbios/family/arm/MPU.h>
Functions |
Void | |
Void | |
Void | |
Bool | |
Void | |
Functions common to all target modules |
|
|
Typedefs |
typedef struct | |
typedef struct | |
typedef enum | |
Constants |
| |
| |
| |
| |
extern const Bool | |
extern const Bool | |
Variables |
| |
DETAILS
This module manages the Memory Protect Unit (MPU) present in many ARM
Cortex-R and Cortex-M devices. It enables the application to partition
the memory into different regions and set protection attributes for
each region.
The number of memory regions supported is device specific and may vary
on different devices. The Cortex-R5F based TMS570DCxx/RM57D8xx devices
for instance support 16 memory regions.
Programming a memory region requires specifying the base address and
size of the region, and the region's protection attributes. It is also
possible to overlap different memory regions with higher region numbers
enjoying higher priority than lower region numbers i.e. region 15 has
a higher priority than region 14, and if both were overlapping, the
overlapped memory region's attributes would be defined by region 15's
entry.
The protection attributes for each region include attributes such as
memory type (strongly-ordered, device or normal), shareability,
cacheability and read-write access permission.
By default, this module programs the MPU regions with some default
settings/attributes. Please see this
MPU Region Settings table for
a list of default settings used for various supported devices.
MEMORY REGION ATTRIBUTES
Memory regions can be configured as different memory types by setting
the
bufferable,
cacheable and
tex (type extension) fields of the
RegionAttrs
structure which is passed as an argument to
MPU_setRegion() function. The three memory types
supported by the hardware are "Normal" (cacheable), "Device" and
"Strongly-ordered" memory. "Device" and "Strongly-ordered" memory types
are recommended for mapping peripheral address space like memory-mapped
registers. These two types ensure that the memory accesses to the
peripheral memory are not performed speculatively, are not repeated and
are performed in order. The "Normal" memory type is recommended for mapping
memory regions storing application code and data.
Here are some common settings for the
bufferable,
cacheable and
tex fields to
define different memory region types:
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
+ Memory Type | bufferable | cacheable | tex +
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
+ Shareable Strongly-ordered memory | false | false | 0 +
+-----------------------------------------+------------+-----------+-----+
+ Shareable Device memory | true | false | 0 +
+-----------------------------------------+------------+-----------+-----+
+ Outer & Inner Non-cacheable | false | false | 1 +
+-----------------------------------------+------------+-----------+-----+
+ Outer & Inner Write-back Write-allocate | true | true | 1 +
+ cacheable | | | +
++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++
For an exhaustive list of all different memory type settings and a
detailed explanation of the memory region attributes, please read the
'Protected Memory System Architecture (PMSA)' chapter of the
ARM v7AR Architecture Reference Manual.
CHANGING SHAREABILITY ATTRIBUTES OF A CACHEABLE MEMORY REGION
If changing the shareability attribute of a cacheable memory region,
it is possible for coherency problems to arise. In order to avoid possible
coherency errors, the below sequence should be followed to change the
shareability attributes of the memory region:
- Make the memory region Non-cacheable and outer-shareable
- Clean and invalidate the memory region from the cache
- Change the shareability attribute to the desired value
EXAMPLES
Example showing how to set attributes for a given memory region using
*.cfg script:
var MPU = xdc.useModule('ti.sysbios.family.arm.MPU');
// Mark memory region as normal outer and inner write-back
// and write-through cacheable
var attrs = new MPU.RegionAttrs();
MPU.initRegionAttrsMeta(attrs);
attrs.enable = true;
attrs.bufferable = true;
attrs.cacheable = true;
attrs.shareable = false;
attrs.noExecute = false;
attrs.accPerm = 6; // Read-only at PL1 and PL0
attrs.tex = 1;
// Set attributes for memory region of size 4MB starting at address 0x0
// using MPU region Id 0 to store the attributes.
MPU.setRegionMeta(0, 0x00000000, MPU.RegionSize_4M, attrs);
Calling Context
Function | Hwi | Swi |
Task | Main | Startup |
disable | Y | Y |
Y | Y | Y |
enable | Y | Y |
Y | Y | Y |
initRegionAttrs | Y | Y |
Y | Y | Y |
isEnabled | Y | Y |
Y | Y | Y |
setRegion | Y | Y |
Y | Y | Y |
Definitions:
- Hwi: API is callable from a Hwi thread.
- Swi: API is callable from a Swi thread.
- Task: API is callable from a Task thread.
- Main: API is callable during any of these phases:
- In your module startup.
- During xdc.runtime.Startup.lastFxns.
- During main().
- During BIOS.startupFxns.
- Startup: API is callable during any of these phases:
- During xdc.runtime.Startup.firstFxns.
- In your module startup.
|
enum MPU_RegionSize |
|
typedef enum MPU_RegionSize {
MPU_RegionSize_32,
MPU_RegionSize_64,
MPU_RegionSize_128,
MPU_RegionSize_256,
MPU_RegionSize_512,
MPU_RegionSize_1K,
MPU_RegionSize_2K,
MPU_RegionSize_4K,
MPU_RegionSize_8K,
MPU_RegionSize_16K,
MPU_RegionSize_32K,
MPU_RegionSize_64K,
MPU_RegionSize_128K,
MPU_RegionSize_256K,
MPU_RegionSize_512K,
MPU_RegionSize_1M,
MPU_RegionSize_2M,
MPU_RegionSize_4M,
MPU_RegionSize_8M,
MPU_RegionSize_16M,
MPU_RegionSize_32M,
MPU_RegionSize_64M,
MPU_RegionSize_128M,
MPU_RegionSize_256M,
MPU_RegionSize_512M,
MPU_RegionSize_1G,
MPU_RegionSize_2G,
MPU_RegionSize_4G
} MPU_RegionSize;
struct MPU_DeviceRegs |
|
Memory Protection Unit (MPU) registers. Symbol "MPU_deviceRegs" is
a physical device
typedef struct MPU_DeviceRegs {
UInt32 TYPE;
// 0xD90 Type Register
UInt32 CTRL;
// 0xD94 Control Register
UInt32 RNR;
// 0xD98 Region Register
UInt32 RBAR;
// 0xD9C Region Base Address Register
UInt32 RASR;
// 0xDA0 Region Attribute and Size Register
UInt32 RBAR_A1;
// 0xDA4 MPU Alias 1
UInt32 RASR_A1;
// 0xDA8 MPU Alias 1
UInt32 RBAR_A2;
// 0xDAC MPU Alias 2
UInt32 RASR_A2;
// 0xDB0 MPU Alias 2
UInt32 RBAR_A3;
// 0xDB4 MPU Alias 3
UInt32 RASR_A3;
// 0xDB8 MPU Alias 3
} MPU_DeviceRegs;
struct MPU_RegionAttrs |
|
Structure for setting the region attributes
typedef struct MPU_RegionAttrs {
Bool enable;
// is MPU region enabled
Bool bufferable;
// is memory region bufferable (B)
Bool cacheable;
// is memory region cacheable (C)
Bool shareable;
// is memory region shareable (S)
Bool noExecute;
// is memory region not executable (XN)
UInt8 accPerm;
// access permission bits value 0-7
(AP[2:0])
UInt8 tex;
// memory region attr type extension
field (TEX[2:0])
UInt8 subregionDisableMask;
// disable mask for all 8 subregions
} MPU_RegionAttrs;
DETAILS
The B (Bufferable), C (Cacheable), TEX (Type extension), S (Shareable),
XN (No execute or Execute never) and AP (Access permission) bits in the
memory region entry define the memory region attributes.
See the 'Memory region attributes' section in the 'Protected Memory
System Architecture (PMSA)' of the ARM v7-AR Architecture Reference
Manual for more details.
config MPU_A_invalidRegionId // module-wide |
|
Assert raised when an invalid region number is passed to MPU_setRegion()
extern const Assert_Id MPU_A_invalidRegionId;
config MPU_A_nullPointer // module-wide |
|
Assert raised when a pointer is null
config MPU_A_unalignedBaseAddr // module-wide |
|
Assert raised when region's base address is not aligned to the region's
size
extern const Assert_Id MPU_A_unalignedBaseAddr;
config MPU_defaultAttrs // module-wide |
|
Default region attributes structure
DETAILS
The default attributes structure marks the memory region as outer and
inner non-cacheable and non-shareable, with read-write access in
privileged mode (PL1) only.
config MPU_enableBackgroundRegion // module-wide |
|
Configuration parameter to enable background region
extern const Bool MPU_enableBackgroundRegion;
DETAILS
If the MPU is enabled and background region is also enabled, any
privileged access that does not map to any MPU memory region is
handled using the default memory map.
config MPU_enableMPU // module-wide |
|
Configuration parameter to enable MPU
extern const Bool MPU_enableMPU;
extern MPU_deviceRegs |
|
MPU_DeviceRegs MPU_deviceRegs; // linked as extern ti_sysbios_family_arm_MPU_deviceRegs
MPU_disable() // module-wide |
|
Disables the MPU
DETAILS
If the MPU is already disabled, then simply return.
Otherwise this function does the following:
- If the L1 data cache is enabled, write back invalidate all
of L1 data cache.
- If the L1 program cache is enabled, invalidate all of L1
program cache.
NOTE
This function does not change the cache L1 data/program settings.
MPU_enable() // module-wide |
|
Enables the MPU
DETAILS
If the MPU is already enabled, then simply return.
Otherwise this function does the following:
- If the L1 program cache is enabled, invalidate all of L1
program cache.
This function enables the MPU on the core it is called from.
NOTE
This function does not change the L1 data/program cache settings.
MPU_initRegionAttrs() // module-wide |
|
Initializes the region attribute structure
ARGUMENTS
attrs
Pointer to region attribute struct
MPU_isEnabled() // module-wide |
|
Determines if the MPU is enabled
MPU_setRegion() // module-wide |
|
Sets the MPU region attributes
ARGUMENTS
regionId
MPU region number
regionBaseAddr
MPU region base address
regionSize
MPU region size
attrs
Protection attributes
SEE
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool MPU_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool MPU_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 MPU_Module_getMask();
// Returns the diagnostics mask for this module
Void MPU_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var MPU = xdc.useModule('ti.sysbios.family.arm.MPU');
module-wide constants & types
module-wide config parameters
msg: "A_invalidRegionId: MPU Region number passed is invalid."
};
msg: "A_nullPointer: Pointer is null"
};
msg: "A_unalignedBaseAddr: MPU region base address not aligned to size."
};
enable: true,
bufferable: false,
cacheable: false,
shareable: false,
noExecute: false,
accPerm: 1,
tex: 1,
subregionDisableMask: 0
};
module-wide functions
enum MPU.RegionSize |
|
values of type MPU.RegionSize
const MPU.RegionSize_32;
const MPU.RegionSize_64;
const MPU.RegionSize_128;
const MPU.RegionSize_256;
const MPU.RegionSize_512;
const MPU.RegionSize_1K;
const MPU.RegionSize_2K;
const MPU.RegionSize_4K;
const MPU.RegionSize_8K;
const MPU.RegionSize_16K;
const MPU.RegionSize_32K;
const MPU.RegionSize_64K;
const MPU.RegionSize_128K;
const MPU.RegionSize_256K;
const MPU.RegionSize_512K;
const MPU.RegionSize_1M;
const MPU.RegionSize_2M;
const MPU.RegionSize_4M;
const MPU.RegionSize_8M;
const MPU.RegionSize_16M;
const MPU.RegionSize_32M;
const MPU.RegionSize_64M;
const MPU.RegionSize_128M;
const MPU.RegionSize_256M;
const MPU.RegionSize_512M;
const MPU.RegionSize_1G;
const MPU.RegionSize_2G;
const MPU.RegionSize_4G;
C SYNOPSIS
struct MPU.DeviceRegs |
|
Memory Protection Unit (MPU) registers. Symbol "MPU_deviceRegs" is
a physical device
var obj = new MPU.DeviceRegs;
obj.TYPE = UInt32 ...
// 0xD90 Type Register
obj.CTRL = UInt32 ...
// 0xD94 Control Register
obj.RNR = UInt32 ...
// 0xD98 Region Register
obj.RBAR = UInt32 ...
// 0xD9C Region Base Address Register
obj.RASR = UInt32 ...
// 0xDA0 Region Attribute and Size Register
obj.RBAR_A1 = UInt32 ...
// 0xDA4 MPU Alias 1
obj.RASR_A1 = UInt32 ...
// 0xDA8 MPU Alias 1
obj.RBAR_A2 = UInt32 ...
// 0xDAC MPU Alias 2
obj.RASR_A2 = UInt32 ...
// 0xDB0 MPU Alias 2
obj.RBAR_A3 = UInt32 ...
// 0xDB4 MPU Alias 3
obj.RASR_A3 = UInt32 ...
// 0xDB8 MPU Alias 3
C SYNOPSIS
struct MPU.RegionAttrs |
|
Structure for setting the region attributes
var obj = new MPU.RegionAttrs;
obj.enable = Bool ...
// is MPU region enabled
obj.bufferable = Bool ...
// is memory region bufferable (B)
obj.cacheable = Bool ...
// is memory region cacheable (C)
obj.shareable = Bool ...
// is memory region shareable (S)
obj.noExecute = Bool ...
// is memory region not executable (XN)
obj.accPerm = UInt8 ...
// access permission bits value 0-7
(AP[2:0])
obj.tex = UInt8 ...
// memory region attr type extension
field (TEX[2:0])
obj.subregionDisableMask = UInt8 ...
// disable mask for all 8 subregions
DETAILS
The B (Bufferable), C (Cacheable), TEX (Type extension), S (Shareable),
XN (No execute or Execute never) and AP (Access permission) bits in the
memory region entry define the memory region attributes.
See the 'Memory region attributes' section in the 'Protected Memory
System Architecture (PMSA)' of the ARM v7-AR Architecture Reference
Manual for more details.
C SYNOPSIS
config MPU.A_invalidRegionId // module-wide |
|
Assert raised when an invalid region number is passed to MPU_setRegion()
msg: "A_invalidRegionId: MPU Region number passed is invalid."
};
C SYNOPSIS
config MPU.A_nullPointer // module-wide |
|
Assert raised when a pointer is null
msg: "A_nullPointer: Pointer is null"
};
C SYNOPSIS
config MPU.A_unalignedBaseAddr // module-wide |
|
Assert raised when region's base address is not aligned to the region's
size
msg: "A_unalignedBaseAddr: MPU region base address not aligned to size."
};
C SYNOPSIS
config MPU.defaultAttrs // module-wide |
|
Default region attributes structure
enable: true,
bufferable: false,
cacheable: false,
shareable: false,
noExecute: false,
accPerm: 1,
tex: 1,
subregionDisableMask: 0
};
DETAILS
The default attributes structure marks the memory region as outer and
inner non-cacheable and non-shareable, with read-write access in
privileged mode (PL1) only.
C SYNOPSIS
config MPU.enableBackgroundRegion // module-wide |
|
Configuration parameter to enable background region
MPU.enableBackgroundRegion = Bool true;
DETAILS
If the MPU is enabled and background region is also enabled, any
privileged access that does not map to any MPU memory region is
handled using the default memory map.
C SYNOPSIS
config MPU.enableMPU // module-wide |
|
Configuration parameter to enable MPU
MPU.enableMPU = Bool true;
C SYNOPSIS
metaonly config MPU.common$ // module-wide |
|
Common module configuration parameters
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config MPU.rovViewInfo // module-wide |
|
metaonly MPU.initRegionAttrsMeta() // module-wide |
|
Initializes the region attribute structure
ARGUMENTS
attrs
Pointer to region attribute struct
metaonly MPU.setRegionMeta() // module-wide |
|
Statically sets the MPU region attributes
ARGUMENTS
regionId
MPU region number
regionBaseAddr
MPU region base address
regionSize
MPU region size
attrs
Protection attributes
SEE
generated on Fri, 10 Jun 2016 23:29:08 GMT