1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32
33 34 35
36 package ti.platforms.simplelink;
37
38 /*!
39 * ======== Platform ========
40 * A generic platform that supports any CC13xx, CC26xx, or CC32xx device
41 *
42 * The device to be used by this platform is passed as the platform instance
43 * name. On the `xdc.tools.configuro` command line, it is done in the
44 * following way:
45 * @p(code)
46 * xs xdc.tools.configuro ... -p "ti.platforms.simplelink:CC3200"
47 * @p
48 *
49 * In package.bld, the platform instance is selected as in:
50 * @p(code)
51 * Pkg.addExecutable("test", target, "ti.platforms.simplelink:CC3200");
52 * @p
53 */
54 @Template ("./Platform.xdt")
55 metaonly module Platform inherits xdc.platform.IPlatform
56 {
57 config xdc.platform.IPlatform.Board BOARD = {
58 id: "0",
59 boardName: "simplelink",
60 boardFamily: null,
61 boardRevision: null
62 };
63
64 /*!
65 * ======== nameFormat ========
66 * Encoding of instance creation parameters in the instance's name
67 *
68 * For this platform, the parameters `deviceName`, `includeLinkCmdFile`
69 * and `clockRate` can be encoded in the instance name supplied on
70 * `xdc.tools.configuro` command line, for example:
71 * @p(code)
72 * xs xdc.tools.configuro ... -p ti.platforms.simplelink:CC3200:1:20
73 * @p
74 * Optional parameters can be omitted:
75 * @p(code)
76 * xs xdc.tools.configuro ... -p ti.platforms.simplelink:CC3200
77 * @p
78 */
79 readonly config string nameFormat
80 = "$(deviceName):$(includeLinkCmdFile):$(clockRate)";
81
82 /*!
83 * ======== useGnuRomLinkCmd ========
84 * Use ROM compatible linker script when building using GNU tools
85 *
86 * If this config param is set to true and "includeLinkCmdFile" is true,
87 * the ROM compatible linker script will be used. The ROM compatible
88 * linker script is required when building a ROM based application.
89 */
90 config Bool useGnuRomLinkCmd = false;
91
92 instance:
93
94 95 96 97 98
99
100 config xdc.platform.IExeContext.Cpu CPU = {
101 id: "0",
102 clockRate: 80.0,
103 catalogName: "ti.catalog.arm.cortexm4",
104 deviceName: "CC32xx",
105 revision: "",
106 };
107
108 /*!
109 * ======== deviceName ========
110 * The name of an `ICpuDataSheet` module for the device
111 *
112 * This parameter is required, but it does not have to be set explicitly;
113 * it can be encoded in the instance's name.
114 */
115 config string deviceName;
116
117 /*!
118 * ======== clockRate ========
119 * The clock rate for this device.
120 */
121 config Double clockRate;
122
123 override config string codeMemory = null;
124
125 override config string dataMemory = null;
126
127 override config string stackMemory = null;
128
129 /*!
130 * ======== includeLinkCmdFile ========
131 * The flag that specifies if the platform should include a linker command
132 * file.
133 *
134 * By default, a user is responsible for adding a linker command file to
135 * the project, or to the linker command line. However, if this flag is
136 * set, this platform will include a default linker command file for the
137 * selected device.
138 */
139 config Bool includeLinkCmdFile = false;
140 };