The Boot module supports boot initialization for the Concerto M3 core.
A special boot init function is created based on the configuration
settings for this module. This function is hooked into the
xdc.runtime.Reset.fxns[] array and called very early at boot time (prior
to cinit processing).
The code to support the boot module is placed in a separate section
named
".text:.bootCodeSection" to allow placement of this section in
the linker .cmd file if necessary. This section is a subsection of the
".text" section so this code will be placed into the .text section unless
explicitly placed, either through
Program.sectMap or through a linker
command file.
config Boot_configureClocks // module-wide |
|
Clock configuration flag, default is false
extern const Bool Boot_configureClocks;
DETAILS
Set to true to configure the PLL and system and M3 subsystem clock
dividers.
config Boot_sharedMemoryAccess // module-wide |
|
Shared RAM M3 write access
extern const Bits32 Boot_sharedMemoryAccess[8];
DETAILS
This parameter is used for writing the MSxSRCR registers.
It determines the M3 write access for each shared RAM segment only
when the M3 is the owner of the shared RAM segment.
By default, the M3 is allowed to CPU fetch, DMA write, and CPU write.
Bit 0 is for CPU fetch. 0 - fetch allowed, 1 - fetch not allowed
Bit 1 is for DMA write. 0 - write allowed, 1 - write not allowed
Bit 2 is for CPU write. 0 - write allowed, 1 - write not allowed
config Boot_sharedMemoryEnable // module-wide |
|
Shared RAM memory enable mask
extern const Bits32 Boot_sharedMemoryEnable;
DETAILS
This parameter is used for writing the MEMCNF register.
By default, all shared RAM segments will be enabled at runtime.
To disable a shared RAM segment, set the corresponding bit to 0.
If any data is loaded to a shared RAM segment, the segment must
be enabled prior to loading the program through other means.
config Boot_sharedMemoryOwnerMask // module-wide |
|
Shared RAM owner select mask
extern const Bits32 Boot_sharedMemoryOwnerMask;
DETAILS
This parameter is used for writing the MSxMSEL register.
By default, each value of each shared RAM select bit is '0'.
This means the M3 is the owner and has write access based upon
the sharedMemoryAccess bits. Setting a '1' in any bit position
makes the C28 the owner of that shared RAM segment.
metaonly enum Boot.FractMult |
|
System PLL Fractional Multiplier (SPLLFMULT) value
values of type Boot.FractMult
const Boot.Fract_0;
// Fractional multiplier is 0
const Boot.Fract_25;
// Fractional multiplier is 0.25
const Boot.Fract_50;
// Fractional multiplier is 0.5
const Boot.Fract_75;
// Fractional multiplier is 0.75
metaonly enum Boot.M3Div |
|
M3 Subsystem Clock Divider (M3SSDIVSEL) value
values of type Boot.M3Div
const Boot.M3Div_1;
// Divide by 1
const Boot.M3Div_2;
// Divide by 2
const Boot.M3Div_4;
// Divide by 4
metaonly enum Boot.SysDiv |
|
System Clock Divider (SYSDIVSEL) value
values of type Boot.SysDiv
const Boot.Div_1;
// Divide by 1
const Boot.Div_2;
// Divide by 2
const Boot.Div_4;
// Divide by 4
const Boot.Div_8;
// Divide by 8
metaonly struct Boot.ModuleView |
|
var obj = new Boot.ModuleView;
obj.configureClocks = Bool ...
obj.OSCCLK = UInt ...
obj.SPLLIMULT = UInt ...
obj.SPLLFMULT = String ...
obj.SYSDIVSEL = String ...
obj.M3SSDIVSEL = String ...
obj.bootC28 = Bool ...
config Boot.configureClocks // module-wide |
|
Clock configuration flag, default is false
Boot.configureClocks = Bool false;
DETAILS
Set to true to configure the PLL and system and M3 subsystem clock
dividers.
C SYNOPSIS
config Boot.sharedMemoryAccess // module-wide |
|
Shared RAM M3 write access
Boot.sharedMemoryAccess = Bits32[8] undefined;
DETAILS
This parameter is used for writing the MSxSRCR registers.
It determines the M3 write access for each shared RAM segment only
when the M3 is the owner of the shared RAM segment.
By default, the M3 is allowed to CPU fetch, DMA write, and CPU write.
Bit 0 is for CPU fetch. 0 - fetch allowed, 1 - fetch not allowed
Bit 1 is for DMA write. 0 - write allowed, 1 - write not allowed
Bit 2 is for CPU write. 0 - write allowed, 1 - write not allowed
C SYNOPSIS
config Boot.sharedMemoryEnable // module-wide |
|
Shared RAM memory enable mask
Boot.sharedMemoryEnable = Bits32 0xffffffff;
DETAILS
This parameter is used for writing the MEMCNF register.
By default, all shared RAM segments will be enabled at runtime.
To disable a shared RAM segment, set the corresponding bit to 0.
If any data is loaded to a shared RAM segment, the segment must
be enabled prior to loading the program through other means.
C SYNOPSIS
config Boot.sharedMemoryOwnerMask // module-wide |
|
Shared RAM owner select mask
Boot.sharedMemoryOwnerMask = Bits32 0;
DETAILS
This parameter is used for writing the MSxMSEL register.
By default, each value of each shared RAM select bit is '0'.
This means the M3 is the owner and has write access based upon
the sharedMemoryAccess bits. Setting a '1' in any bit position
makes the C28 the owner of that shared RAM segment.
C SYNOPSIS
metaonly config Boot.M3SSDIVSEL // module-wide |
|
M3 Subsystem Clock Divider (M3SSDIVSEL) value
metaonly config Boot.OSCCLK // module-wide |
|
OSCCLK input frequency to PLL, in MHz. Default is 20 MHz
DETAILS
This is the frequency of the oscillator clock (OSCCLK) input to the
PLL.
metaonly config Boot.SPLLFMULT // module-wide |
|
System PLL Fractional Multiplier (SPLLFMULT) value
metaonly config Boot.SPLLIMULT // module-wide |
|
System PLL Integer Multiplier (SPLLIMULT) value
metaonly config Boot.SYSDIVSEL // module-wide |
|
System Clock Divider (SYSDIVSEL) value
metaonly config Boot.bootC28 // module-wide |
|
Initiate booting of the C28 processor. Default is false
Boot.bootC28 = Bool false;
DETAILS
Set to true to enable the M3 to initiate boot of the C28.
If enabled, this will occur after the optional clock configuration
step, enabled by
configureClocks.
metaonly config Boot.bootFromFlash // module-wide |
|
Boot from Flash flag. Default is true
Boot.bootFromFlash = Bool true;
DETAILS
Set to true to enable booting the M3 from Flash.
metaonly config Boot.configSharedRAMs // module-wide |
|
Configure Shared RAM regions before booting the C28 processor.
Default is true
Boot.configSharedRAMs = Bool true;
DETAILS
Set to true to enable Shared RAM regions S0-S7, to set the
owner of each region and the write access permissions for the onwer.
metaonly config Boot.configureFlashController // module-wide |
|
Flash controller configuration flag, default is true
Boot.configureFlashController = Bool true;
DETAILS
Set to true to enable the configuration of the Flash controller
wait states, program and data cache.
metaonly config Boot.configureFlashWaitStates // module-wide |
|
Flash controller wait states configuration flag, default is true
Boot.configureFlashWaitStates = Bool true;
DETAILS
Set to true to configure the Flash controller wait states. The number
of wait states is computed based upon the CPU frequency.
metaonly config Boot.enableFlashDataCache // module-wide |
|
Flash controller data cache enable flag, default is true
Boot.enableFlashDataCache = Bool true;
DETAILS
Set to true to enable the Flash controller's data cache.
metaonly config Boot.enableFlashProgramCache // module-wide |
|
Flash controller program cache enable flag, default is true
Boot.enableFlashProgramCache = Bool true;
DETAILS
Set to true to enable the Flash controller's program cache.
metaonly config Boot.initC28RAMs // module-wide |
|
Initialize C28 RAM regions before booting the C28 processor.
Default is true
Boot.initC28RAMs = Bool true;
DETAILS
Set to true to enable initialization of these C28 RAM regions: M1,
CtoM, LO, L1, L2, and L3. RAM locations will be zeroed, and the ECC or
parity bits will be initialized.
metaonly config Boot.limpAbortFunction // module-wide |
|
Function to be called when Limp mode is detected
Boot.limpAbortFunction = Fxn undefined;
DETAILS
This function is called when the Boot module is about to configure
the PLL, but finds the device operating in Limp mode (i.e., the mode
when a missing OSCCLK input has been detected).
If this function is not specified by the application, a default
function will be used, which spins in an infinite loop.
metaonly config Boot.loadSegment // module-wide |
|
Specifies where to load the flash function
Boot.loadSegment = String undefined;
DETAILS
If 'configureFlashWaitStates' is true, then this parameter
determines where the ".ti_catalog_c2800_initF2837x_flashfuncs"
section gets loaded.
metaonly config Boot.rovViewInfo // module-wide |
|
metaonly config Boot.runSegment // module-wide |
|
Specifies where to run the flash function
Boot.runSegment = String undefined;
DETAILS
If 'configureFlashWaitStates' is true then this parameter
determines where the ".ti_catalog_c2800_initF2837x_flashfuncs"
section gets executed at runtime.