This release note is divided into the following sections:
Introduction,
Documentation,
What's New,
Upgrading And
Compatibility Information,
Host Support,
Dependencies,
Device Support,
Validation Information,
Known Issues,
Benchmarks,
Versioning,
Technical Support
And Product Updates,
SYS/BIOS 6.41.01.36 is a GA release of SYS/BIOS
6.40.00. CCS users must use CCSv6.0.0 or higher. This
release also has support for GCC (for Cortex-M) and IAR (for Cortex-M
and MSP430).
Please read the SYS/BIOS User's Guide for help installing and setting
up your environment to use SYS/BIOS 6.41.01.36.
back to top
The following documentation is provided with this release. These
documents are also available via the CCS Eclipse help table of
contents.
License and manifest.
Additional online sources of documentation.
Release
notes from previous releases are also available in the
release notes archive
directory.
back to top
SYS/BIOS
6.41.01.36 GA
Release (this release).
- Maintenance release. See bug fix list below.
Defects Fixed in
SYS/BIOS
6.41.01.36 GA (Fixes since SYS/BIOS 6.41.00):
ID
Headline
SDOCM00114363 Deleting a pre-empted task that was executing Event_pend() can result in application crash.
SDOCM00114079 A8 TimestampProvider 64 bit timestamps jump backwards sometimes
SDOCM00113999 avalabench is generating the export file before the benchmark documents
SDOCM00113957
ti/sysbios/smp/LoggerBuf Timestamp proxy is set to early resulting in
TimestampNull (no timestamps in the logs)
SDOCM00113943 Fix MSP430 warnings that occur when building with Codegen tools version 4.4.0B1
SDOCM00113914
ARP32/EVE Hwi_interruptClear() should not clear the IFR register
(problem in Timer/IPC intitialization)
SDOCM00113851 CCS on Linux is unable to find linker cmd files in the installed SYS/BIOS or TI-RTOS product
SDOCM00113827 Need 2 new Cache APIs for global L1D operations on c64+/c66
SDOCM00113716
ROM application link should fail or give good error if user has
incorrect IAR linker command file
SDOCM00113606
ti.sysbios.family Delegates page needs to be updated to show the
relatively new Clock.timerDelegate
SDOCM00113566 Clock module cdoc needs to mention function execution context
SDOCM00113541
Hwi_initStack() routine may generate code that corrupts the stack
during boot time (gcc v4.8 Arm issue)
SDOCM00113119 BIOS needs to support creating a secure context
SDOCM00113005 Add ASID tagging support for Cortex-A8 and Cortex-A15 and new API to invalidate TLB
SDOCM00112319 F2837x initFlash() code incorrectly programs the flash wait states
SDOCM00108394 Document that C6x Cache_xxxAll() does not wait for whole memory system to complete before return
back to top
SYS/BIOS
software downloads
SYS/BIOS 6.35 and 6.37
- Binary compatible for all targets except MSP430 and C2000.
- MSP430
and C2000 users must recompile all source files that use the Semaphore,
Mailbox, or Event modules. The timeout parameter was changed from
UInt to UInt32 which are different sizes.
- All other users can use libraries built with 6.35.0x and 6.37.0x with 6.40.00.
SYS/BIOS 6.34 and older
- Source compatible. All APIs are supported but all source files must be recompiled.
back to top
- Supported
Operating Systems
- Windows 8, Windows
7
- Ubuntu [10.04, 12.04, 12.10, 13.04]
back to top
- Minimum Required Software Versions
- Code Composer Studio v6.0.x or later
- TI Code Generation Tools
- C28X
version 6.2.5 or later
- C6X version 7.4.7 or later
- ARM version 5.1.5 or later
- MSP430 version 4.3.1 or later
- XDCTools 3.30.00.21 or later
- GNU Code Generation Tools (for ARM only)
- ARM gcc-arm-none-eabi-4_7-2013q3 or later
- XDCtools 3.30.00.21 or later
- IAR Code Generation Tools (for Arm Cortex-M and MSP430 only)
- ARM version 6.70.1
- MSP430 version 5.60.1
- XDCtools 3.30.00.21 or later
- Required Hardware
- See Device Support Section below.
back to top
Click here
for the list of supported devices.
back to top
Click
here
for the list of compilers used to build and validate this release
(scroll down to Supported Targets section).
back to top
The
following issues are known to affect this release:
back to top
For a full description of Benchmarks please see the
appendices in the SYS/BIOS
6 User's
Guide.
back to top
All releases
have 4 digits (M.mm.pp.bb).
This includes GA and pre-releases (engineering, alpha/EA, beta, etc.).
Pre-releases are denoted with a suffix (e.g. 6.30.00.00-eng or
6.30.00.10-beta).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit
Major number, mm
is 2 digit minor number, pp
is a 2 digit patch number, and b
is an unrestricted set of digits used as an incrementing build counter.
To
support multiple side-by-side installations of the product, the product
version is encoded in the top level directory (e.g. bios_6_30_00_00).
Subsequent
releases of patch upgrades will be identified by the patch number, ex.
SYS/BIOS 6.30.01.15 with directory bios_6_30_01_15. Typically, these
patches only include critical bug fixes.
Please note that
version numbers and compatibility keys are NOT the same. For an
explanation of compatibility keys, please refer to the 'Upgrade and
Compatibility Information' section.
back to top
Technical
Support and Product Updates
back to top
Last
updated: January 07, 2015 Build Ver: 6.41.01.36 Rev: p36