1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 31
32 33 34 35 36
37
38 package ti.sysbios.family.c28;
39
40 /*!
41 * ======== TimestampProvider ========
42 *
43 * @p(html)
44 * <h3> Calling Context </h3>
45 * <table border="1" cellpadding="3">
46 * <colgroup span="1"></colgroup> <colgroup span="5" align="center"></colgroup>
47 *
48 * <tr><th> Function </th><th> Hwi </th><th> Swi </th><th> Task </th><th> Main </th><th> Startup </th></tr>
49 * <!-- -->
50 * <tr><td> {@link #get32} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
51 * <tr><td> {@link #get64} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
52 * <tr><td> {@link #getFreq} </td><td> Y </td><td> Y </td><td> Y </td><td> Y </td><td> N </td></tr>
53 * <tr><td colspan="6"> Definitions: <br />
54 * <ul>
55 * <li> <b>Hwi</b>: API is callable from a Hwi thread. </li>
56 * <li> <b>Swi</b>: API is callable from a Swi thread. </li>
57 * <li> <b>Task</b>: API is callable from a Task thread. </li>
58 * <li> <b>Main</b>: API is callable during any of these phases: </li>
59 * <ul>
60 * <li> In your module startup after this module is started (e.g. TimestampProvider_Module_startupDone() returns TRUE). </li>
61 * <li> During xdc.runtime.Startup.lastFxns. </li>
62 * <li> During main().</li>
63 * <li> During BIOS.startupFxns.</li>
64 * </ul>
65 * <li> <b>Startup</b>: API is callable during any of these phases:</li>
66 * <ul>
67 * <li> During xdc.runtime.Startup.firstFxns.</li>
68 * <li> In your module startup before this module is started (e.g. TimestampProvider_Module_startupDone() returns FALSE).</li>
69 * </ul>
70 * </ul>
71 * </td></tr>
72 * </table>
73 * @p
74 *
75 */
76
77 @ModuleStartup
78
79 module TimestampProvider inherits xdc.runtime.ITimestampProvider
80 {
81 /*!
82 * TimestampProvider timer id: 0, 1, or 2
83 *
84 * This parameter is ignored if useClockTimer is true.
85 */
86 config UInt timerId = Timer.ANY;
87
88 /*!
89 * Whether the TimestampProvider should share the Clock's timer.
90 *
91 * This parameter overrides the timeId setting.
92 *
93 * Sharing the Clock timer leaves more timers available for other uses,
94 * but makes the Timestamp APIs less efficient. If the Clock timer is
95 * used, the timestamp is calculated as:
96 * (Clock ticks) x (tick period) + (current timer count)
97 * This also limits the maximum value of the timestamp:
98 * max timestamp = 2^32 x (Clock tick period)
99 *
100 * Using a dedicated timer allows for a full 64-bit timestamp and does not
101 * require any multiplication to retrieve the value.
102 */
103 config Bool useClockTimer = false;
104
105 /*!@_nodoc
106 * Internal use. If Timestamp is using a dedicated timer, this function is
107 * added to Startup.lastFxns to start the timer before reaching main.
108 *
109 * There are no C symbol references to this function, so it must be kept
110 * above the internal section so that it does not fall away when building
111 * a ROM image. If the function falls out of the ROM, when the ROM
112 * application finally references the symbol, it will not exist, and the
113 * library will be brought in a second time resulting in multiple symbol
114 * definitions.
115 */
116 Void startTimer();
117
118 /*!@_nodoc
119 * Internal use. If Timestamp is using a dedicated timer, this function is
120 * the timer interrupt handler which maintains a count which is the upper
121 * 32-bits of the timestamp.
122 *
123 * This function must be kept 'public' for ROM concerns. See startTimer
124 * for explanation.
125 */
126 Void rolloverFunc(UArg unused);
127
128 internal:
129
130 struct Module_State {
131 Timer.Handle timer;
132 volatile UInt32 hi;
133 }
134 }
135 136 137 138
139