1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Defaults.xdc ========
    15     */
    16    
    17    package xdc.runtime;
    18    
    19    /*!
    20     *  ======== Defaults ========
    21     *  Default attributes inherited by all target modules
    22     *
    23     *  This module defines default values for `common$` structure. If other 
    24     *  modules do not set `common$` properties explicitly, these values will be
    25     *  used.
    26     */
    27    module Defaults {
    28    
    29        /*! 
    30         *  ======== common$ ========
    31         *  Defaults inherited by all target modules
    32         *
    33         *  This structure defines the default values for the configuration
    34         *  parameters shared by all modules in a system.  Unless otherwise
    35         *  noted, setting one of the fields defined below will set the
    36         *  corresponding value for all modules in the system which have not
    37         *  been explicitly set; i.e., it will establish a default value for
    38         *  the parameter.
    39         *
    40         *  However, the modules from this package (`xdc.runtime`) are an
    41         *  exception. The values from `Default.common$` are not copied to
    42         *  `logger` and `diags_` properties of `common$` in `xdc.runtime`
    43         *  modules. The property `diags_ASSERT` is an exception to that exception.
    44         *  Its value from 'Default.common$` is copied to all modules for which
    45         *  `diags_ASSERT` has not been explicitly set.
    46         *
    47         *  @a(diags_ASSERT) 
    48         *  Enables asserts at runtime. Default is `ALWAYS_ON`
    49         *
    50         *  @a(diags_ENTRY)
    51         *  Enables entry trace for all functions. Default is `ALWAYS_OFF`
    52         *
    53         *  @a(diags_EXIT)
    54         *  Enables exit trace for all functions. Default is `ALWAYS_OFF`
    55         *
    56         *  @a(diags_INTERNAL)
    57         *  Enables internal asserts. Default is `ALWAYS_OFF`. When set to
    58         *  `ALWAYS_ON`, requires `diags_ASSERT` to be `ALWAYS_ON`.
    59         *
    60         *  @a(diags_LIFECYCLE)
    61         *  Enables logging of lifecycle events. These events are logged during 
    62         *  creates and deletes. Default is `ALWAYS_OFF`. 
    63         *
    64         *  @a(diags_STATUS)
    65         *  Enables logging of status events, such as error and warning events. 
    66         *  Default is `ALWAYS_ON`. Note that this does not mean that logging will
    67         *  occur by default--a logger instance must also be configured for the 
    68         *  module in order for events to be logged.
    69         *
    70         *  @a(diags_INFO)
    71         *  Enables logging of generic informational events. Default is 
    72         *  `ALWAYS_OFF`.
    73         *
    74         *  @a(diags_ANALYSIS)
    75         *  Enables logging of analysis events, such as benchmarking events. 
    76         *  Default is `ALWAYS_OFF`.
    77         *
    78         *  @a(diags_USER)
    79         *  Each `diags_USER` field controls a separate user-defined
    80         *  logging level. Default is `ALWAYS_OFF` for all `diags_USER` fileds.
    81         *
    82         *  @a(gate)
    83         *  Default gate used by all modules which are declared as being `@Gated`.
    84         *  By default, this parameter points to an instance of `{@link GateNull}`,
    85         *  which means there is no protection.
    86         *
    87         *  @a(gateParams)
    88         *  The default parameters used to create gates at runtime. See
    89         *  `{@link Types#Common$.gateParams}`.  Default is `null`.
    90         *
    91         *  @a(instanceHeap)
    92         *  Specify heap to be used for module instances. Default is `null`.
    93         *  If `instanceHeap` is `null`, instances will be allocated from
    94         *  the heap specified by `{@link Memory#defaultHeapInstance}`.
    95         *  
    96         *  @a(instanceSection)
    97         *  Specify section to be used to place module instances. Default is
    98         *  `null`.
    99         *
   100         *  @a(logger)
   101         *  Default logger used by modules to write logs. By default there is 
   102         *  no logger.
   103         *
   104         *  @a(memoryPolicy)
   105         *  Used to specify type of application. `Types.STATIC_POLICY` is used when
   106         *  all objects are created statically. `Types.CREATE_POLICY` is used when 
   107         *  the application creates objects at runtime. `Types.DELETE_POLICY` is
   108         *  used when the application creates and deletes objects at runtime. This
   109         *  helps eliminate unwanted create and delete code.
   110         *
   111         *  @a(namedInstance)
   112         *  This parameter should be set to true if space needs to be allocated in
   113         *  instance objects for instance names. Allocating space for a name
   114         *  allows object view tools to display the names. The runtime functions
   115         *  `Mod_Handle_name()` and `Mod_Handle_label()` defined for each module
   116         *  `Mod` can be used to retrieve the name at runtime.
   117         *
   118         *  @a(namedModule)
   119         *  This field allows the name of the module to be retained on the target.
   120         *  Setting this to `false` will save space but will also prevent
   121         *  the target from being able to display the module names appearing
   122         *  in `Log` events and `Error`s.
   123         *
   124         *  Setting `namedModule` to `false` causes all modules, except for
   125         *  `{@link Memory}` and `{@link Main}` to be unnamed by default.  To
   126         *  eliminate the string names for these modules you must explicitly
   127         *  set their `common$.namedModule` parameters to `false`; without these
   128         *  two names, target-side display of error messages is somewhat cryptic.
   129         *
   130         *  @a(romPatchTable)
   131         *  Specify whether modules that are allocated to ROM are patchable.
   132         */
   133        override metaonly config Types.Common$ common$ = {
   134            diags_ASSERT:       Diags.ALWAYS_ON,
   135            diags_ENTRY:        Diags.ALWAYS_OFF,
   136            diags_EXIT:         Diags.ALWAYS_OFF,
   137            diags_INTERNAL:     Diags.ALWAYS_OFF,
   138            diags_LIFECYCLE:    Diags.ALWAYS_OFF,
   139            diags_STATUS:       Diags.ALWAYS_ON,
   140            diags_USER1:        Diags.ALWAYS_OFF,
   141            diags_USER2:        Diags.ALWAYS_OFF,
   142            diags_USER3:        Diags.ALWAYS_OFF,
   143            diags_USER4:        Diags.ALWAYS_OFF,
   144            diags_USER5:        Diags.ALWAYS_OFF,
   145            diags_USER6:        Diags.ALWAYS_OFF,
   146            diags_USER7:        Diags.ALWAYS_OFF,
   147            diags_INFO:         Diags.ALWAYS_OFF,
   148            diags_USER8:        Diags.ALWAYS_OFF,
   149            diags_ANALYSIS:     Diags.ALWAYS_OFF,
   150            fxntab:             true,
   151            gate:               null,
   152            gateParams:         null,
   153            instanceHeap:       null,
   154            instanceSection:    null,
   155            logger:             null,
   156            memoryPolicy:       Types.DELETE_POLICY,
   157            namedInstance:      false,
   158            namedModule:        true,
   159            romPatchTable:      false,
   160        };
   161    
   162        /*! 
   163         *  ======== noRuntimeCommon$ ========
   164         *  Defaults inherited by the target modules that do not need the runtime
   165         *  support.
   166         *
   167         *  Modules for which the attribute NoRuntime is set do not use any
   168         *  functionality controlled by the parameters in their `common$`
   169         *  structures. For such modules, these parameters are set to the
   170         *  following values, and cannot be changed, to guarantee that NoRuntime
   171         *  modules do not accidentally request functionality they don not use.
   172         */
   173        metaonly readonly config Types.Common$ noRuntimeCommon$ = {
   174            diags_ASSERT:       Diags.ALWAYS_OFF,
   175            diags_ENTRY:        Diags.ALWAYS_OFF,
   176            diags_EXIT:         Diags.ALWAYS_OFF,
   177            diags_INTERNAL:     Diags.ALWAYS_OFF,
   178            diags_LIFECYCLE:    Diags.ALWAYS_OFF,
   179            diags_STATUS:       Diags.ALWAYS_OFF,
   180            diags_USER1:        Diags.ALWAYS_OFF,
   181            diags_USER2:        Diags.ALWAYS_OFF,
   182            diags_USER3:        Diags.ALWAYS_OFF,
   183            diags_USER4:        Diags.ALWAYS_OFF,
   184            diags_USER5:        Diags.ALWAYS_OFF,
   185            diags_USER6:        Diags.ALWAYS_OFF,
   186            diags_USER7:        Diags.ALWAYS_OFF,
   187            diags_INFO:         Diags.ALWAYS_OFF,
   188            diags_USER8:        Diags.ALWAYS_OFF,
   189            diags_ANALYSIS:     Diags.ALWAYS_OFF,
   190            fxntab:             false,
   191            gate:               null,
   192            gateParams:         null,
   193            instanceHeap:       null,
   194            instanceSection:    null,
   195            logger:             null,
   196            memoryPolicy:       Types.STATIC_POLICY,
   197            namedInstance:      false,
   198            namedModule:        false,
   199            romPatchTable:      false,
   200        };
   201        
   202        /*!
   203         *  ======== getCommon ========
   204         *  Get a specified common parameter from a module
   205         *
   206         *  Get the value of a member of the structure `common$` based on
   207         *  defaults and the current value of the parameter. If the current value
   208         *  of `param` is `undefined`, the function returns the default value
   209         *  for that parameter from `Default.common$`.
   210         *
   211         *  @param(eb)  module whose parameter is queried
   212         *
   213         *  @param(param)   string naming the queried parameter
   214         *
   215         *  @a(returns)
   216         *  Returns the value of the parameter named `param` from the module
   217         *  `mod`.
   218         */
   219        metaonly Any getCommon(IModule.Module mod, String param);
   220    };
   221    /*
   222     *  @(#) xdc.runtime; 2, 1, 0,359; 11-16-2011 11:00:13; /db/ztree/library/trees/xdc/xdc-y13x/src/packages/
   223     */
   224