interface xdc.runtime.ITimestampProvider

Timestamp provider interface

This interface is implemented by platform-specific modules that "provide" underlying timestamp services for the xdc.runtime.Timestamp module. [ more ... ]
XDCspec summary sourced in xdc/runtime/ITimestampProvider.xdc
interface ITimestampProvider {  ...
    // inherits xdc.runtime.IModule
XDCspec declarations sourced in xdc/runtime/ITimestampProvider.xdc
package xdc.runtime;
 
interface ITimestampProvider inherits ITimestampClient {
module-wide config parameters
module-wide functions
}
DETAILS
This interface is implemented by platform-specific modules that "provide" underlying timestamp services for the xdc.runtime.Timestamp module.
Only the xdc.runtime.Timestamp module and the xdc.runtime.ITimestampClient interface should be directly referenced by platform-independent applications.
This interface is part of a design pattern that includes the ITimestampClient interface and the Timestamp module. This pattern allows client code to:
  • use the platform-independent interfaces provided by either ITimestampClient and Timestamp and remain 100% portable
  • optionally leverage platform-specific capabilities of any module that implements ITimestampProvider and still always have access to the platform-independent methods specified by ITimestampClient (because ITimestampProvider inherits from ITimestampClient)
This pattern is in contrast to other "provider" interfaces that exist only to specify the methods necessary to enable "higher-level" modules; client code *never* accesses these provider interfaces directly, clients always only use the higher-level modules.
 
metaonly config ITimestampProvider.common$  // module-wide

Common module configuration parameters

XDCspec declarations sourced in xdc/runtime/ITimestampProvider.xdc
metaonly config Types.Common$ common$;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
 
ITimestampProvider.get32()  // module-wide

Return a 32-bit timestamp

XDCspec declarations sourced in xdc/runtime/ITimestampProvider.xdc
Bits32 get32();
 
RETURNS
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
SEE
 
ITimestampProvider.get64()  // module-wide

Return a 64-bit timestamp

XDCspec declarations sourced in xdc/runtime/ITimestampProvider.xdc
Void get64(Types.Timestamp64 *result);
 
ARGUMENTS
result — pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
SEE
 
ITimestampProvider.getFreq()  // module-wide

Get the timestamp timer's frequency (in Hz)

XDCspec declarations sourced in xdc/runtime/ITimestampProvider.xdc
Void getFreq(Types.FreqHz *freq);
 
ARGUMENTS
freq — pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
SEE
generated on Fri, 17 May 2019 20:27:13 GMT