Third party open source tools required by XDCtools
The following jars are part of this package:
[
more ... ]
XDCspec declarations |
sourced in xdc/shelf/package.xdc |
package xdc.shelf [1, 0, 0] {
}
DETAILS
The following jars are part of this package:
In addition to the jars above, XDCtools requires the following
third-party software:
Although the following tools are not required, they are optionally shipped
with XDCtools distributions to ensure consistent behavior across various
development platforms.
Exe |
Version |
License |
From |
Description |
zip, unzip |
2.3 and 5.50 |
info-zip |
http://www.info-zip.org |
command line utilities to zip and unzip package releases |
tar |
1.21 |
GPL v3 |
http://www.gnu.org/software/tar |
command line utilities to archive package directories |
sh, gunzip, gzip, sed |
cygwin 1.5.25-15 |
GPL v2 |
http://cygwin.com |
(Windows only) korn shell compatible shell used by GNU make |
cat, cp, date, echo, mkdir, mv, pwd, rm, touch |
cygwin 1.5.25-15 (coreutils 6.10) |
GPL v3 |
http://cygwin.com |
(Windows only) common utilites called from GNU make makefiles |
All other files that are part of XDCtools are licensed under either
EPL v1.0 or dual-licensed under
EDL v1.0.
generated on Fri, 16 Feb 2018 20:50:34 GMT