Introduction, Documentation, License, Special Notes, What's New, Defect History, Upgrade & Compatibility Information, Host Support, Dependencies, Device Support, Validation Info, Known Issues, Version Information, Technical Support.
RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.
The XDCtools product includes the following components:
The product documentation for this release is available in two formats:
Both formats are delivered with the product in the docs subdirectory. The most up-to-date docs can also be viewed in the RTSC-pedia
Release notes from previous product releases are available in the relnotes_archive directory. Note that XDCtools 3.21 (supports only the MSP430 device family) is shipped only with the Grace product.
XDCtools contains elements released under the Eclipse Public License v1.0 and a number of other open-source licenses, detailed here.
The following significant changes are included in XDCtools 3.23 :
Host OS | Default Install Directory |
MS Windows (XP and 7) | C:\ti |
Linux root user | /opt/ti |
Linux non-root user | $HOME/ti |
Bugs against the XDCtools product may be filed in Eclipse Bugzilla.
The following defects and enhancement requests were resolved in this release. For more information on these bugs, or to see a more up to date list, go here.
ID | Description |
360745 | remove --symbol_map from linker.cmd (.xdl) files for TI/ELF targets |
364431 | xdc.runtime Grace .xml files need to be updated to use new instance scheme |
366639 | move 'atexit()' call in System to a "lastFxn" instead of module_startup |
366646 | Add new platforms for OMAPL138 and C6748 Low cost development kit (LCDK) boards |
367139 | M3 and C28 frequencies need to be shown on the Concerto Boot config page |
367140 | The flash is slow on Concerto's M3 with SYS/BIOS |
367520 | MSP430F2618 timer interrupts and number of interrupts in peripheral definitions is incorrect |
367674 | A command line passed to xdc.exec works on Windows but fails on Linux |
367805 | tar-based release archives may include excluded directories. |
369158 | generated instance create function sometimes contains unnecessary initialized variables |
369572 | google.targets's remoteHost support should switch from rsh to ssh |
369719 | Enable targets to create/set new env vars when executing cmds |
370016 | Add QNX target |
The packages comprising the XDCtools release are uniquely identified by a compatibility key defined in the package.xdc file of a package. Please note that the package compatibility keys are independent of XDC product release numbers.
Package compatibility keys are intended to:
Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:
This release supports the following hosts:
This release requires the following other software components and tools versions to successfully function:
This release supports the following device families:
This release was built and validated against using the following components:
RTSC Target | Code Generation Tools |
ti.targets.[C64P,C64P_big_endian,C67P,C674,C674_big_endian,C64T,C64T_big_endian] | 7.0.3 (TMS320C6x) |
ti.targets.[C28,C28_large,C28_float] | 5.2.3 (TMS320C2000) |
ti.targets.[C66,C66_big_endian];ti.targets.elf.[C64P,C64P_big_endian,C64T,C64T_big_endian,C674,C674_big_endian,C67P,C66,C66_big_endian] | 7.2.0 (TMS320C6x) |
ti.targets.arm.elf.[TMS470,Arm7,Arm9,Arm9t,A8Ft,M3,M3_big_endian,R4,R4_big_endian,R4t,R4t_big_endian,R4F,R4F_big_endian,R4Ft_big_endian] | 4.9.0 (ARM/TMS470) |
gnu.targets.MVArm9,gnu.targets.arm.GCArmv5T | 3.4.3 (GCC Montavista) |
gnu.targets.UCArm9 | 4.2.1 (GCC Opensource) |
gnu.targets.arm.GCArmv6,GCArmv7A | 4.3.2 (GCC Codesourcery) |
gnu.targets.[Linux86,Sparc] | 4.1.0 (GCC Opensource) |
gnu.targets.Mingw | 4.4.0 (GCC MingW) |
microsoft.targets.Net32 | 13.10.3052 (Microsoft .NET C/C++) |
microsoft.targets.Win32 | 14.00.50727.42 (Microsoft Visual C/C++) |
microsoft.targets.VC98 | 12.00.8168 (Microsoft Visual C/C++) |
microsoft.targets.arm.WinCE | Microsoft WinCE 6.00 |
ti.targets.msp430.[MSP430,MSP430X,MSP430X_small] | 3.3.0(MSP430) |
Android Bionic | 4.4.3 |
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.
Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
Support questions on the product should be posted to the RTSC newsgroup. Check the XDCtools download site for the latest releases.
Last updated: February 10, 2012 Build Ver: 3.23.01.43 Rev: