1    /*
     2     *  Copyright 2014 by Texas Instruments Incorporated.
     3     *
     4     */
     5    
     6    /*!
     7     *  ======== Main ========
     8     *  Command-line tool for generating projectspec files for RTSC content
     9     *
    10     *  The `trexgen` tool allows RTSC content producers to
    11     *  create projectspec files that allows their content to be
    12     *  integrated in the CCS Resource Explorer environment. As input,
    13     *  the tool requires
    14     *  @p(blist)
    15     *      - a RTSC module implementing {@link xdc.tools.product.IProduct}
    16     *  @p
    17     *  Refer to {@link ./doc-files/ExampleProduct.xdc ExampleProduct}
    18     *  for an implementation of {@link xdc.tools.product.IProduct IProduct}.
    19     *
    20     *  The tool generates starter examples that will showup
    21     *  in the Resource explorer. This is accomplished by implementing
    22     *  {@link xdc.tools.product.IProductTemplate IProductTemplate} and setting
    23     *  the {@link xdc.tools.product.IProduct#templateModule templateModule}
    24     *  configuration parameter of the {@link xdc.tools.product.IProduct IProduct}
    25     *  implementation to the name of the implementation module.
    26     *  Refer to {@link ./doc-files/Examples.xdc Examples}
    27     *  for a sample implementation of {@link
    28     *  xdc.tools.product.IProductTemplate IProductTemplate}.
    29     *
    30     *  The tool operates on a product that is either specified by the `-p`
    31     *  option or is present in the folder from which the tool is executed.
    32     *  The tool will create the resources sub-folder in the output directory
    33     *  specified with `-o` option. If the `-o`
    34     *  option is not specified the resources is created in the product root
    35     *  directory.
    36     *
    37     *  The tool will search the repositories specified in the module
    38     *  implementing {@link xdc.tools.product.IProduct} for RTSC platforms.
    39     *  This search can be disabled by specifying the`--disable_repo_search`
    40     *  option. The user needs to ensure that the repositories are installed
    41     *  in the product root directory before using the tool.
    42     *
    43     *  @a(Example)
    44     *  @p(code)
    45     *      xs xdc.tools.product.trexgen
    46     *                      -p exampleprod_1_0_0_00
    47     *                      -m xdc.tools.product.plugingen.examples.ExampleProduct
    48     *  @p
    49     */
    50    metaonly module Main inherits xdc.tools.ICmd
    51    {
    52        override config String usage[] = [
    53            '[-p product_root_directory]',
    54            ' -m module',
    55            '[-o outdir]'
    56        ];
    57    
    58    instance:
    59    
    60        /*!
    61         *  ======== productDir ========
    62         *  Product root directory
    63         *
    64         *  This option names the product root directory that is used by the
    65         *  tool to generate the projectspec files.  For example, it's declared
    66         *  repositories are added to the package path and are searched for
    67         *  contributed platforms.
    68         *
    69         *  If the '-o' option is not specified, the tool generates the resources
    70         *  directory in the product root directory.
    71         *
    72         *  If this option is not specified, the product root directory is
    73         *  assumed to be `./`.
    74         *
    75         */
    76        @CommandOption("p")
    77        config String productDir = "./";
    78    
    79        /*!
    80         *  ======== productModule ========
    81         *  Input description of the plug-in to be specified
    82         *
    83         *  This required option names a module that implements
    84         *  `{@link xdc.tools.product.IProduct}`.
    85         */
    86        @CommandOption("m")
    87        config String productModule;
    88    
    89        /*!
    90         *  ======== outputDir ========
    91         *  Output directory in which the plugin will be generated.
    92         *
    93         *  This option names the directory in which the project spec
    94         *  will be generated in a sub-directory named `eclipse`.
    95         *  If this option is not specified the tool will generate
    96         *  the plugin in the product root directory specified with
    97         *  the '-p' option.
    98         */
    99        @CommandOption("o")
   100        config String outputDir = null;
   101    
   102        /*!
   103         *  ======== generationFormat ========
   104         *  Plugin generation format
   105         */
   106        @CommandOption("generation_format")
   107        config String generationFormat = null;
   108    
   109        /*!
   110         *  ======== run ========
   111         */
   112        override Any run(xdc.tools.Cmdr.Instance cmdr, String args[]);
   113    }
   114    /*
   115     *  @(#) xdc.tools.product.trexgen; 1, 0, 0,48; 10-15-2014 16:33:59; /db/ztree/library/trees/xdctools/xdctools-f57x/src/
   116     */
   117