![]() |
![]() |
Introduction, Documentation, License, What's New, Upgrade & Compatibility Information, Host Support, Dependencies, Device Support, Validation Info, Known Issues, Version Information, Technical Support.
RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.
The XDCtools product includes the following components:
The product documentation for this release is available in two formats:
Both formats are delivered with the product in the docs subdirectory. The most up-to-date docs can also be viewed in the RTSC-pedia
Release notes from previous product releases are available in the relnotes_archive directory. Note that XDCtools 3.21 (supports only the MSP430 device family) is shipped only with the Grace product.
XDCtools contains elements released under the Eclipse Public License v1.0 and a number of other open-source licenses, detailed here.
The following significant changes are included in XDCtools 3.22 :
Bugs against the XDCtools product maybe filed in the eclipse bugzilla.
The following defects were resolved in this release:
ID Headline ECL283354 Templates that throw exceptions can corrupt the config model ECL291248 Closing XGCONF "Available Packages" view before it is populated causes an exception ECL291845 mod__prologue.h and mod__epilogue.h are not automatically added to pkg ECL293232 gconf: closing the outline view of a config corrupts the GUI lists ECL303338 xgconf: should remember previous property page when configuring a module ECL315708 cannot set 'fxn' field in ti.sysbios.family.c64p.EventCombiner array ECL317527 IInstance.name needs link to common$.namedInstance ECL321075 XDCtool error parser should filter out stack traceback error ECL321158 Config crash when XDCBUILDCFG assigned a file with a space in its path ECL322858 Building Java code in packages fails if pathnames have spaces ECL328989 setting Text.isLoaded to true causes Diags_setMask() to access random memory ECL329837 Platform wizard throws an exception while using the TMS320DM365 device ECL331949 gnu.targets.ITarget.xs's link cmd should first rm the generated .map file (in case it's read only) ECL332570 xdc.tools.Server SecurityManager can cause CCSv5 to refuse to close ECL332985 gnu.targets link fails if a filename contains '-' ECL334317 trailing white space in XDCTARGETS corrupts the environment ECL340213 Platform wizard does not search user repository while importing platforms
The packages comprising the XDCtools release are uniquely identified by a compatibility key defined in the package.xdc file of a package. Please note that the package compatibility keys are independent of XDC product release numbers.
Package compatibility keys are intended to:
Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:
This release supports the following hosts:
This release requires the following other software components and tools versions to successfully function:
This release supports the following device families:
This release was built and validated against using the following components:
RTSC Target | Code Generation Tools |
ti.targets.[C64P,C64P_big_endian,C67P,C674,C674_big_endian,C64T,C64T_big_endian] | 7.0.3 (TMS320C6x) |
ti.targets.[C28,C28_large,C28_float] | 5.2.3 (TMS320C2000) |
ti.targets.[C66,C66_big_endian];ti.targets.elf.[C64P,C64P_big_endian,C64T,C64T_big_endian,C674,C674_big_endian,C67P,C66,C66_big_endian] | 7.2.0 (TMS320C6x) |
ti.targets.arm.elf.[TMS470,Arm7,Arm9,Arm9t,A8Ft,M3,M3_big_endian,R4,R4_big_endian,R4t,R4t_big_endian,R4F,R4F_big_endian,R4Ft_big_endian] | 4.9.0 (ARM/TMS470) |
gnu.targets.MVArm9,gnu.targets.arm.GCArmv5T | 3.4.3 (GCC Montavista) |
gnu.targets.UCArm9 | 4.2.1 (GCC Opensource) |
gnu.targets.arm.GCArmv6,GCArmv7A | 4.3.2 (GCC Codesourcery) |
gnu.targets.[Linux86,Sparc] | 4.1.0 (GCC Opensource) |
gnu.targets.Mingw | 4.4.0 (GCC MingW) |
microsoft.targets.Net32 | 13.10.3052 (Microsoft .NET C/C++) |
microsoft.targets.Win32 | 14.00.50727.42 (Microsoft Visual C/C++) |
microsoft.targets.VC98 | 12.00.8168 (Microsoft Visual C/C++) |
microsoft.targets.arm.WinCE | Microsoft WinCE 6.00 |
ti.targets.msp430.[MSP430,MSP430X,MSP430X_small] | 3.3.0(MSP430) |
ID Headline ECL280863 xgconf: If instances have required args, should force user to enter something ECL280869 xgconf: Can create two instances with the same name ECL305948 xgconf does not respond to config file rename ECL321074 xgconf and XDCtools error parser add duplicate errors to Problems view ECL342651 XGCONF should allow disable static creation in a RTSC modules
All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng).
This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.
Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.
Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.
Support questions on the product should be posted to the RTSC newsgroup. Check the XDCtools download site for the latest releases.
Last updated: May 02, 2011 Build Ver: 3.22.00.09 Rev: