Texas Instruments Technology for Innovators(tm)

XDCtools 3.30.00.21 GA Release Notes

March 23, 2014

Contents


Introduction

RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.

The XDCtools product includes the following components:

XDCtools releases prior to release 3.30 also included the following components:

For more information about where these components are now available, see the Upgrade & Compatibility Information section below.

back to top


Licensing

Almost all of XDCtools is released under either EPL v1.0 or dual-licensed under EPL or EDL v1.0. However, there are also a number of third-party components included which are made available under a number of other open-source licenses. A complete manifest along with export control information is detailed here.

back to top


Documentation

The product documentation for this release is available in two formats:

Both formats are delivered with the product in the docs subdirectory. The most up-to-date docs can also be viewed in the RTSC-pedia.

Release notes from previous product releases are available in the relnotes_archive directory.

back to top


What's New

Over 50 issues have been addressed in this release. The following notable defects and enhancements were resolved in this release:

ID Severity Headline
417736 critical ErrorParser fails to add errors/warnings from config to Problems View
314748 critical xgconf: names of new instances don't always stick; sometimes rename required
425836 major Place all Big.c constants and data in their own section for GNU targets
280867 major xgconf: Add module instance while script is validating is ignored
426201 major GCC rtsv7M/startup.c should copy initial .data values only if load and run addresses are different
427431 normal "When loading jvm.dll, xs.exe can fail to find msvcr71.dll
425917 normal require new #define to access deprecated std.h types
425832 normal xdc.tools.configuro -D option does not work
424486 normal Products that have their own XDC runtime support need a way to disable the standard implementation
424399 normal Add support for new ROM build
423117 normal Add DWARF parser for ROV Mod_Construct support
413743 normal New RTSC Config wizard does not use selected project to create new cfg file.
365673 normal remove references to atexit(), exit() and abort() from System module
423119 normal iar.tools.configuro fails when multiple .cfg files are in a project.
324022 normal Time optimization for RTSC configuration
428926 normal cdoc meta-domain instance creation Params structure links to target-domain Params
427404 normal MSP430 rts library needs auto_init_hold_wdt to work with new --cinit_hold_wdt link option
428830 normal cdoc generates 'null' name for C SYNOPSIS links of instance config params
428953 normal cdoc meta-domain metaonly per-instance config parameters have broken links
324468 enhancement ROV top level views
323548 enhancement Reduce module list clicks in ROV
423076 normal Cntrl - C and Cntrl - V functionality within ROV cells does not work.
423341 normal HeapMin needs an ROV view
428051 normal LoggerBuf should set it's timestamp proxy in package close()
320943 normal Can't use a Module API name as a project name if xdc/cfg/globals.h is included
309891 minor Viewing ROV "UArg" fields in ROV should allow choosing radix

To see a complete list of issues fixed in this release, click here.

back to top


Upgrade and Compatibility Information

Deleted Content

Beginning with the 3.30 release, all embedded targets and platforms have been removed from the default release (a.k.a. the "Core" release) so they can be delivered with middleware products, such as TI-RTOS and Grace, that have dependencies only on specific targets and platforms. This has the advantage of greatly reducing the size of XDtools for users who are only interested in a relatively small number of embedded architectures. But, it also breaks compatibility for users who expect to always have their favorite architecture's support included in XDCtools releases.

To simplify the migration to this new distribution and to support size reduced installations, XDCtools 3.30 is available in several different release bundles:

Target Runtime APIs

The xdc.runtime package: As part of the effort to enable xdc.runtime to more easily fit into the ROM of most devices (Bug 424399), several significant optimizations had to be made made that break strict binary compatibility with target content libraries built with XDCtools 3.25.x (or earlier). In particular, target content built against XDCtools 3.25.x xdc.runtime can be

Deprecated types: To reduce conflicts with target content produced by other groups, the deprecated types Uns, Uint, Uint16, etc. are no longer defined by default. If you still need to use these types, you must now define the symbol xdc__deprecated_types when compiling sources that reference these types. See Bug 425917 for details.

Package Compatibility

Package internal files: All generated package internal files are backwards compatible starting from XDCtools 3.20. So, packages created using XDCtools 3.20 or later can be consumed using this release. Because of the addition of the target type CString to XDCtools 3.25.x, packages created with this release that contain non-metaonly modules cannot be used with XDCtools releases earlier than XDCtools 3.25.x. This includes the xdc.runtime package. See XDCtools Internal Version Numbers for additional details.

Package-specific APIs: Each package has a compatibility key defined in its package.xdc specification file. No package compatibility keys were changed in this release.

Please note that the package compatibility keys are independent of XDCtools product release numbers (described in Versioning below). Package compatibility keys:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey end-user requirements when re-integrating specific components.

Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:

back to top


Host Support

This release supports the following hosts:

back to top


Dependencies

With the exception of a C compiler, XDCtools is a fully self-contained set of development tools to create, build, run, and monitor embedded target content. If you use any of the tool sets listed below, you should use the version named in order to successfully use this version of XDCtools:

back to top


Device Support

Starting with release 3.30, each release of XDCtools is available in one of several distribution bundles each supporting a varying number of device families. This allows products (such as CCS) to selectively embed a distribution that is as small as possible.

The "Core" distribution (identified by the "_core" qualifier in installation directory name) has no embedded device support. As a result, "Core" users must either use another product (such as TI-RTOS 2.0) which includes any necessary device support or explicitly add a repository containing the desired device support to the package path of their projects.

The "full" distribution (identified by the lack of any qualifier in the installation directory name) supports the following device families:

The complete list of targets supported by this release can be found here.

back to top


Validation Information

This release was built and validated using Code Composer Studio version 6.0.

The targets supported by this release and the versions of the compilers used to validate them are listed here.

Go to the Known Issues section of these release notes to see any issues with the supported targets that were found during the validation of this release.

back to top


Known Issues

To see a complete list of open XDCtools issues, go to the Eclipse RTSC project's Bugzilla database.

The following table highlights known issues of particular importance.

ID Headline
399012 ti.targets.arm.ARP32_far link may fail

To file a new bug in this database, click here.

back to top


Versioning

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, release candidates, etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng) and should not be used in a production environment.

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.

Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top


Technical Support and Product Updates

Support questions on the product should be posted to the Eclipse RTSC project's newsgroup. Check the XDCtools download site for the latest releases.

back to top


Last updated: March 23, 2014 Build Ver: 3.30.00.21 Rev: t21