1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== ISemProcessSupport.xdc ========
    15     */
    16    
    17    import xdc.runtime.Error;
    18    
    19    /*! 
    20     *  ======== ISemProcessSupport ========
    21     *  Interface for OS specific back-end.
    22     *
    23     *  The {@link xdc.runtime.knl} package contains modules that provide typical
    24     *  OS services. These xdc.runtime.knl modules however require proxies to be
    25     *  bound to an OS specific delegate. This specifies the interface to 
    26     *  be implemented by the OS specific delegate for 
    27     *  {@link xdc.runtime.knl#SemProcess} module.
    28     *
    29     *  create() takes a 32-bit integer key parameter to be used for identifying
    30     *  the semaphore to create across processes. For example, for Linux System V
    31     *  semaphores, the key is necessary so that different processes can access
    32     *  the same semaphore.
    33     */
    34    interface ISemProcessSupport inherits ISemaphore
    35    {
    36    
    37    instance:
    38    
    39       /*!
    40        *  ======== create ========
    41        *  Create a SemProcess object.
    42        *
    43        *  This function creates a new `SemProcess` object which is 
    44        *  initialized to count.  
    45        *  All semaphores created with the same key reference the same
    46        *  underlying synchronization object and work between processes.  The
    47        *  underlying synchronization object should be automatically deleted when
    48        *  all references to it have been deleted, and the reference count should
    49        *  be maintained consistently across process forks or similar operations.
    50        *  An implementation for a platform on which this is technically impossible
    51        *  (e.g. an operating system that does not support multiple processes) may
    52        *  provide a 'toy' implementation with behavior matching that of
    53        *  `{@link ISemProcessSupport}`.
    54        *
    55        *  @param(count)    initial semaphore count
    56        *  @param(key)      globally unique key
    57        */
    58        create(Int count, Int key);
    59    
    60    }
    61    /*
    62     *  @(#) xdc.runtime.knl; 1, 0, 0,293; 5-30-2014 17:53:52; /db/ztree/library/trees/xdc/xdc-A42x/src/packages/
    63     */
    64