Texas Instruments Technology for Innovators(tm)

XDCtools 3.25.01.65 GA Release Notes

June 11, 2013

Contents


Introduction

RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.

The XDCtools product includes the following components:

back to top


Licensing

Almost all of XDCtools is released under either EPL v1.0 or dual-licensed under EPL or EDL v1.0. However, there are also a number of third-party components included which are made available under a number of other open-source licenses. A complete manifest along with export control information is detailed here.

back to top


Documentation

The product documentation for this release is available in two formats:

Both formats are delivered with the product in the docs subdirectory. The most up-to-date docs can also be viewed in the RTSC-pedia.

Release notes from previous product releases are available in the relnotes_archive directory.

back to top


What's New

The following significant changes are included in this release:

The following notable defects and enhancements were also resolved in this release:

ID Headline
407679 memory is setup incorrectly in TMS320F28332.cmd file
405824 When loading jvm.dll, xs.exe should find msvcr71.dll in jre/bin

To see a complete list of issues fixed in this release, click here.

back to top


Upgrade and Compatibility Information

Additions

The following table lists the targets, platforms, and other packages that have been added (relative to XDCtools 3.24.x).

Category Packages
Targets
Platforms ti.platforms.arm, ti.platforms.arp32, ti.platforms.c6000, ti.platforms.evmTCI6638K2K, ti.platforms.evmDRA7XX
Other

Deletions

The legacy BIOS 5 tconf configuration utility has been removed along will all support for .tcf configuration scripts.

The following table lists the targets, platforms, and other packages that have been removed (relative to XDCtools 3.24.x).

Category Packages
Targets gnu.targets.arm.rts470MV gnu.targets.arm.rts470uC, gnu.targets.rts470MV, gnu.targets.rts470uC, ti.targets.rts5400, ti.targets.rts5500
Platforms ti.platforms.app510, ti.platforms.control28055, ti.platforms.doc, ti.platforms.dsk5402, ti.platforms.dsk5416, ti.platforms.dsk5505, ti.platforms.dsk5510, ti.platforms.dsk6211, ti.platforms.dsk6416, ti.platforms.dsk6711, ti.platforms.dsk6713, ti.platforms.evm2530, ti.platforms.evm5471, ti.platforms.evm5505, ti.platforms.evm5505ext, ti.platforms.evm5509, ti.platforms.evm5509A, ti.platforms.evm5515, ti.platforms.evm5517, ti.platforms.evm5525, ti.platforms.evmC6A8168, ti.platforms.evmDM357, ti.platforms.evmDM420, ti.platforms.evmDM642, ti.platforms.evmDM6446, ti.platforms.evmDM6467, ti.platforms.evmDM6467T, ti.platforms.evmDRA416, ti.platforms.evmDRA446, ti.platforms.evmDRA459, ti.platforms.expOMAPL138, ti.platforms.ezdsp2808, ti.platforms.ezdsp2812, ti.platforms.ezdsp5502, ti.platforms.ezdsp5505, ti.platforms.ezdsp5535, ti.platforms.h2omap1610, ti.platforms.h3omap1710, ti.platforms.h4omap2420, ti.platforms.innovator1510, ti.platforms.osk5912, ti.platforms.padk6727, ti.platforms.sdbTitan, ti.platforms.sdp2430, ti.platforms.sim2810, ti.platforms.sim54xx, ti.platforms.sim55xx, ti.platforms.sim62xx, ti.platforms.sim64xx, ti.platforms.sim67xx, ti.platforms.simDM420, ti.platforms.simDM730, ti.platforms.simDM740, ti.platforms.simDucati, ti.platforms.simTCI6498, ti.platforms.skAM3358, ti.platforms.teb5561, ti.platforms.teb6416, ti.platforms.app510
Other xdc.tools.configuro.ccs, ti.catalog.c5400, ti.catalog.c5500

Package Compatibility

Package internal files: All generated package internal files are backwards compatible starting from XDCtools 3.20. So, packages created using XDCtools 3.20 or later can be consumed using this release. Because of the addition of the new target type CString, packages created with this release that contain non-metaonly modules can not be used with earlier XDCtools releases. This includes the xdc.runtime package. See XDCtools Internal Version Numbers for additional details.

Package-specific APIs: Each package has a compatibility key defined in its package.xdc specification file. No package compatibility keys were changed in this release.

Please note that the package compatibility keys are independent of XDCtools product release numbers (described in Versioning below). Package compatibility keys:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey end-user requirements when re-integrating specific components.

Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:

back to top


Host Support

This release supports the following hosts:

back to top


Dependencies

With the exception of a C compiler, XDCtools is a fully self-contained set of development tools to build and run embedded target content. If you use any of the tool sets listed below, you should use the version named in order to successfully use this version of XDCtools:

back to top


Device Support

This release supports the following device families:

The complete list of targets supported by this release can be found here.

back to top


Validation Information

This release was built and validated using Code Composer Studio version 5.4.0.

The targets supported by this release and the versions of the compilers used to validate them are listed here.

Go to the Known Issues section of these release notes to see any issues with the supported targets that were found during the validation of this release.

back to top


Known Issues

To see a complete list of open XDCtools issues, go to the Eclipse RTSC project's Bugzilla database.

The following table highlights known issues of particular importance.

ID Headline
399012 ti.targets.arm.ARP32_far link may fail

To file a new bug in this database, click here.

back to top


Versioning

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, release candidates, etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng) and should not be used in a production environment.

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.

Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top


Technical Support and Product Updates

Support questions on the product should be posted to the Eclipse RTSC project's newsgroup. Check the XDCtools download site for the latest releases.

back to top


Last updated: June 11, 2013 Build Ver: 3.25.01.65 Rev: r65