package xdc.tools.product.trexgen |
|
Command-line tool for generating projectspec files for RTSC content
The
trexgen tool allows RTSC content producers to
create projectspec files that allows their content to be
integrated in the CCS Resource Explorer environment. As input,
the tool requires
[
more ... ]
package xdc.tools.product.trexgen [1, 0, 0] {
// Command implementation
}
USAGE
xs xdc.tools.product.trexgen [--help]
[-p product_root_directory]
-m module
[-o outdir]
OPTIONS
- -p
- Product root directory
This option names the product root directory that is used by the
tool to generate the projectspec files. For example, it's declared
repositories are added to the package path and are searched for
contributed platforms.
If the '-o' option is not specified, the tool generates the resources
directory in the product root directory.
If this option is not specified, the product root directory is
assumed to be ./.
- -m
- Input description of the plug-in to be specified
This required option names a module that implements
xdc.tools.product.IProduct.
- -o
- Output directory in which the plugin will be generated
This option names the directory in which the project spec
will be generated in a sub-directory named eclipse.
If this option is not specified the tool will generate
the plugin in the product root directory specified with
the '-p' option.
- --generation_format
- Plugin generation format
DETAILS
The trexgen tool allows RTSC content producers to
create projectspec files that allows their content to be
integrated in the CCS Resource Explorer environment. As input,
the tool requires
Refer to
ExampleProduct
for an implementation of
IProduct.
The tool generates starter examples that will showup
in the Resource explorer. This is accomplished by implementing
IProductTemplate and setting
the
templateModule
configuration parameter of the
IProduct
implementation to the name of the implementation module.
Refer to
Examples
for a sample implementation of
IProductTemplate.
The tool operates on a product that is either specified by the -p
option or is present in the folder from which the tool is executed.
The tool will create the resources sub-folder in the output directory
specified with -o option. If the -o
option is not specified the resources is created in the product root
directory.
The tool will search the repositories specified in the module
implementing
xdc.tools.product.IProduct for RTSC platforms.
This search can be disabled by specifying the
--disable_repo_search
option. The user needs to ensure that the repositories are installed
in the product root directory before using the tool.
EXAMPLE
xs xdc.tools.product.trexgen
-p exampleprod_1_0_0_00
-m xdc.tools.product.plugingen.examples.ExampleProduct
generated on Tue, 16 Oct 2012 23:14:48 GMT