1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== IGateProcessSupport.xdc ========
15 */
16
17 import xdc.runtime.Error;
18
19 /*!
20 * ======== IGateProcessSupport ========
21 * Interface for OS specific back-end.
22 *
23 * The {@link xdc.runtime.knl} package contains modules that provide typical
24 * OS services. These xdc.runtime.knl modules require proxies to be
25 * bound to an OS specific delegate. This specifies the interface to
26 * be implemented by the OS specific delegate for
27 * {@link xdc.runtime.knl#GateProcess} module.
28 *
29 * The implementation of IGateThreadSupport should try to implement a gate
30 * that supports priority inversion.
31 */
32 interface IGateProcessSupport inherits IGateThreadSupport
33 {
34
35 /*! Status returned by {@link #getReferenceCount} when there is an error */
36 const Int GETREFCOUNT_FAILED = -1;
37
38 instance:
39
40 config Int key = -1; /*! globally unique key for SysV-style semaphore */
41
42 /*!
43 * ======== create ========
44 * Create a GateProcess object.
45 *
46 * This function creates a new `GateProcess` object which is initialized to
47 * count. All gates created with the same key reference the same
48 * underlying synchronization object and work between processes. The
49 * underlying synchronization object should be automatically deleted when
50 * all references to it have been deleted, and the reference count should
51 * An implementation for a platform on which this is technically impossible
52 * (e.g. an operating system that does not support multiple processes) may
53 * provide a 'toy' implemenation with behavior matching that of
54 * IGateProcessSupport.
55 */
56 override create();
57
58 /*!
59 * ======== getReferenceCount ========
60 * Get the number of processes with references to this Gate.
61 *
62 * @param(err) Pointer to Error.Block
63 * @a(returns) Returns the number of processes that possess a
64 * reference to this gate, or GETREFCOUNT_FAILED if an
65 * error occured.
66 * A 'toy' implementation should always return 0.
67 */
68 Int getReferenceCount(Error.Block* err);
69
70 }
71 /*
72 * @(#) xdc.runtime.knl; 1, 0, 0,197; 10-7-2012 14:10:05; /db/ztree/library/trees/xdc/xdc-y37x/src/packages/
73 */
74