1 /*
2 * Copyright (c) 2012 by Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12
13 /*
14 * ======== Platform.xdc ========
15 */
16 package ti.platforms.stellaris;
17
18 /*!
19 * ======== Platform ========
20 * A generic platform that supports any Stellaris device
21 *
22 * The device to be used by this platform is passed as the platform instance
23 * name. On the `xdc.tools.configuro` command line, it is done in the
24 * following way:
25 * @p(code) 26 * xs xdc.tools.configuro ... -p "ti.platforms.stellaris:LM3S8971"
27 * @p 28 *
29 * In package.bld, the platform instance is selected as in:
30 * @p(code) 31 * Pkg.addExecutable("test", target, "ti.platforms.stellaris:LM3S8971");
32 * @p 33 */
34 metaonlymodule Platform inherits xdc.platform.IPlatform
35 {
36 config xdc.platform.IPlatform.Board BOARD = {
37 id: "0",
38 boardName: "stellaris",
39 boardFamily: null,
40 boardRevision: null
41 };
42
43 /*!
44 * ======== nameFormat ========
45 * Encoding of instance creation parameters in the instance's name
46 *
47 * For this platform, the parameters `deviceName` and `includeLinkCmdFile`
48 * can be encoded in the instance name supplied on `xdc.tools.configuro`
49 * command line, for example:
50 * @p(code) 51 * xs xdc.tools.configuro ... -p ti.platforms.stellaris:LM3S8971:1
52 * @p 53 * Optional parameters can be omitted:
54 * @p(code) 55 * xs xdc.tools.configuro ... -p ti.platforms.stellaris:LM3S8971
56 * @p 57 */
58 readonlyconfig string nameFormat = "$(deviceName):$(includeLinkCmdFile)";
59
60 instance:
61
62 /*
63 * This platform supports either M3 or M4. M3 or M4 is selected
64 * in Platform.xs based on target.isa.
65 */
66 config xdc.platform.IExeContext.Cpu M3 = {
67 id: "0",
68 clockRate: 1.0,
69 catalogName: "ti.catalog.arm.cortexm3",
70 deviceName: "Stellaris",
71 revision: "",
72 };
73
74 config xdc.platform.IExeContext.Cpu M4 = {
75 id: "0",
76 clockRate: 1.0,
77 catalogName: "ti.catalog.arm.cortexm4",
78 deviceName: "Stellaris",
79 revision: "",
80 };
81
82 /*!
83 * ======== deviceName ========
84 * The name of an `ICpuDataSheet` module for the device
85 *
86 * This parameter is required, but it does not have to be set explicitly;
87 * it can be encoded in the instance's name.
88 */
89 config string deviceName;
90
91 /*!
92 * ======== clockRate ========
93 * The clock rate for this device.
94 */
95 config Double clockRate = 20;
96
97 overrideconfig string codeMemory = null;
98
99 overrideconfig string dataMemory = null;
100
101 overrideconfig string stackMemory = null;
102
103 /*!
104 * ======== includeLinkCmdFile ========
105 * The flag that specifies if the platform should include a linker command
106 * file.
107 *
108 * By default, a user is responsible for adding a linker command file to
109 * the project, or to the linker command line. However, if this flag is
110 * set, this platform will include a default linker command file for the
111 * selected device.
112 */
113 config Bool includeLinkCmdFile = false;
114 };
115 /*
116 * @(#) ti.platforms.stellaris; 1, 0, 0,57; 8-17-2012 22:18:11; /db/ztree/library/trees/platform/platform-n27x/src/
117 */
118