Grace support for the MSP430
This package provides the top-level runtime interface to the code
generated by Grace. At this time, the only function externally callable
by applications is
Grace_init(). To
use this function you must include the header file that declares its
prototype. For example,
[
more ... ]
package ti.mcu.msp430 [1, 0, 0] {
}
DETAILS
This package provides the top-level runtime interface to the code
generated by Grace. At this time, the only function externally callable
by applications is Grace_init(). To
use this function you must include the header file that declares its
prototype. For example,
#include <ti/mcu/msp430/Grace.h>
:
int main(void)
{
Grace_init(); // initialize device peripherals
: // do something interesting ...
return (0); // return status to C runtime
}
SYNOPSYS
#include <ti/mcu/msp430/Grace.h>
void Grace_init(void)
DESCRIPTION
The function Grace_init() initializes the peripherals of your device
according to the settings specified by your application's .cfg file.
This file can be created "by hand" but is more typically created using
the Grace graphical configuration tool.
Grace_init() assumes that, prior to execution, peripherals are in their
power-on-reset state. This allows it to to avoid spending unnecessary
time and code space setting registers to default values already
established by the hardware during reset. However, this also means that
Grace_init() can not be used to "soft reset" peripherals during
runtime.
SEE ALSO
generated on Tue, 16 Oct 2012 23:16:09 GMT