1 /*
2 * Copyright (c) 2009 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*
13 * ======== Win32.xdc ========
14 */
15
16 /*!
17 * ======== Win32 ========
18 * Microsoft Windows 32-bit target using the Visual C/C++ compiler
19 *
20 * This target can be configured to be used with different versions of
21 * Microsoft Visual C/C++ and different installations of Platform SDK (or a
22 * newer equivalent Windows SDK). The optional Platform SDK is needed only
23 * for building applications that use Windows API.
24 * The target `Win32` contains default configurations for Visual C/C++
25 * versions 6.0, 7.0 and 8.0, but in order to support future versions of
26 * Visual C/C++ and different Platform SDK installations, there
27 * is a parameter {@link #vcPath}, which users can set in their `config.bld`
28 * files to enable usage of this target with their installations.
29 *
30 * Unlike the Visual C/C++ 6.x tool chain, this compiler complies very
31 * closely with the C/C++ language specification. This target may be
32 * necessary in situations that take full advantage of the C++ language.
33 */
34 metaonlymodule Win32 inherits microsoft.targets.ITarget {
35
36 overridereadonlyconfig string name = "Win32";
37 overridereadonlyconfig string os = "Windows";
38 overridereadonlyconfig string suffix = "86W";
39 overridereadonlyconfig string isa = "x86";
40 overridereadonlyconfig xdc.bld.ITarget.Model model = {
41 endian: "little"
42 };
43
44 overridereadonlyconfig string rts = "microsoft.targets.rts";
45
46 overrideconfig string platform = "host.platforms.PC";
47 overrideconfig string execExt = ".exe";
48
49 /*!
50 * ======== VCPath ========
51 *
52 * Object that defines various paths in a particular Visual Studio
53 * installation.
54 *
55 * Different Visual Studio installations keep the actual compiler and
56 * additional required DLLs in separate directories. Also, a Platform SDK
57 * installation is needed for building programs that use Windows API.
58 *
59 * @field(compilerDir) Relative path from this target's rootDir to the
60 * directory that contains the compiler.
61 *
62 * @field(dllPath) Relative path from this target's rootDir to the
63 * directory that contains mspdb.dll, mspdbcore.dll, etc.
64 *
65 * @field(sdkPath) Relative path from this target's rootDir to a
66 * Platform SDK installation or an absolute path to a Platform SDK
67 * installation. Platform SDK is required if the target is used to
68 * build executables that use Windows API.
69 *
70 * @field(libs) List of libraries to be added to the linker command line.
71 * If Platform SDK is used, the list should contain required
72 * libraries from sdkPath/lib. Otherwise, only the libraries from
73 * compilerDir/lib can be added to 'libs'.
74 */
75 struct VCPath {
76 string compilerDir;
77 string dllPath;
78 string sdkPath;
79 string libs;
80 };
81
82 /*!
83 * ======== vcPath ========
84 * Location of the compiler, additional DLLs, and Platform SDK
85 * installation
86 *
87 * This parameter is a map that contains information about paths to DLLs
88 * needed for building applications, and paths to the optional Platform
89 * SDK. Keys in the map are user-selected aliases for different Visual
90 * C/C++ releases. The values are {@link #VCPath} objects.
91 * This parameter can be set only in `config.bld`, together with
92 * `rootDir`. If `vcPath` is not set in `rootDir`, the default values
93 * specified below are used. After a user sets this target's `rootDir`,
94 * XDCtools search through the
95 * values in `vcPath`, looking for a field `compilerDir` whose content
96 * matches a name of a subdirectory in `rootDir`. Once a match is found,
97 * the content of that element of the map is used to find a path to
98 * required DLLs, a path to Platform SDK and a list of libraries.
99 *
100 * @a(Examples) 101 * If the content of `vcPath`, set in `config.bld` is
102 * @p(code) 103 * Win32.vcPath = [
104 * ["Visual Studio 7",
105 * {
106 * compilerDir: "Vc7",
107 * dllPath: "Common7/IDE;VisualStudio.NETProfessional-English",
108 * sdkPath: "C:/PlatformSDK",
109 * libs: " msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib mfc70.lib msvcirt.lib"
110 * }
111 * ],
112 * ["Visual Studio C++ 2005",
113 * {
114 * compilerDir: "VC",
115 * dllPath: "Common7/IDE",
116 * sdkPath: "VC/PlatformSDK",
117 * libs: " msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib"
118 * }
119 * ]
120 * ];
121 * @p 122 * and the `rootDir` for the target `Win32` is set to
123 * `"C:/Program Files/Microsoft Visual Studio 8"`, XDCtools will first
124 * check if there is a directory `"Vc7"` under `rootDir`. If the directory
125 * is not found, the next element in the map and its `compilerDir` field
126 * are queried. In this case, the next element's `compilerDir` is `"VC"`.
127 * If that directory is found under `rootDir`, the other fields in that
128 * element are used as follows: `compilerDir` and `dllPath` are added to
129 * the environment variable `PATH`. The contents of `sdkPath` and `libs`
130 * are added to appropriate command lines.
131 *
132 * If none of the elements in the map has `compilerDir` that corresponds
133 * to a subdirectory in `rootDir`, the configuration fails.
134 *
135 * Once a user sets up `vcPath` with all available installations of
136 * Visual Studio, simply by switching `rootDir` for this target, the
137 * right component of `vcPath` will be selected.
138 *
139 * The default version of this parameter contains settings for several
140 * Visual Studio releases. Therefore, a user does not have to completely
141 * redefine `vcPath`. Only the fields that corresponds to settings that
142 * differ between user's configuration and the default configuration
143 * need to be changes. For example, if the only difference between the
144 * default configuration and a user's environment is that the user
145 * installed Platform SDK to be used with Visual C/C++ 8 in a different
146 * directory, only that field needs to be changed.
147 * @p(code) 148 * var Win32 = xdc.module('microsoft.targets.Win32');
149 * Win32.vcPath["VC8"].sdkPath = "C:/WindowsSDK";
150 * @p 151 *
152 * If Platform SDK is not installed, sdkPath should be empty and the
153 * libraries from Platform SDK should be removed from 'libs':
154 * @p(code) 155 * var Win32 = xdc.module('microsoft.targets.Win32');
156 * Win32.vcPath = [
157 * ["VC8",
158 * {
159 * compilerDir: "VC",
160 * dllPath: "Common7/IDE",
161 * sdkPath: "",
162 * libs: " msvcrt.lib setargv.obj oldnames.lib"
163 * }
164 * ],
165 * ];
166 * @p 167 *
168 */
169 config VCPath vcPath[string] = [
170 ["VC6", {compilerDir: "vc98", dllPath: "common/msdev98/bin",
171 sdkPath: "",
172 libs: " msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib mfc42.lib msvcirt.lib"}],
173 ["VC7", {compilerDir: "Vc7",
174 dllPath: "Common7/IDE;VisualStudio.NETProfessional-English",
175 sdkPath: "Vc7/PlatformSDK",
176 libs: " msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib mfc70.lib msvcirt.lib"}],
177 /* Free version of VC8.0 doesn't include mfc libraries. */
178 ["VC8", {compilerDir: "VC", dllPath: "Common7/IDE",
179 sdkPath: "VC/PlatformSDK",
180 libs: " msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib"}],
181 ];
182
183 /*!
184 * ======== profiles ========
185 * Standard options profiles are overwritten because we can't use 'MTs'
186 * and -D_DEBUG=1. Both of them added the debug version of the C runtime
187 * library to the manifest.
188 */
189 overrideconfig xdc.bld.ITarget.OptionSet profiles[string] = [
190 ["debug", {
191 compileOpts: {
192 copts: "-Z7 -Odi -MT",
193 defs: "",
194 },
195 linkOpts: "-debug ",
196 }],
197
198 ["release", {
199 compileOpts: {
200 copts: "-O2 -MT",
201 defs: "",
202 },
203 linkOpts: "",
204 }],
205 ];
206
207 /*!
208 * ======== ar ========
209 * The archiver command and all required options
210 * @p(dlist) 211 * -`-nologo`
212 * don't display archiver copyright
213 */
214 overridereadonlyconfig xdc.bld.ITarget2.Command ar = {
215 cmd: "$(rootDir)/$(compilerDir)/bin/lib.exe -nologo",
216 opts: ""
217 };
218
219 /*!
220 * ======== cc ========
221 * The compile command and all required options
222 * @p(dlist) 223 * -`-W3`
224 * enable all warnings recommended for production purposes.
225 * -`-c`
226 * don't link
227 * -`-nologo`
228 * don't display compiler copyright
229 * -`-Zp1`
230 * Packs structure members on 1-byte boundry
231 */
232 overridereadonlyconfig xdc.bld.ITarget2.Command cc = {
233 cmd: "$(rootDir)/$(compilerDir)/bin/cl.exe -nologo -c",
234 opts: '-Zp1 -W3 -DWIN32 -D_DLL -D_AFXDLL -DEXPORT=""'
235 };
236
237 /*!
238 * ======== asm ========
239 * The assemble command and all required options
240 * @p(dlist) 241 * -`-c`
242 * don't link
243 * -`-nologo`
244 * don't display macro assembler copyright
245 */
246 overridereadonlyconfig xdc.bld.ITarget2.Command asm = {
247 cmd: "$(rootDir)/$(compilerDir)/bin/ml -c",
248 opts: "-nologo"
249 };
250
251 /*!
252 * ======== lnk ========
253 * The linker command and all required options
254 * @p(dlist) 255 * -`-nologo`
256 * Don't display linker copyright
257 */
258 overridereadonlyconfig xdc.bld.ITarget2.Command lnk = {
259 cmd: "$(rootDir)/$(compilerDir)/bin/link",
260 opts: "-nologo"
261 };
262
263 /*!
264 * ======== ccOpts ========
265 * User modifiable default options.
266 * @p(dlist) 267 * -`-G5` (removed because it is incompatible with VC8.0)
268 * Optimizes code to favor the Pentium processor
269 * -`-Ob1`
270 * Expand only functions marked as inline or, in a C++
271 * member function, defined within a class declaration
272 * -`-Gs`
273 * Probe stack to automatically grow stack as necessary
274 * -`-GX` (removed because it is incompatible with VC8.0)
275 * Enables synchronous exception handling
276 * -`-WL`
277 * Write errors/warnings on a single output line
278 */
279 overrideconfig xdc.bld.ITarget2.Options ccOpts = {
280 prefix: "-Ob1 -Gs",
281 suffix: "-Dfar= "
282 };
283
284 /*!
285 * ======== lnkOpts ========
286 * User modifiable linker options
287 * @p(dlist) 288 * -`-libpath`...
289 * directories to search for toolchain specific libraries
290 * -`-nodefaultlib`
291 * don't search for default libraries when linking; all
292 * libraries used must be explicitly named
293 * -`-incremental:no`
294 * link for execution (no subsequent link will occur)
295 * -`-machine:ix86`
296 * link for the Intel x86 architecture
297 * -`-map:$(XDCCFGDIR)/$@.map`
298 * output any link map information to the specified file
299 * ($(XDCCFGDIR) is usually package/cfg)
300 * -`-pdb:$(XDCCFGDIR)/$@.pdb`
301 * output any program debug information to the specified file
302 * ($(XDCCFGDIR) is usually package/cfg)
303 */
304 overrideconfig xdc.bld.ITarget2.Options lnkOpts = {
305 prefix: "-libpath:$(rootDir)/$(compilerDir)/lib -libpath:$(rootDir)/$(compilerDir)/atlmfc/lib -libpath:$(rootDir)/$(compilerDir)/mfc/lib -libpath:$(sdkPath)/lib",
306 suffix: "-map:$(XDCCFGDIR)/$@.map -pdb:$(XDCCFGDIR)/$@.pdb -machine:ix86 -nodefaultlib -incremental:no"
307 };
308
309 /*!
310 * ======== includeOpts ========
311 * User modifiable include paths
312 * @p(dlist) 313 * -`-I$(rootDir)/$(compilerDir)/include`
314 * include compiler specific headers
315 */
316 overrideconfig string includeOpts = "-I$(rootDir)/$(compilerDir)/include -I$(rootDir)/$(compilerDir)/atlmfc/include -I$(rootDir)/$(compilerDir)/mfc/include -I$(rootDir)/$(compilerDir)/atl/include -I$(sdkPath)/include";
317 }
318 /*
319 * @(#) microsoft.targets; 1, 0, 2, 0,605; 10-8-2012 14:17:05; /db/ztree/library/trees/xdctargets/xdctargets-f38x/src/ xlibrary
320 321 */
322