1    /* 
     2     *Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     *
    11     * */
    12    /*!
    13     *  ======== Main ========
    14     *  Graphical interface to path tool
    15     *
    16     *  This graphical interactive tool displays the packages located along any
    17     *  specified package repository path.
    18     *
    19     *  At startup, this tool shows the packages located along the current package
    20     *  path; i.e.,
    21     *  @p(code)
    22     *      $XDCPATH;$XDCROOT/packages;^
    23     *  @p
    24     *
    25     *  where `$XDCPATH` is the value of the the user settable prefix of the
    26     *  package path, `$XDCROOT` is the installation directory of the XDC tools,
    27     *  and `^` is the repository of the package in the current working directory
    28     *  (if it exists). To specify a package path other than the current package
    29     *  path, use the --packagepath option. Only semicolon delimited canonical 
    30     *  paths should be specifed as arguments with the --packagepath option.
    31     *  Environment variables such as $XDCROOT and special designators such as
    32     *  '^' should not be used.
    33     * 
    34     *  @b(Usage)
    35     *  @p(code)
    36     *    xs xdc.tools.path.sg [--packagepath PATH]
    37     *  @p
    38     *
    39     *  @a(Bugs)
    40     *  
    41     *  This tool scans all packages available along the current
    42     *  package path before displaying the user interface.  So, a repository in
    43     *  the package path that contains a large number of sub-directories, such
    44     *  as '/', causes very long delays before the user interface is displayed.
    45     *
    46     *  While it is easy to see that you should not put '/' in the package path,
    47     *  it is less obvious that installing a package at '/' has the same effect.
    48     */
    49    metaonly module Main inherits xdc.tools.ICmd {
    50    
    51        override config String usage[] = [
    52           '[--packagepath PATH]'
    53        ];
    54    
    55        /*!
    56         *  ======== createPartControl ========
    57         *  @_nodoc
    58         */
    59        function createPartControl(parent);
    60    
    61    instance:
    62    
    63        //! package path to scan for packages
    64        @CommandOption('packagepath')
    65        config string pathArg = null;
    66    
    67    }
    68    /*
    69     *  @(#) xdc.tools.path.sg; 1, 0, 0,222; 8-27-2012 11:52:39; /db/ztree/library/trees/xdctools/xdctools-f15x/src/
    70     */
    71