package xdc.platform |
![](../../Arrow_right.png) |
Interfaces and modules necessary for the XDC Platform Model
package xdc.platform [1, 0, 1, 0] {
// CPU information provided by the HW model
// Execution environment interface between a platform and an executable
// Configuration-time representation of a peripheral
// Configuration-time interface to all platforms
// Stock implementation of xdc.platform.IExeContext
// Misc platform utilities
}
CUSTOM MEMORY CHECK
If a custom memory map is specified for a platform, through the
configuration parameter
xdc.platform.IPlatform.customMemoryMap,
the custom map is checked
against the default memory map to verify if the custom map fits within
the default map. The environment variable
xdc.platform.custom.check
controls this check.
By default, the check is enabled. It can be disabled by passing
-Dxdc.platform.custom.check="false" to the XDCscript shell (
xs),
which is used to run the
configuro command
line configuration tool.
If, on the other hand, you are using
xdc to run the configuration step
you can set this variable by setting the
xsopts attribute of an
xdc.bld.Executable within a build script.
generated on Thu, 27 Sep 2012 23:21:11 GMT