package xdc.rta.tools.file |
Tool for reading and decoding RTA data from a file
XDCspec declarations | sourced in xdc/rta/tools/file/package.xdc |
You may use this tool to simply print the decoded records, or you may have them redirected to a file to be processed elsewhere.
Without this flag, the tool will simply print all of the records in the data file to the screen. If this flag is set, then the tool will wait the user to press enter in between displaying each packet.
The tool will write the decoded records out as text to the specified out file. The record properties will be separated with a delimeter character so that they can be imported into a spreadsheet such as Excel.
Delimiter character to use when writing out the file.
The character specified here will be inserted between each of the record fields so that the file can be imported into a spreadsheet such as excel.