1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== IPlatform.xdc ========
    14     */
    15    
    16    package xdc.platform;
    17    
    18    /*!
    19     *  ======== IPlatform ========
    20     *  Configuration-time interface to all platforms.
    21     *
    22     *  This interface defines the elements that must be implemented by all
    23     *  "platform packages".  All programs are built to execute on a platform
    24     *  and each program includes exactly one platform package (which defines
    25     *  the platform).
    26     *
    27     *  Platform packages contain exactly one module named "Platform" which
    28     *  implements the `xdc.platform.IPlatform` interface defined here.
    29     *
    30     *  Program configuration scripts may read (but not modify) the attributes
    31     *  provided by this interface from the global `Program` object; see
    32     *  `{@link xdc.cfg.Program#platform}`.
    33     */
    34    metaonly interface IPlatform
    35    {
    36        /*!
    37         *  ======== Board ========
    38         *  Board-level description.
    39         */
    40        struct Board {
    41            string   id;            /*! unique id within the platform */
    42            string   boardName;     /*! name of the board */
    43            string   boardFamily;   /*! optional family name */
    44            string   boardRevision; /*! optional revision string */
    45        };
    46    
    47        /*!
    48         *  ======== Memory ========
    49         *  A named contiguous range of addresses.
    50         *
    51         *  Memory structures are used in the description of the memory available
    52         *  from CPUs and platforms.
    53         */
    54        struct Memory {
    55            string      comment;    /*! description of this block */
    56            string      name;       /*! name of memory segment */
    57            string      space;      /*! "code", "data", "code/data", etc.... */
    58            unsigned    page;       /*! page of memory segment */
    59            unsigned    base;       /*! base address of memory segment */
    60            unsigned    len;        /*! length of memory segment */
    61            string      access;     /*! attributes of memory: "RWX" */
    62        };
    63    
    64        /*! Type to be used for maps of Memory objects */
    65        typedef Memory MemoryMap[string];
    66    
    67    instance:
    68        /*!
    69         *  ======== create ========
    70         *  Constructor for IPlatform instances.
    71         *
    72         *  @param(name)    the name of the platform instance being created
    73         *
    74         *                  This name is the suffix of the platform
    75         *                  specification supplied in the build script after
    76         *                  the platform name (and optional ':') prefix has
    77         *                  been removed.  So the platform instance name
    78         *                  "joes.platform.foo:bar" results in the name "bar"
    79         *                  and the name "joes.platform.foo" result in the name
    80         *                  "".
    81         *
    82         *  @param(args)    deprecated parameter that should not be used in
    83         *                  a platform instance implementation
    84         *
    85         */
    86        create(string name, any args);
    87        
    88        /*
    89         *  ======== memTab ========
    90         *  A mapping of memory names to external memory objects.
    91         *
    92         *  This hash table is used to map linker memory region names ("EPROG",
    93         *  "EDATA", etc.) to `{@link xdc.platform.IPlatform#Memory}` objects.
    94         *  During generation of linker command files, for example, this table
    95         *  may be used to genenerate physical memory map declarations.
    96         *
    97         *  Platforms with a fixed memory map can initialize this table
    98         *  "statically" in Platform.xdc using the following syntax:
    99         *  @p(code)
   100         *      override config xdc.platform.IPlatform.Memory memTab[string] = [
   101         *          ["PMEM", {name: "PMEM", base: 0x00000200, len: 0x0000FE00}],
   102         *              :
   103         *      ];
   104         *  @p
   105         *  Alternatively, platforms can initialize this table dynamically in
   106         *  the platform package's `init()` function (see `{@link xdc.IPackage}`)
   107         *  using the following syntax:
   108         *  @p(code)
   109         *    function init()
   110         *    {
   111         *              :
   112         *        this.memTab["PMEM"] = {name: "PMEM", base: 0x200, len: 0xFE00};
   113         *              :
   114         *    }
   115         *  @p
   116         *  @a(readonly)   this parameter is set by the platform and read by
   117         *              program configuration scripts.
   118         */
   119    //    config Memory memTab[string];     /* memory name => memory object */
   120    
   121        /*!
   122         *  ======== externalMemoryMap ========
   123         *  A mapping of memory names to memory objects for external memory.
   124         *
   125         *  This parameter defines the external portion of the platform's memory
   126         *  map.
   127         */
   128        readonly config xdc.platform.IPlatform.Memory externalMemoryMap[string];
   129    
   130        /*!
   131         *  ======== customMemoryMap ========
   132         *  A custom mapping of memory names to memory objects.
   133         *
   134         *  This parameter allows platform instances to completely overwrite a 
   135         *  default memory map based on the internal memory map coming from CPU's
   136         *  memory map and externalMemoryMap.
   137         *
   138         *  Custom memory map must fit within the default memory map, unless the
   139         *  verification of the fit is disabled (see `{@link xdc.platform}`). 
   140         */
   141        config xdc.platform.IPlatform.Memory customMemoryMap[string];
   142    
   143        /*!
   144         *  ======== renameMap ========
   145         *  A map for renaming memory objects.
   146         *
   147         *  This map renames memory objects. If you do not want to change
   148         *  addresses in the default memory map, but you only want to rename the
   149         *  existing memory objects, you should use this parameter.
   150         *
   151         *  This map and `customMemoryMap` should not be used together because this
   152         *  map renames the default memory, but then `customMemoryMap` replaces the
   153         *  default memory objects. The parameters `codeMemory`, `dataMemory` and
   154         *  `stackMemory` are not automatically reassigned to new names. It is the
   155         *  user's responsibility to set those parameters accordingly to 
   156         *  `renameMap`.
   157         */
   158        config string renameMap[string];
   159    
   160        /*!
   161         *  ======== dataMemory ========
   162         *  The default segment for data sections.
   163         *
   164         *  Each target has a section map with keys equal to the names of all
   165         *  sections that compiler and assembler for that target generate. The
   166         *  value for each key is either "code" or "data" or "stack". A linker
   167         *  template reads that map and puts all "data" sections in the segment
   168         *  defined by this configuration parameter.
   169         *
   170         *  @see #codeMemory
   171         *  @see #stackMemory
   172         */
   173        config string dataMemory;
   174    
   175        /*!
   176         *  ======== codeMemory ========
   177         *  The default segment for code sections.
   178         *
   179         *  Each target has a section map with keys equal to the names of all
   180         *  sections that compiler and assembler for that target generate. The
   181         *  value for each key is either "code" or "data" or "stack". A linker
   182         *  template reads that map and puts all "code" sections in the segment
   183         *  defined by this configuration parameter.
   184         *
   185         *  @see #dataMemory
   186         *  @see #stackMemory
   187         */
   188        config string codeMemory;
   189    
   190        /*!
   191         *  ======== stackMemory ========
   192         *  The default segment for stack.
   193         *
   194         *  Each target has a section map with keys equal to the names of all
   195         *  sections that compiler and assembler for that target generate. The
   196         *  value for each key is either "code" or "data" or "stack". A linker
   197         *  template reads that map and puts all "stack" sections in the segment
   198         *  defined by this configuration parameter.
   199         *
   200         *  @see #dataMemory
   201         *  @see #codeMemory
   202         */
   203        config string stackMemory;
   204    
   205        /*!
   206         *  ======== sectMap ========
   207         *  A mapping of linker output section names to memory segments.
   208         *
   209         *  During the generation of linker command files, the templates used to
   210         *  create these files examine several sources of information to determine 
   211         *  the placement of named output sections into memory segments defined
   212         *  by the platform.  The default placement, described below,
   213         *  uses information from the target and this platform's
   214         *  `{@link #codeMemory}`, `{@link #dataMemory}`, and
   215         *  `{@link #stackMemory}` configuration parameters.
   216         *
   217         *  `sectMap` is used to override this default placement of
   218         *  output sections (".text", ".cinit", etc.) to a memory 
   219         *  segment defined by the platform's memory map.  For example, even if
   220         *  a platform's `codeMemory` parameter is defined to be "SRAM" and
   221         *  ".cinit" output sections are "code" sections, if the platform also
   222         *  defines the following `sectMap`, the section ".cinit" will be placed
   223         *  into a memory segment named "DDR2".
   224         *  @p(code)
   225         *      sectMap[] = [
   226         *          [".cinit", "DDR2"],
   227         *      ];
   228         *  @p
   229         *
   230         *  @a(Note) If an output section has an entry in
   231         *  `{@link xdc.cfg.Program#sectMap Program.sectMap}`, that entry
   232         *  overrides the placement specified by this `sectMap`.  A program's
   233         *  `sectMap` configuration always overrides the platform's `sectMap`
   234         *  settings.
   235         *
   236         *  @a(Default Mapping)
   237         *  The default placement of a target's output sections into memory
   238         *  segments defined by the platform is determined by the following
   239         *  configuration parameters:
   240         *  @p(blist)
   241         *      - `{@link xdc.bld.ITarget#sectMap ITarget.sectMap}`
   242         *          used to map a named output section to either "code", "data",
   243         *          or "stack"
   244         *      - `{@link #codeMemory}`
   245         *          names a memory segment that will contain all "code"
   246         *          output sections
   247         *      - `{@link #dataMemory}`
   248         *          names a memory segment that will contain all "data"
   249         *          output sections
   250         *      - `{@link #stackMemory}`
   251         *          names a memory segment that will contain all "stack"
   252         *          output sections
   253         *  @p
   254         *
   255         *  @see xdc.cfg.Program#sectMap
   256         *  @see xdc.bld.ITarget#sectMap
   257         */
   258        config string sectMap[string]; /* section name => memory segment */
   259        
   260        /*!
   261         *  ======== peripherals ========
   262         *  @_nodoc
   263         *
   264         *  A map of peripherals available on a platform instance
   265         *
   266         *  The map contains peripherals from an 
   267         *  `{@link xdc.platform.ICpuDataSheet}` instance available as
   268         *  `{@link xdc.cfg.Program#cpu.attrs}`, and peripherals defined in this
   269         *  platform instance. The map is initialized by the platform instance,
   270         *  and in multicore platforms the instance must add only peripherals
   271         *  available to the CPU for which an executable is being built.
   272         */
   273        //config IPeripheral.Instance peripherals[string];
   274        
   275        /*!
   276         *  ======== getCpuDataSheet ========
   277         *  Get the Cpu data sheet object corresponding to specified cpu id.
   278         *
   279         *  This function executes in either the Configuration object model
   280         *  or the Build object model.
   281         *
   282         *  @param(cpuId)   a string that corresponds to the platform-specific id
   283         *                  of a CPU on this platform that runs executables.
   284         *
   285         *  @a(returns)     Returns an `{@link xdc.platform.ICpuDataSheet}`
   286         *                  instance object that corresponds to the specified
   287         *                  cpuId.
   288         *
   289         *  @a(throws)      `Error` exceptions are thrown for fatal errors.
   290         */
   291        function getCpuDataSheet(cpuId);
   292    //    xdc.platform.ICpuDataSheet.Instance getCpuDataSheet(string cpuId);
   293    
   294        /*!
   295         *  ======== getCreateArgs ========
   296         *  DEPRECATED
   297         *  @_nodoc
   298         *
   299         *  Get the value of the args parameter used to create this instance
   300         *
   301         *  This function executes in either the Configuration object model
   302         *  or the Build object model.
   303         *
   304         *  @a(returns)     Returns the "args" object that passed to this
   305         *                  module's create method when the instance was created.
   306         *
   307         *  @a(throws)      `Error` exceptions are thrown for fatal errors.
   308         */
   309        function getCreateArgs();
   310    // any getCreateArgs();
   311        
   312        /*!
   313         *  ======== getExeContext ========
   314         *  Get execution context object corresponding to the specified program.
   315         *
   316         *  This is called before the program's configuration script runs to 
   317         *  get the Cpu object that is assigned to the program's cpu field.
   318         *
   319         *  Note: that the build script for the program is responsible for
   320         *  specifying the CPU; this is done by either implicitly naming the
   321         *  platform or explicitly naming a particular CPU on the platform
   322         *  (see `{@link xdc.bld.Executable#Attrs.cpuId}`).
   323         *
   324         *  This function executes in the Configuration object model.
   325         *
   326         *  @param(prog)    the `{@link xdc.cfg.Program}` object representing the
   327         *                  program being configured.
   328         *
   329         *                  This object contains the following properties that
   330         *                  allows the platform to determine the appropriate Cpu
   331         *                  object to return (if there is more than one):
   332         *                      `prog.build.cpuId`,
   333         *                      `prog.build.cpuArgs`, 
   334         *                      `prog.build.target`,
   335         *
   336         *  @a(returns)     Returns an `{@link xdc.platform.IExeContext}` instance
   337         *                  object that corresponds to the CPU that will run the
   338         *                  specified program.
   339         *
   340         *  @a(throws)      `Error` exceptions are thrown for fatal errors.
   341         */
   342        function getExeContext(prog);
   343    //    xdc.platform.IExeContext.Instance getExeContext(xdc.cfg.Program.Module prog);
   344    
   345        /*!
   346         *  ======== getExecCmd ========
   347         *  Get the exec command used to run the program on this platform.  
   348         *
   349         *  This function is called after the program's configuration script runs
   350         *  and returns commands that are used to load and run the specified
   351         *  program.  These commands are placed in a makefile that is included
   352         *  by the client package's generated makefile.  Thus, the commands may
   353         *  refer to macros defined in this environment; e.g., `$(SHELL)` and
   354         *  `$(XDCROOT)`, etc.
   355         *
   356         *  The special macro `$(1)` expands to test-specific arguments
   357         *  (`{@link xdc.bld.Test#attrs.execArgs}`) that are passed from the test
   358         *  to the platform's exec command.  Thus, all platforms that support
   359         *  arguments to their exec command, should embed "`$(1)`" within the
   360         *  command string at the appropriate place to have these arguments
   361         *  interpreted by the exec command.
   362         *
   363         *  For example, a platform that uses a shell script to run executables
   364         *  and allows options to be passed to the shell script might return
   365         *  the following string:
   366         *  @p(code)
   367         *      "$(SHELL) <exec_path> $(1) <exe_name>"
   368         *  @p
   369         *  where, `<exec_path>` is the absolute path to the platform's exec
   370         *  shell script, and `<prog_name>` is the name of the executable relative
   371         *  to the package's base directory (i.e., `{@link xdc.cfg.Program#name}`).
   372         *
   373         *  This function executes in the Configuration object model.
   374         *
   375         *  @param(prog)    the `{@link xdc.cfg.Program}` object representing the
   376         *                  program being configured.
   377         *
   378         *                  This object contains the following properties that
   379         *                  allows the platform to determine the appropriate Cpu
   380         *                  object to return (if there is more than one):
   381         *                      `prog.build.cpuId`,
   382         *                      `prog.build.cpuArgs`,
   383         *                      `prog.build.target`
   384         *
   385         *  @param(platPath) full path to the platform package for the program
   386         *
   387         *  @a(returns)     Returns a string of commands used to execute this
   388         *                  program in the context of the XDC generated makefiles.
   389         *                  
   390         *  @a(throws)      `Error` exceptions are thrown for fatal errors.
   391         */
   392        function getExecCmd(prog, platPath);
   393    //    string  getExecCmd(xdc.cfg.Program.Module prog, string platPath);
   394    
   395        /*!
   396         *  ======== getLinkTemplate ========
   397         *  Get Linker Command file template used to link an executable.
   398         *
   399         *  In the event that no template is provided by the program
   400         *  configuration script (see `{@link xdc.cfg.Program#linkTemplate}`), 
   401         *  the template file identified by this method is used to generate the
   402         *  linker command file used to create the executable.
   403         *
   404         *  This function executes in the Configuration object model and
   405         *  is called after the program configuration script runs.  The template
   406         *  is expanded in the context of the Configuration Object Model.  
   407         *
   408         *  @param(prog)    the `{@link xdc.cfg.Program}` object representing the
   409         *                  program being configured.
   410         *
   411         *                  This object contains the following properties that
   412         *                  allows the platform to determine the appropriate link
   413         *                  template to return:
   414         *                  @p(blist)
   415         *                      - `prog.build.cpuId`,
   416         *                      - `prog.build.cpuArgs`,
   417         *                      - `prog.build.target`
   418         *                  @p
   419         *  @a(returns)     Returns a path string to a template file or `null`.  If
   420         *                  `null`, no linker command file is generated; otherwise
   421         *                  this path is relative to the package path.
   422         *                  
   423         *  @a(throws)      `Error` exceptions are thrown for fatal errors.
   424         */
   425        function getLinkTemplate(prog);
   426    //    string getLinkTemplate(prog);
   427    }
   428    /*
   429     *  @(#) xdc.platform; 1, 0, 1, 0,385; 9-3-2012 16:22:09; /db/ztree/library/trees/xdc/xdc-y35x/src/packages/
   430     */
   431