1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*!
    13     *  ======== xdc ========
    14     *  Core interfaces and modules necessary for the XDC runtime.
    15     *
    16     *  In addition to the interfaces specified below, this package also supplies
    17     *  a C/C++ header, `std.h` that facilitates the creation of portable sources.
    18     *  This header defines a set of "base" types that enable the creation
    19     *  of C-code that is portable between any two targets.  C source code that
    20     *  relies exclusively on these types is portable to all targets and
    21     *  platforms.  Where appropriate, the types defined below are related to the
    22     *  types defined in the library headers prescribed by the C99 standard
    23     *  (ISO/IEC 9899:1999).
    24     *
    25     *  Why not simply use the C99 types?  Having a
    26     *  unique set of names provides a layer of insulation between a portable code
    27     *  base and a particular compiler; e.g., even if a compiler does not support
    28     *  the C99 types or defines them inappropriately for a particular device, it
    29     *  is possible to use the compiler without changing the code base.  Thus, the
    30     *  developer is not forced to choose the lesser of two evils: waiting for a
    31     *  change to the compiler or forking the code base for a particular compiler
    32     *  device combination.
    33     *
    34     *  There are several situations where a small separate set of portable types
    35     *  can help the maintainability of a code base.
    36     *  @p(blist)
    37     *      - not all of the types described in the C99 standard are required to 
    38     *        be defined by conformant implementations nor is it possible for all
    39     *        devices to implement some of the types specified (e.g., `int8_t` is
    40     *        not implemented on C54 devices); so it is difficult to identify
    41     *        non-portable source code.
    42     *      - not all compilers provide C99 type support; if XDC supplies the type
    43     *        definition and the compiler is updated to include C99 types, a
    44     *        compilation error will occur if the source includes the C99
    45     *        headers.
    46     *      - not all compiler and device combinations are conformant; even high
    47     *        quality compilers may not properly define the types for each device
    48     *        supported by compiler.
    49     *
    50     *  @a(Usage)
    51     *  @p(code)
    52     *      #include <xdc/std.h>
    53     *  @p
    54     *
    55     *  To compile sources that include `xdc/std.h`, two symbols must be defined
    56     *  before including this header:
    57     *  @p(dlist)
    58     *      - `xdc_target_types__`
    59     *          the package qualified path of the target's standard types header;
    60     *          e.g., `ti/targets/std.h`.  This value is specified in the target's
    61     *          `stdInclude` config parameter; see
    62     *          `{@link xdc.bld.ITarget#stdInclude}`
    63     *
    64     *      - `xdc_target_name__`
    65     *          the target's module name without the package prefix; e.g., `C64`
    66     *          rather than `ti.targets.C64`.
    67     *  @p
    68     *  For example, to compile sources for the `ti.targets.C64` target using TI's
    69     *  `cl6x` compiler, the following command line is sufficient:
    70     *  @p(code)
    71     *      cl6x -Dxdc_target_types__=ti/targets/std.h -Dxdc_target_name__=C64
    72     *  @p
    73     *
    74     *  Each of the type names below has an equivalent "long name"; i.e., a name
    75     *  that has an "`xdc_`" prefix.  For example, the type `Bool` can also be
    76     *  written as "`xdc_Bool`".  Long names exist to avoid conflicts with
    77     *  names defined or used by existing code bases.
    78     *
    79     *  In the event that one of the short type names below conflicts with another
    80     *  type name (that can not be changed), it is possble to disable the short
    81     *  names by defining the symbol `xdc__nolocalnames` before including
    82     *  `xdc/std.h`.
    83     *  @p(code)
    84     *      #define xdc__nolocalnames
    85     *      #include <xdc/std.h>
    86     *  @p
    87     *
    88     *  @a(Standard Types)
    89     *  This header may be included multiple times and defines the following
    90     *  target-dependent types:
    91     *  @p(dlist)
    92     *      - `Bool`
    93     *          this type is large enough to hold the values `0` or `1`.  The
    94     *          constants TRUE and FALSE are of this type; see below.
    95     *      - `String`
    96     *          this type is defined to be a `char *` and exists to allow code
    97     *          to distinguish between pointers to buffers of raw data and
    98     *          '\0' terminated strings.
    99     *      - `Int`n, where n = 8, 16, or 32
   100     *          signed integer type that is large enough to hold n bits; the
   101     *          actual target type may by be larger than n.  This type is
   102     *          equivalent to one of the C99 types `int_least`n`_t` or
   103     *          `int_fast`n`_t`; see  Section 7.18.
   104     *      - `UInt`n, where n = 8, 16, or 32
   105     *          unsigned integer type that is large enough to hold n bits; the
   106     *          actual target type may by be larger than n.  This type is
   107     *          equivalent to one of the C99 types `uint_least`n`_t` or
   108     *          `uint_fast`n`_t`; see ISO/IEC 9899:1999 Section 7.18.
   109     *      - `Bits`n, where n = 8, 16, or 32
   110     *          unsigned integer type that is precisely n bits. Not all targets
   111     *          support all values of n; if the target does not support an exact
   112     *          size the corresponding type is not defined.  This type is
   113     *          equivalent to the corresponding C99 type `uint`n`_t`; see ISO/IEC
   114     *          9899:1999 Section 7.18.
   115     *      - `Fxn`
   116     *          this type is a pointer to code; it can hold a pointer to any
   117     *          function.
   118     *      - `Ptr`
   119     *          this type is a pointer to data; it can hold a pointer to any
   120     *          data structure.
   121     *      - `IArg`
   122     *          this integer type is large enough to hold a `Fxn`, `Ptr`, or
   123     *          `Int`.
   124     *      - `UArg`
   125     *          this unsigned integer type is large enough to hold a `Fxn`,
   126     *          `Ptr`, or `Int`.
   127     *      - `LLong`
   128     *          this long integer type is large enough to hold a `Long` and is
   129     *          defined as a 'long long' type on targets that support this type;
   130     *          otherwise, it is simply a `Long`.
   131     *
   132     *          Note that C99 requires the `long long` type to be at least 64-bits
   133     *          wide (See ISO/IEC 9899:1999 Section 5.2.4.2.1).  But some
   134     *          compilers do not support 64-bit integral types and some don't
   135     *          support the `long long` even though they do support 64-bit
   136     *          integral types.  Since these variations limit the portability of
   137     *          valid C sources, the LLong type is always defined, is always at
   138     *          least as wide as the `Long` type, and is at least 64-bits wide for
   139     *          targets that support 64-bit integral types.
   140     *
   141     *      - `ULLong`
   142     *          this unsigned long integer type is large enough to hold a `ULong`
   143     *          and is defined as a 'unsigned long long' type on targets that
   144     *          support this type; otherwise, it is simply a `ULong`.
   145     *  @p
   146     *
   147     *  The `xdc/std.h` header also defines the following aliases for the base C
   148     *  types.  These aliases exist so that C sources can consistently follow
   149     *  a naming convention in which all type names are written in camel-case.
   150     *  @p(dlist)
   151     *      - `Char` and `UChar`
   152     *          aliases for `char` and `unsigned char`, respectively
   153     *      - `Short` and `UShort`
   154     *          aliases for `short` and `unsigned short`, respectively
   155     *      - `Int` and `UInt`
   156     *          aliases for `int` and `unsigned int`, respectively
   157     *      - `Long` and `ULong`
   158     *          aliases for `long` and `unsigned long`, respectively
   159     *      - `Double` and `LDouble`
   160     *          aliases for `double` and `long double`, respectively
   161     *      - `SizeT`
   162     *          alias for `size_t`
   163     *      - `VaList`
   164     *          alias for `va_list`
   165     *  @p
   166     *  The types above are defined for all targets.  Some targets can support
   167     *  the following additional types.  Since these types are not always
   168     *  supported by a target, these types should only be used when no other
   169     *  type sufficies.
   170     *  @p(dlist)
   171     *      - `Bits`n, where n = 8, 16, or 32
   172     *          this unsigned integer type is precisely n-bits wide.  This type is
   173     *          equivalent to the optional C99 type `uint`n`_t`; see ISO/IEC
   174     *          9899:1999 Section 7.18.1.1.  This type is defined if and
   175     *          only if the preprocessor macro `xdc__BITS`n`__` is defined.
   176     *  @p
   177     *  
   178     *  @a(64-Bit Types)
   179     *  Although the C99 standard requires support for 64-bit types, not all
   180     *  compiler/device combinations can usefully support them.  As a result,
   181     *  the 64-bit types described here may not be defined for all targets.  For
   182     *  each type there is a corresponding pre-processor macro which is
   183     *  defined if and only if the type is supported.
   184     *  @p(dlist)
   185     *      - `Int64`
   186     *          signed integer type that is large enough to hold 64 bits; the
   187     *          actual target type may by be wider than 64 bits.  This type is
   188     *          equivalent to one of the C99 types `int_least64_t` or
   189     *          `int_fast64_t`; see  Section 7.18.  This type is defined if and
   190     *          only if the preprocessor macro `xdc__INT64__` is defined.
   191     *      - `UInt64`
   192     *          unsigned integer type that is large enough to hold n bits; the
   193     *          actual target type may by be wider than 64 bits.  This type is
   194     *          equivalent to one of the C99 types `uint_least64_t` or
   195     *          `uint_fast64_t`; see ISO/IEC 9899:1999 Section 7.18.  This type
   196     *          is defined if and only if the preprocessor macro
   197     *          `xdc__INT64__` is defined.
   198     *      - `Bits64`
   199     *          unsigned integer type that is precisely 64 bits wide. If the target
   200     *          does not support an exact 64-bit size, this type is not defined.
   201     *          This type is equivalent to the corresponding C99 type
   202     *          `uint64_t`; see ISO/IEC 9899:1999 Section 7.18.  This type is
   203     *          defined if and only if the preprocessor macro `xdc__BITS64__` is
   204     *          defined.
   205     *  @p
   206     *
   207     *  @a(Predefined Macros)
   208     *  In addition to the type definitions above, `xdc/std.h` also defines the
   209     *  following commonly used constants
   210     *  @p(dlist)
   211     *      - `NULL`
   212     *          defined as `0`
   213     *      - `TRUE`
   214     *          defined as `((Bool)1)`
   215     *      - `FALSE`
   216     *          defined as `((Bool)0)`
   217     *  @p
   218     *
   219     *  Finally, `xdc/std.h` defines the following target-independent symbols
   220     *  that have target-dependent values; these predefined macros enable
   221     *  conditional compilation of source files based on target-specific
   222     *  attributes.  
   223     *  @p(dlist)
   224     *      - {c_target_name}
   225     *          this symbol (the target's fully qualified name with all '.'s
   226     *          replaced with '_') is always defined and allows one to easily
   227     *          include target-specific headers or define symbols with
   228     *          target-specific values.
   229     *
   230     *      - `xdc_target__isaCompatible_`{isa_name}
   231     *          for every ISA named in the array returned by this target's
   232     *          `{@link xdc.bld.ITarget#getISAChain()}` method, a symbol of this
   233     *          name is defined.  In addition to enabling one to create code
   234     *          specific to a particular ISA, this allows one to create code that
   235     *          depends on TI's C6x architecture without being dependent
   236     *          on a particular member of the C6x family, for example.
   237     *
   238     *      - `xdc_target__isa_`{isa}
   239     *          this symbol is always defined  and {isa} is the
   240     *          target's `isa` (see `{@link xdc.bld.ITarget#isa}`).
   241     *
   242     *      - `xdc_target__`{little,big}`Endian`
   243     *          if this target's `{@link xdc.bld.ITarget#model}.endian` property is
   244     *          specified, this symbol is defined and {little,big} is replaced
   245     *          by `model.endian`.
   246     *
   247     *      - `xdc_target__`{code_model_name}`Code`
   248     *          if this target's `{@link xdc.bld.ITarget#model}.codeModel` is
   249     *          specified, this symbol is defined and {code_model_name} is
   250     *          replaced by `model.codeModel`.
   251     *
   252     *      - `xdc_target__`{data_model_name}`Data`
   253     *          if this target's `{@link xdc.bld.ITarget#model}.dataModel` is
   254     *          specified, this symbol is defined and {data_model_name} is
   255     *          replaced by `model.dataModel`.
   256     *
   257     *      - `xdc_target__os_`{os_name}
   258     *          this symbol is always defined  and {os_name} is the
   259     *          target's os name (see `{@link xdc.bld.ITarget#os}`).
   260     *
   261     *      - `xdc_target__sizeof_`{type_name}
   262     *          this symbol is defined for each type name supported in the target's
   263     *          `{@link xdc.bld.ITarget#stdTypes}` structure, {type_name} is the
   264     *          name of one of the standard types supported above, and the 
   265     *          value is `sizeof(type_name)`.
   266     *
   267     *      - `xdc_target__alignof_`{type_name}
   268     *          this symbol is defined for each type name supported in the target's
   269     *          `{@link xdc.bld.ITarget#stdTypes}` structure, {type_name} is the
   270     *          name of one of the standard types supported above, and the
   271     *          value is the alignment required by the compiler for {type_name}.
   272     *
   273     *      - `xdc_target__bitsPerChar`
   274     *          this symbol is always defined and specifies the number of bits 
   275     *          in the target's `char`.  This value combined with the
   276     *          `xdc_target__sizeof_` values allows C code to determine the
   277     *          precise number of bits in any of the standard types.
   278     *  @p
   279     *
   280     *  @a(See)
   281     *  {@link http://www.open-std.org/jtc1/sc22/wg14/www/standards ISO-IEC JTC1-SC22-WG14 - C Approved standards}
   282     *
   283     *  @a(Throws)
   284     *  `XDCException` exceptions are thrown for fatal errors. The following
   285     *  error codes are reported in the exception message:
   286     *  @p(dlist)
   287     *      - `xdc.PACKAGE_NOT_FOUND`
   288     *           This error is reported whenever a specified package is not found
   289     *           This may happen for the following reasons:
   290     *      @p(blist)
   291     *            -  Ensure that the package in question is contained in one of
   292     *               the repositories named in the package path.  
   293     *            -  The package has not been built by the `xdc` tool even though
   294     *               the physical package directory may be present along the
   295     *               package path
   296     *   @p(dlist)
   297     *     - `xdc.FILE_NOT_FOUND`
   298     *            This error is reported when a specified file is not found. 
   299     *            Ensure that any directory name prefix in the name is a package
   300     *            directory contained in one of the repositories named in the
   301     *            package path.  For example, if "ti/targets/linkcmd.xdt" can't
   302     *            be found, make sure the directory `ti/targets/` is contained in
   303     *            at least one repository named in the package path.
   304     *      - `xdc.MODULE_NOT_FOUND`
   305     *            This error is reported when a specified module can't be
   306     *            found. Ensure that the package containing the module in
   307     *            question is contained in at least one repository named in
   308     *            the package path.
   309     *            Also ensure that the module name is qualified with the
   310     *            package name. For example, to refer to the module `Engine`
   311     *            in the package `ti.sdo.ce`, the module name should be
   312     *            specified as `ti.sdo.ce.Engine`.
   313     *      - `xdc.TOOL_USAGE_ERROR`
   314     *            This error may happen when the `xs` tool is not passed the
   315     *            expected command line arguments. 
   316     *      - `xdc.MODULE_UNDEFINED_MAIN_FUNCTION`
   317     *            This error is reported when the `xs` tool is passed a module
   318     *            that does not define a `main` function. Ensure that the
   319     *            meta-domain implementation of the module has a `main` function.
   320     *      - `xdc.SPEC_FILE_ERROR`
   321     *            This error is reported when there is a parsing error in a
   322     *            specification file. Check the spec. file for syntax errors.
   323     *      - `xdc.DEPRECATED_FUNCTION`
   324     *            This error is reported whenever a deprecated function is called.
   325     *      - `xdc.STATIC_INSTANCE`
   326     *            This error is reported when a function create() is called at the
   327     *            configuration time for a module that does not implement the
   328     *            function instance$static$init and therefore does not support
   329     *            static instances. 
   330     */
   331    package xdc [1,1,1] {
   332        /* base interface for all XDC packages */
   333        interface IPackage;
   334    }
   335    /*
   336     *  @(#) xdc; 1, 1, 1,389; 9-3-2012 16:22:00; /db/ztree/library/trees/xdc/xdc-y35x/src/packages/
   337     */
   338