1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*!
    13     *  ======== SourceDir ========
    14     *  Manage config generated source directories
    15     *
    16     *  Every "product" can generate a collection of source files that
    17     *  must be compiled into a single library and linked with the
    18     *  application.  Each collection of source files is placed in a
    19     *  subdirectory of a top-level directory and contains a GNU make file,
    20     *  named makefile, which builds the library.
    21     *
    22     *  This module generates a top-level makefile that builds all "product"
    23     *  libraries, the top-level directory that houses the "product"
    24     *  sub-directories, and any files necessary for integration with eclipse/CDT
    25     *  managed make.  The generated "product" files need only ensure their
    26     *  sources can be built via their generated makefile (from their
    27     *  sub-directory).
    28     */
    29    @Template("./SourceDir.xdt")
    30    metaonly module SourceDir
    31    {
    32        /*!
    33         *  ======== outputDir ========
    34         *  Top-level directory for config generated sources and makefiles
    35         *
    36         *  This directory path can be either an absolute path or a path
    37         *  relative to the build working directory at the time source files
    38         *  are generated (this is NOT necessarily the same as the build
    39         *  directory at the time the generated sources are built!)
    40         *
    41         *  This parameter must never be set to an existing directory with source
    42         *  files in it. The directory referenced by this parameter can be
    43         *  deleted when a CCS project or a RTSC package containing the
    44         *  configuration is cleaned.
    45         *
    46         *  If `outputDir` is not set, files will be output to the `./src`
    47         *  sub-directory of the directory containing the configuration script.
    48         */
    49        config String outputDir;
    50    
    51        /*
    52         *  ======== toBuildDir ========
    53         *  Top-level build working directory
    54         *
    55         *  This config parameter is the build working directory for the
    56         *  sources generated into `{@link #outputDir}` and is used to determine
    57         *  a relative path from the build directory to the output directory.
    58         *
    59         *  The directory path can be either an absolute path, a path
    60         *  relative from the build working directory at the time source files
    61         *  are generated, or `undefined`.
    62         *
    63         *  If `toBuildDir` and `outputDir` are `undefined`
    64         *  `toBuildDir` is set to be the parent of the build working directory
    65         *  at the time source files are generated; i.e., `"../"`
    66         *
    67         *  If `toBuildDir` is `undefined` and `outputDir` is defined,
    68         *  `toBuildDir` is set to be the build working directory at the time
    69         *  source files are generated; i.e., `"./"`.
    70         */
    71        config String toBuildDir;
    72    
    73        /*!
    74         *  ======== makefileName ========
    75         *  Top-level makfile name
    76         *
    77         *  This name is the base name of the makefile which is created in 
    78         *  `outputDir`.
    79         */
    80        config String makefileName = "makefile.libs";
    81    
    82        /*!
    83         *  ======== verbose ========
    84         *  Output progress messages during a build
    85         *
    86         *  Positive values cause additional progress messages to be displayed.
    87         *  The greater the value, the more information is displayed.
    88         *  @p(dlist)
    89         *      - 0
    90         *          no build progress output
    91         *      - 1
    92         *          output a message when the build is started and when it
    93         *          completes
    94         *      - 2
    95         *          output build progrss output (both stdout and stderr) as well
    96         *          all level 1 output
    97         *      - 3
    98         *          output the build commands used as well as all level 2 output
    99         *  @p
   100         */
   101        config Int verbose = 0;
   102        
   103        /*!
   104         *  ======== getRelativePath ========
   105         */
   106        metaonly String getRelativePath(String fm, String to);
   107    
   108        /*!
   109         *  ======== build ========
   110         *  Run make using the generated makefiles
   111         */
   112        metaonly Int build();
   113        
   114    instance:
   115        /*
   116         *  ======== create ========
   117         */
   118        create(String name);
   119        
   120        /*!
   121         *  ======== getName ========
   122         */
   123        metaonly String getName();
   124        
   125        /*!
   126         *  ======== getGenSourceDir ========
   127         *  Get name of the output directory for this set of source files
   128         *
   129         *  The name is either an absolute path or a path relative to the 
   130         *  build directory at the time configuration is run.
   131         */
   132        metaonly String getGenSourceDir();
   133    
   134        /*!
   135         *  ======== getGenLibraryName ========
   136         *  Get name of the output library for this set of source files
   137         *
   138         *  The name is either an absolute path or a path relative to the 
   139         *  build directory at the time configuration is run.
   140         */
   141        metaonly String getGenLibraryName();
   142        
   143        /*!
   144         *  ======== sourceDir ========
   145         *  Source directory for a specific "product's" generated sources
   146         *
   147         *  This path must be relative to `outputDir`.
   148         */
   149        config String sourceDir;
   150    
   151        /*!
   152         *  ======== libraryName ========
   153         *  Name of library of compiled sources in `sourceDir`
   154         *
   155         *  This path must be relative to `outputDir`.
   156         */
   157        config String libraryName;
   158    
   159        /*!
   160         *  ======== buildLibs ========
   161         *  Build generated library sources
   162         *
   163         *  If set to `false`, the configuration step will not attempt to
   164         *  build the generated library sources.
   165         */
   166        config Bool buildLibs = true;
   167    }
   168    /*
   169     *  @(#) xdc.cfg; 1, 0, 2, 0,385; 9-3-2012 16:22:06; /db/ztree/library/trees/xdc/xdc-y35x/src/packages/
   170     */
   171