1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== Object.xdc ========
    14     */
    15    package xdc.bld;
    16    
    17    /*!
    18     *  ======== Object ========
    19     *  Model of a compiled (or assembled) form of a source file.
    20     *
    21     *  Instances of this module represent object files.  Instances must be
    22     *  created via either the `{@link xdc.bld.Library#addObjects()}` or
    23     *  `{@link xdc.bld.Executable#addObjects()}` functions; this ensures that each
    24     *  object file created appears in the package's manifest and that it
    25     *  properly "inherits" appropriate default attributes from the containing
    26     *  library or executable.
    27     */
    28    metaonly module Object {
    29        /*!
    30         *  ======== Attrs ========
    31         *  Optional attributes for an Object instance
    32         *
    33         *  Unspecified attributes are "inherited" from
    34         *  `{@link xdc.bld.Executable#Attrs}`
    35         *  (`{@link xdc.bld.Library#Attrs}`) if this Object is added to an
    36         *  `{@link xdc.bld.Executable}` (`{@link xdc.bld.Library}`); i.e., if one
    37         *  of fields in this structure is unspecified *and* this field's name
    38         *  matches a field name in `{@link xdc.bld.Executable#attrs}`,
    39         *  then this field's value defaults to the value in specified by
    40         *  `{@link xdc.bld.Executable#attrs}`.  This mechanism makes it possible
    41         *  to establish executable-wide default value for any of the "inherited"
    42         *  attributes.
    43         *
    44         *  Suppose, for example, that you want all object files in this package
    45         *  to be build with the '`-o4`' optimization flag, but one particular file
    46         *  must be built with '`-o2`' (because the optimizer has a bug that it
    47         *  causes it to fail on this file).  The following build script fragment
    48         *  shows how this can be accomplished:
    49         *  @p(code)
    50         *      var exe = Pkg.addExecutable(..., {copts: '-o4'});
    51         *      exe.addObjects(['complex'], {copts: '-o2'});
    52         *      exe.addObjects(['foo', 'bar', ...]);
    53         *  @p
    54         *  Since many `Executable.attrs` are "inherited" from
    55         *  `{@link xdc.bld.PackageContents#attrs}`, it is also possible to
    56         *  establish package-wide default for these attributes.
    57         *
    58         *  @field(profile)  This string names a profile defined by the
    59         *          target used to produce the object file.  The profile
    60         *          specifies a set of compiler and assembler options that are
    61         *          to be used when producing the object.  Note that these tool
    62         *          options are in addition to any options specified via aopts,
    63         *          copts, etc.
    64         *
    65         *  @field(incs)  This string contains include path options used by
    66         *          the compiler (or assembler) to locate include files; e.g.,
    67         *          "`-I ../../include -I ../c55xx`".  Note that the syntax of 
    68         *          this string may be target dependent.
    69         *
    70         *  @field(defs)  This string contains options used by the
    71         *          compiler (or assembler) to define macros; e.g.,
    72         *          "`-D_C6xxx -DDEBUG=1`".  Note that the syntax of 
    73         *          this string may be target dependent.
    74         *
    75         *  @field(aopts)  This string contains options used by the assembler
    76         *          to produce object files; e.g., "`-mP1`".  Note that the syntax
    77         *          of this string may be target dependent.
    78         *
    79         *  @field(copts)  This string contains options used by the C/C++
    80         *          compiler to produce object files; e.g., "`-o3 -mi1`".  Note
    81         *          that the syntax of this string may be target dependent.
    82         *
    83         *  @field(preBuilt) If equal to `true`, this Boolean flag indicates
    84         *          that this object does not need to be built from sources; e.g.,
    85         *          it has been pre-built and delivered as a binary file without
    86         *          sources or some custom rule already built this object file.
    87         *          For pre-built objects, no rule will be created to remove the
    88         *          file as part of a package clean operation, the relative path
    89         *          to the file must be fully specified, and all other Object
    90         *          attributes are ignored.
    91         *
    92         *  @see #attrs
    93         *  @see xdc.bld.PackageContents#Attrs
    94         *  @see xdc.bld.Library#Attrs
    95         *  @see xdc.bld.Executable#Attrs
    96         */
    97        struct Attrs {
    98            String profile; /*! target options profile */
    99            String aopts;   /*! asm options for this object */
   100            String copts;   /*! C/C++ options for this object */
   101            String defs;    /*! definitions for this object */
   102            String incs;    /*! include options for this object */
   103            Bool   preBuilt;/*! don't create a rule to generate this file */
   104        };
   105        
   106    instance:
   107        /*!
   108         *  ======== create ========
   109         *  @_nodoc
   110         *  Instances should only be created via Executable.addObjects()
   111         */
   112        create();
   113    
   114        /*!
   115         *  ======== name ========
   116         *  The base name of the object file.
   117         *
   118         *  This name is passed as the name field of the
   119         *  `{@link xdc.bld.ITarget#CompileGoal}`.  The object file's name is
   120         *  composed as follows:
   121         *  @p(code)
   122         *      <name>.o<target_suffix>
   123         *  @p
   124         *  where `<name>` is name and `<target_suffix>` is the suffix defined 
   125         *  by each target that the file is built for.
   126         */
   127        config String name;
   128    
   129        /*!
   130         *  ======== attrs ========
   131         *  This instance's attributes.
   132         *
   133         *  These attributes (unless otherwise specified) are "inherited" from
   134         *  the container object that contains this instance.
   135         *
   136         *  @see xdc.bld.PackageContents#Attrs
   137         *  @see xdc.bld.Executable#Attrs
   138         *  @see xdc.bld.Library#Attrs
   139         */
   140        config Object.Attrs attrs;  
   141    }
   142    /*
   143     *  @(#) xdc.bld; 1, 0, 2,388; 9-3-2012 16:22:03; /db/ztree/library/trees/xdc/xdc-y35x/src/packages/
   144     */
   145