1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Sync.xdc ========
    15     */
    16    import xdc.runtime.Error;
    17    import xdc.runtime.Assert;
    18    import xdc.runtime.knl.ISync;
    19    
    20    /*!
    21     *  ======== Sync ========
    22     *  Provides synchronization APIs when an ISync.Handle is available
    23     *
    24     *  The application must first obtain an ISync.Handle. 
    25     *  It can get such a handle by directly calling {@link SyncGeneric#create} or 
    26     *  {@link SyncSemThread#create}. Then the application can use the generic 
    27     *  APIs provided by this module.
    28     */
    29    
    30    module Sync
    31    {
    32        /*!
    33         *  ======== WaitStatus ========
    34         *  Error codes returned by Sync_wait
    35         */
    36        enum WaitStatus {
    37            WaitStatus_ERROR = -1,
    38            WaitStatus_TIMEOUT = 0,
    39            WaitStatus_SUCCESS = 1
    40        };
    41        
    42        /*!
    43         *  ======== WAIT_FOREVER ========
    44         *  Used to wait forever
    45         */
    46        const UInt WAIT_FOREVER = ISync.WAIT_FOREVER;
    47    
    48        /*!
    49         *  ======== NO_WAIT ========
    50         *  Used to specify no waiting 
    51         */
    52        const UInt NO_WAIT = ISync.NO_WAIT;
    53    
    54        /*!
    55         *  ======== Proxy ========
    56         *  Platform-specific implementation
    57         *
    58         *  If ALL `ISync.Handles` were created using the same module 
    59         *  (e.g SyncSemProcess), then setting `Proxy` to `SyncSemProcess` and 
    60         *  `Sync.Proxy.abstractInstances$` to `false` will improve the
    61         *  performance of the `Sync` APIs.
    62         */
    63        proxy Proxy inherits ISync;
    64    
    65        /*!
    66         *  ======== query ========
    67         *  Query for a particular quality
    68         *
    69         *  FALSE is returned if quality not supported.
    70         *
    71         *  @param(sync)    sync handle
    72         *  @param(qual)    quality
    73         *
    74         *  @a(returns)     TRUE or FALSE.
    75         */
    76        Bool query(ISync.Handle sync, Int qual);
    77    
    78        /*!
    79         *  ======== signal ========
    80         *  Called at completion of an activity.
    81         *
    82         *  This function is non-blocking. It is also required that the underlying
    83         *  sync be binary in nature.
    84         *
    85         *  @param(sync)    sync handle
    86         */
    87        Void signal(ISync.Handle sync);
    88    
    89        /*!
    90         *  ======== wait ========
    91         *  Called to wait/poll for completion of an activity.
    92         *
    93         *  This function can block and typically waits for a semaphore to become
    94         *  available.
    95         *
    96         *  Non-blocking implementations should return {@link #WaitStatus_TIMEOUT}.
    97         *
    98         *  @param(sync)        sync handle
    99         *  @param(timeout)     timeout in microseconds
   100         *
   101         *  @a(returns)
   102         *  @p(blist)
   103         *  -{@link #WaitStatus_ERROR} if an error occured.
   104         *  -{@link #WaitStatus_TIMEOUT} denotes timeout.
   105         *  -{@link #WaitStatus_SUCCESS} semaphore was decremented. 
   106         *  @p
   107         */
   108        Int wait(ISync.Handle sync, UInt timeout, Error.Block *eb);
   109    }
   110    /*
   111     *  @(#) xdc.runtime.knl; 1, 0, 0,194; 9-3-2012 16:22:18; /db/ztree/library/trees/xdc/xdc-y35x/src/packages/
   112     */
   113