1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== GateProcess.xdc ========
    15     */
    16     
    17    import xdc.runtime.Assert;
    18    import xdc.runtime.Error;
    19    import xdc.runtime.IGateProvider;
    20    import xdc.runtime.knl.IGateProcessSupport;
    21    
    22    /*!
    23     *  ======== GateProcess ========
    24     *  Provides protection of critical sections across processes.
    25     *
    26     *  This module provides services through its proxy 
    27     *  IGateProcessSupport interface. It has a module wide config parameter 
    28     *  {@link #Proxy} which needs to be bound to an OS specific delegate before 
    29     *  this module can be used.
    30     *  
    31     *  Here is an example showing how the proxy is bound to an BIOS 6.x specific 
    32     *  delegate.
    33     *   
    34     *  @p(code)
    35     *  var GateProcess = xdc.useModule('xdc.runtime.knl.GateProcess');
    36     *  GateProcess.Proxy = 
    37     *      xdc.useModule('ti.sysbios.xdcruntime.GateProcessSupport');
    38     *  @p
    39     *
    40     *  Typically the package containing the delegates have a Settings module that 
    41     *  will bind all {@link xdc.runtime.knl} proxies. The following
    42     *  example sets up all the xdc.runtime.knl proxies.
    43     *   
    44     *  @p(code) 
    45     *  xdc.useModule("ti.sysbios.xdcruntime.Settings");
    46     *  @p
    47     */
    48    @InstanceInitError      /* because initialization can fail */
    49    @InstanceFinalize       /* have to GateProcess_Proxy_delete(gate) on delete */
    50    
    51    module GateProcess inherits IGateProvider
    52    {
    53        /*! Status returned by {@link #getReferenceCount} when there is an error */
    54        const Int GETREFCOUNT_FAILED = -1;
    55    
    56        /*! Proxy that needs to be bound to an OS specific delegate. */
    57        proxy Proxy inherits IGateProcessSupport;
    58        
    59        /*! Assert when  an invalid key is passed to create */
    60        config Assert.Id A_invalidKey = {
    61            msg: "A_invalidKey: the key must be set to a non-default value"
    62        };
    63    
    64    instance:
    65    
    66        /*! 
    67         *  globally unique key for SysV-style semaphore 
    68         *
    69         *  This is a required parameter.
    70         */
    71        config Int key = -1;
    72    
    73       /*!
    74        *  ======== create ========
    75        *  Create a GateProcess object.
    76        *
    77        *  This function creates a new `GateProcess` object which is initialized to
    78        *  count.  All gates created with the same key reference the same
    79        *  underlying synchronization object and work between processes.  For
    80        *  compatibility with the IGateProvider interface the argument key is
    81        *  passes in the params struct rather than as a full argument, but it is
    82        *  required.  Therefore calling this function with a `NULL` params struct
    83        *  is illegal.
    84        */
    85        override create();
    86    
    87        /*!
    88         *  ======== getReferenceCount ========
    89         *  Get the number of processes with references to this Gate.
    90         *
    91         *  @param(eb)        Pointer to Error.Block
    92         *  @a(returns)       Returns the number of processes that possess a 
    93         *                    reference to this gate, or GETREFCOUNT_FAILED if an 
    94         *            error occured.
    95         */
    96        Int getReferenceCount(Error.Block *eb);
    97        
    98    internal:
    99    
   100        struct Instance_State {
   101            Proxy.Handle proxyHandle;
   102        }
   103    }
   104    /*
   105     *  @(#) xdc.runtime.knl; 1, 0, 0,194; 9-3-2012 16:22:17; /db/ztree/library/trees/xdc/xdc-y35x/src/packages/
   106     */
   107