1    /* --COPYRIGHT--,EPL
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     *
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     *
    11     * --/COPYRIGHT--*/
    12    
    13    /*!
    14     *  ======== RTC_B ========
    15     *  MSP430 Real-Time Clock B
    16     */
    17    metaonly module RTC_B inherits IRTC {
    18    
    19    instance:
    20        /*!
    21         *  ======== baseAddr ========
    22         *  Address of the peripheral's control register.
    23         *
    24         *  A peripheral's registers are commonly accessed through a structure
    25         *  that defines the offsets of a particular register from the lowest
    26         *  address mapped to a peripheral. That lowest address is specified by
    27         *  this parameter.
    28         */
    29        config UInt baseAddr;
    30    
    31        /*! RTC interrupt enables */
    32        config regIntVect_t interruptSource[4];
    33    
    34        /*! Determine if each Register needs to be forced set or not */
    35        readonly config ForceSetDefaultRegister_t forceSetDefaultRegister[] =
    36        [
    37        ];
    38    
    39    }