1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    package xdc.tools.cdoc;
    13    
    14    /*!
    15     *  ======== Example ========
    16     *  XDOC markup language examples for modules and interfaces
    17     *
    18     *  This module demonstrates the features of XDOC on the declarations
    19     *  of an XDC module. View the source text of this .xdc file for details
    20     *  on how to use these examples.
    21     */
    22    module Example {
    23        /*!
    24         *  ======== AStruct ========
    25         *  Example structure declaration
    26         *
    27         * @field(aField) example field documentation
    28         */
    29        struct AStruct {
    30            Int aField;
    31        };
    32    
    33        /*!
    34         *  ======== aFunction ========
    35         *  Example function documentation
    36         *
    37         * @param(aParam) example function parameter documentation
    38         */
    39        Void aFunction(Int aParam);
    40    
    41        /*!
    42         *  ======== AnEnum ========
    43         *  Example enum documentation
    44         *
    45         *  @value(AVALUE)  example enum value documentation
    46         */
    47        enum AnEnum {
    48            AVALUE
    49        };
    50        /*!
    51         *  ======== AUnion ========
    52         *  Example union documentation
    53         *
    54         *  @field(aString) example union field documentation
    55         */
    56        union AUnion {
    57            String aString;
    58            Int anInt;
    59        };
    60    
    61        /*!
    62         *  ======== u ========
    63         *  Example statically initialized union documentation
    64         */
    65        config AUnion u = {aString: 'hello', anInt: 1234};
    66    
    67        /*!
    68         *  ======== ATypedEnum ========
    69         *  Example typed enumeration
    70         *
    71         *  This declaration defines a new type named ATypedEnum which is
    72         *  an alias of Int and two constants of type ATypedEnum.
    73         *
    74         *  Unlike ordinary C enums, where the compiler is free to choose an
    75         *  arbitrary type for enums, this declaration ensures that the new
    76         *  type is of a specific named type (in this case, Int).
    77         *
    78         *  @value(LOOP)  example "typed" enum value documentation
    79         */
    80        enum ATypedEnum : Int {
    81            LOOP = 6,
    82            PRINT = 28
    83        };
    84        
    85        /*!
    86         *  ======== ACmd ========
    87         *  Example "tagged union" documentation
    88         *
    89         *  This structure illustrates the "tagged union" pattern: one
    90         *  field of the structure indicates how to interpret the rest of the
    91         *  structure.
    92         *
    93         * @field(args) example structure field documentation
    94         */
    95        struct ACmd {
    96            ATypedEnum cmdId;
    97            union  {
    98                struct {
    99                    Int count;
   100                } loop;
   101    
   102                struct {
   103                    String msg;
   104                } print;
   105            } args;
   106        };
   107    
   108    }
   109    /*
   110     *  @(#) xdc.tools.cdoc; 1, 0, 0, 0,280; 6-27-2012 10:25:32; /db/ztree/library/trees/xdc/xdc-y30x/src/packages/
   111     */
   112