1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== ICpuDataSheet.xdc ========
    14     */
    15    package xdc.platform;
    16    
    17    /*!
    18     *  ======== ICpuDataSheet ========
    19     *  CPU information provided by the HW model.
    20     *
    21     *  The information in this interface is read-only, defined by the chip's
    22     *  data sheet, and is obtained by naming a module in a package that
    23     *  implements this interface.
    24     *
    25     *  Data sheets are created by platforms as part of creating an "execution
    26     *  context" (see `{@link xdc.platform.IPlatform#getExeContext}`).  This
    27     *  execution context includes the CPU's memory map as well as any external
    28     *  memory provided by the platform itself, for example.
    29     */
    30    metaonly interface ICpuDataSheet
    31    {
    32    
    33    instance:
    34        /*!
    35         *  ======== create ========
    36         *  Create a "data-sheet" for the specified revision of a CPU.
    37         *
    38         *  A "data sheet" for a CPU allows one to get specific attributes
    39         *  for a CPU programatically; e.g., the memory map of the CPU.
    40         *
    41         *  Notice that we don't specify CPU registers when we create a
    42         *  a data-sheet; registers are provided as necessary to the other
    43         *  functions defined in this interface.  This allows one to more easily
    44         *  get memory maps for several different setting of the registers,
    45         *  for example.
    46         *
    47         * @param(revision) a string that identifies revision of the CPU to be
    48         *                  created.
    49         */
    50        create(string revision);
    51        
    52        /*!
    53         *  ======== cpuCore ========
    54         *  A string identifying the CPU Core.
    55         *
    56         *  This uniquely identifies the instruction set that the CPU can
    57         *  decode and execute.
    58         */
    59        config string cpuCore;          /* 5400, 5500, etc... */
    60    
    61        /*!
    62         *  ======== cpuCoreRevision ========
    63         *  A string that uniquely identifies a revision of the core.
    64         */
    65        config string cpuCoreRevision;    /* 1.2, 2.0, etc... */
    66    
    67        /*!
    68         *  ======== minProgUnitSize ========
    69         *  The minimum addressable program unit size in 8-bit bytes
    70         */
    71        config int minProgUnitSize;
    72    
    73        /*!
    74         *  ======== minDataUnitSize ========
    75         *  The minimum addressable data unit size in 8-bit bytes
    76         */
    77        config int minDataUnitSize;
    78    
    79        /*!
    80         *  ======== dataWordSize ========
    81         *  The size of an int on the target in 8-bit bytes
    82         */
    83        config int dataWordSize;
    84        
    85        /*!
    86         *  ======== peripherals ========
    87         *  A map of peripherals available on the device
    88         */
    89        config xdc.platform.IPeripheral.Instance peripherals[string];
    90    
    91        /*!
    92         *  ======== deviceHeader ========
    93         *  The optional header file that define device specific constants and
    94         *  structures.
    95         */
    96        config string deviceHeader;
    97    
    98        /*!
    99         *  ======== getMemoryMap ========
   100         *  Get the memory map that corresponds to the values of the specified
   101         *  registers.
   102         *
   103         *  If a register is not specified and this register can affect the
   104         *  memory map, the register is assumed to be set to its reset
   105         *  value (the value of the register immediately after a CPU reset).
   106         *
   107         *  @param(registers)   a hash of named registers to values at the time
   108         *                      an executable is to be loaded (for example)
   109         *
   110         *  @a(returns)         Returns an array of
   111         *                      `{@link xdc.platform.IPlatform#Memory}`
   112         *                      objects that represent the memory visible to an
   113         *                      executable running on the CPU.
   114         */
   115    //    xdc.platform.IPlatform.Memory [] getMemoryMap(int registers [string]);
   116        function getMemoryMap(registers);
   117    
   118        /*!
   119         *  ======== getRegisterSet ========
   120         *  The set of valid register names for this CPU
   121         *
   122         *  This function returns the complete set of register names that may be
   123         *  passed to the `{@link #getMemoryMap()}` function.  This function is
   124         *  only used to enable one to write a "requires contract" for the
   125         *  `{@link #getMemoryMap()}` function.
   126         *
   127         *  @a(returns) Returns an array of valid register names (strings) for 
   128         *              this device; only names from this array are valid keys 
   129         *              for the registers argument to `{@link #getMemoryMap()}`.
   130         */
   131    //    string [] getRegisterSet();
   132        function getRegisterSet();
   133    };
   134    /*
   135     *  @(#) xdc.platform; 1, 0, 1, 0,381; 6-27-2012 10:24:49; /db/ztree/library/trees/xdc/xdc-y30x/src/packages/
   136     */
   137