1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== Release.xdc ========
    14     */
    15    package xdc.bld;
    16    
    17    /*!
    18     *  ======== Release ========
    19     *  Model of an archive of all files that are part of a release.
    20     *
    21     *  Release instances define a container object that represents all files that
    22     *  are part of a release of a package.  A release may, for example, include
    23     *  just the files necessary to support a particular ISA even though the
    24     *  package as a whole can support multiple ISAs.
    25     *
    26     *  Each Release instance is realized as a tar file containing the files
    27     *  that are part of a release of a package.
    28     */
    29    metaonly module Release {
    30    
    31        /*!
    32         *  ======== Attrs ========
    33         *  Optional Release attributes
    34         *
    35         *  Unspecified attributes are "inherited" from
    36         *  `{@link xdc.bld.PackageContents#Attrs}`; i.e., if one of fields in
    37         *  this structure is unspecified *and* this field's name matches a field
    38         *  name in `{@link xdc.bld.PackageContents#Attrs}`, then
    39         *  this field's value defaults to the value in specified by
    40         *  `{@link xdc.bld.PackageContents#attrs}`.  This mechanism makes it
    41         *  possible to establish package-wide default values for any of the
    42         *  "inherited" attributes.
    43         *
    44         *  However, elements added to a release can "override" these attributes.
    45         *  For example, when an executable is added to a release and the
    46         *  executable's attributes specify `'exportSrc = false'`, the release
    47         *  will not contain the executable's sources (even if the release's
    48         *  `{@link #attrs}.exportSrc` attribute is set to `true`).
    49         *
    50         *  @field(exportCfg)  If this field is set to `true`, configuration
    51         *          scripts will be part of the release.  If it is unspecified
    52         *          (or set to `null`), program configuration scripts will not
    53         *          be added to this release.
    54         *
    55         *  @field(exportDoc)  If this field is set to `true`,  generated
    56         *          documentation will be part of the release.
    57         *
    58         *  @field(exportSrc)  If this field is set to `true`, sources
    59         *          used to produce object files will be part of the release.
    60         *          If it is unspecified (or set to `null`), no sources will
    61         *          be part of this release.
    62         *
    63         *  @field(exportExe)  If this field is set to `true`, executables
    64         *          will be part of the release.  If it is unspecified (or set
    65         *          to `null`), executables will not be part of this release.
    66         *
    67         *  @field(exportAll)  If this field is set to `true`, all files
    68         *          in this package that are not known to be generated are in
    69         *          the release.  If it is unspecified (or set to `null`), these
    70         *          files will not be added to this release.
    71         *
    72         *          Note that the set of files specified by `exportAll` is
    73         *          determined at the time the package's makefile is generated.
    74         *          If one of these files is subsequently removed before the
    75         *          release is built, the build of the release will fail; a file
    76         *          required by the release no longer exists.  If the file is
    77         *          not really required for the release, you must trigger a
    78         *          rebuild for the generated makefiles; either touch
    79         *          `package.bld` or remove the generated makefile and re-build
    80         *          the release.
    81         *
    82         *  @field(relScript)  If this field is non-`null`, the string names a
    83         *          "release script" that is run to post-process the
    84         *          files that are part of a release.  Like
    85         *          configuration scripts, the string names a script
    86         *          file that is searched for first in the in package's
    87         *          base directory, and then along the package path.  See
    88         *          `{@link Manifest}` for more information about release scripts
    89         *          and what they can do.
    90         *
    91         *  @field(relScriptArgs)  If this field is non-`null`, the string is
    92         *          used to initialize the `arguments[]` array which is
    93         *          accessible to the release script named by `relScript`.  The
    94         *          elements of the `argumants[]` array are formed from the white
    95         *          space separated elements of `relScriptArgs`.  If this string
    96         *          is `null` or empty, the `arguments[]` array has length `0`.
    97         *
    98         *  @field(label)  This string allows one to "tag" each release with a
    99         *          label that can be used by other tools to select appropriate
   100         *          releases.  For example, the label might contain customer names.
   101         *
   102         *          This label is not interpreted by the XDC tools.  It is simply 
   103         *          recorded in the package's build model XML file
   104         *          (`package/package.bld.xml`) and retrieved via
   105         *          `{@link xdc.bld.BuildEnvironment#getReleaseDescs()}`
   106         *
   107         *  @field(prefix)  This string allows one to "export" each release to a
   108         *          location outside of the package.  `prefix` is prepended
   109         *          to the name of the release name to form the name of the
   110         *          release archive.
   111         *
   112         *          For example, setting `prefix` to `"../"` implies that a 
   113         *          release named `"exports/foo"` generates an archive file named
   114         *          `foo.tar` in the directory `"../exports"`.
   115         *
   116         *          `prefix` must either begin with the '^' character or
   117         *          be a path that is relative to the package's "base"
   118         *          directory; i.e., the directory containing the package's
   119         *          specification file `package.xdc`.
   120         *
   121         *          If `prefix` begins with the '^' character, the
   122         *          remainder of the string is treated as though it is relative
   123         *          to the package's repository.  In effect, the '^' character is
   124         *          replaced with an appropriate number of '../' sequences to
   125         *          sufficient to navigate to the package's repository.
   126         *
   127         *          If it is not specified (or set to `null`) the current setting
   128         *          of `{@link xdc.bld.PackageContents#releasePrefix}` is used.
   129         *
   130         *  @field(compress) If this field is set to `true`, the release
   131         *          archive file will be compressed; otherwise, the
   132         *          archive will not be compressed.  Archives are compressed
   133         *          via `gzip`; compressed archives are `.tar.gz` files.
   134         *
   135         *  @field(archiver) This field names the archiver to use when creating a
   136         *          release.  Two archivers are currently supported:
   137         *          "tar" and "zip".  If the archiver is set to "zip"
   138         *          the `{@link #Attrs.compress}` field is implicitly set to
   139         *          `true`.
   140         *
   141         *  @see #attrs
   142         */
   143        struct Attrs {
   144            String  archiver;       /*! "tar" or "zip"; defaults to "tar" */
   145            Bool    compress;       /*! if `true`, compress package archive */
   146            Bool    exportDoc;      /*! if `true`, export generated docs */
   147            Bool    exportExe;      /*! if `true`, export program executables */
   148            Bool    exportCfg;      /*! if `true`, export program cfg scripts */
   149            Bool    exportSrc;      /*! if `true`, export all package sources */
   150            Bool    exportAll;      /*! if `true`, export all files in package */
   151            String  relScript;      /*! release files post-processing script */
   152            String  relScriptArgs;  /*! optional arguments to relScript */
   153            String  prefix;         /*! prefix for name of install of archive */
   154            String  label;          /*! uninterpreted label for this release */
   155        };
   156    
   157        /*!
   158         *  ======== Desc ========
   159         *  A description of a release
   160         *
   161         *  This structure provides information about a release that can be
   162         *  used to select from multiple releases provided by a package.
   163         *
   164         *  @see xdc.bld.BuildEnvironment#getReleaseDescs()
   165         */
   166        struct Desc {
   167            String name;    /*! the name used to create the release */
   168            String aname;   /*! the file name of the archive */
   169            String label;   /*! the label given to the release */
   170        };
   171        
   172        /*!
   173         *  ======== DescArray ========
   174         *  An array of release descriptors
   175         */
   176        typedef Desc DescArray[];
   177    
   178    instance:
   179        /*!
   180         *  ======== create ========
   181         *  @_nodoc
   182         *  Instances should only be created via PackageContents.addRelease()
   183         */
   184        create();
   185    
   186        /*!
   187         *  ======== name ========
   188         *  The name of the release.
   189         *
   190         *  This name is the base name of the generated tar file containing all
   191         *  files that make up the release.  For example, if the name of the
   192         *  release is "foo" then the file "foo.tar" (located in the same
   193         *  directory as package.bld) is a tar file containing the release files.
   194         *
   195         *  Note that each package has at least one release defined, the default
   196         *  release.  The default release's name is the name of the package with
   197         *  '.'s replaced with '_'s.  For example, the default release name for
   198         *  the package "foo.bar" is "foo_bar" and the generated tar file is
   199         *  named "foo_bar.tar".
   200         */
   201        config String name;
   202        
   203        /*!
   204         *  ======== attrs ========
   205         *  This instance's attributes.
   206         *
   207         *  Unless explicitly specified, these attributes are "inherited" from
   208         *  the package's attributes (`{@link xdc.bld.PackageContents#attrs}`)
   209         *
   210         *  @see xdc.bld.PackageContents#attrs
   211         */
   212        config Release.Attrs attrs;
   213    
   214        /*!
   215         *  ======== otherFiles ========
   216         *  Additional files to add to this release.
   217         *
   218         *  This is an array of arbitrary files that are to be included
   219         *  in this release of the package.
   220         *
   221         *  Only those files that are not already directly (or indirectly) named
   222         *  by adding programs or libraries to this release need to appear in
   223         *  this array.
   224         */
   225        config String otherFiles[];
   226    
   227        /*!
   228         *  ======== excludeDirs ========
   229         *  List of directory base names to exclude
   230         *
   231         *  This is an array of arbitrary directory "base names" that should
   232         *  be excluded in this release of the package.  This list only
   233         *  excludes directories that would otherwise be added due to the
   234         *  recursive include of a parent directory.
   235         *
   236         *  For example, if a directory is specified in `{@link #otherFiles}`
   237         *  all of its sub-directories will be added unless those sub-directories
   238         *  are named in the `excludeDirs` list.
   239         *
   240         *  This list is often used to exclude "hidden" directories added by
   241         *  change control systems and IDEs (`.svn`, `.git`, `.settings`, ...).
   242         *
   243         *  @see #otherFiles
   244         *  @see PackageContents#excludeDirs
   245         */
   246        config String excludeDirs[];
   247    }
   248    /*
   249     *  @(#) xdc.bld; 1, 0, 2,384; 6-27-2012 10:24:46; /db/ztree/library/trees/xdc/xdc-y30x/src/packages/
   250     */
   251