1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== ITarget.xdc ========
    14     */
    15    package xdc.bld;
    16    
    17    /*!
    18     *  ======== ITarget ========
    19     *  The interface between code generation tool-chains and the XDC Build
    20     *  Engine.
    21     *
    22     *  This interface defines an abstract interface that must be supported by
    23     *  a compiler tool-chain in order to be used in an XDC build environment.
    24     *  This interface allows the XDC Build engine to treat all compiler tool
    25     *  chains uniformly; thus, it is possible to add support for a new compiler
    26     *  without making *any* changes to the build engine.
    27     */
    28    metaonly interface ITarget {
    29    
    30        /*!
    31         *  ======== Model ========
    32         *  Target runtime model.
    33         *
    34         *  @field(`endian`)    this string specifies the endianess of the
    35         *                      generated code.  Valid values include:
    36         *                      @p(dlist)
    37         *                          - `"big"`
    38         *                              big endian
    39         *                          - `"little"`
    40         *                              little endian
    41         *                          - `null`
    42         *                              unspecified
    43         *                      @p
    44         *
    45         *  @field(`codeModel`) this string specifies a target-specific code size
    46         *                      model.  Valid values include:
    47         *                      @p(dlist)
    48         *                          - `"near"`
    49         *                              C54 near mode
    50         *                          - `"far"`
    51         *                              C54 far mode
    52         *                          - `undefined`
    53         *                              unspecified
    54         *                      @p
    55         *
    56         *  @field(`dataModel`) this string specifies a target-specific data size
    57         *                      model.  Valid values include:
    58         *                      @p(dlist)
    59         *                          - `"large"`
    60         *                              C55, C28 large model
    61         *                          - `undefined`
    62         *                              unspecified
    63         *                      @p
    64         *
    65         *  @field(`shortEnums`) this flag specifies if a target fits the values
    66         *                      of an enumeration into the smallest integer type
    67         *                      that can accept all values. If that is the case,
    68         *                      this flag must be set to `true`. If all values are
    69         *                      the size of an Int, this flag can be either set
    70         *                      to `false` or left unspecified.
    71         * @see #model
    72         */
    73        struct Model {
    74            String endian;      /*! endian-ness of this target */
    75            String codeModel;   /*! target-specific code model */
    76            String dataModel;   /*! target-specific data model */
    77            Bool   shortEnums;  /*! if true, enums are packed into smallest integral type */
    78        }
    79    
    80        /*!
    81         *  ======== name ========
    82         *  Nickname for this target.
    83         *
    84         *  This name is typically the name of the module without the package
    85         *  name prefix.  Thus, it is not necessarily globally unique.
    86         *
    87         *  Use the `$name` property of the module to get a globally unique name
    88         *  for the target.
    89         */
    90        readonly config String name;
    91    
    92        /*!
    93         *  ======== suffix ========
    94         *  Suffix appended to all objs, libraries, and executable.
    95         *
    96         *  All files generated by this target (object files, archives,
    97         *  executables, etc.) have file names whose extensions end with
    98         *  suffix.  In particular, targets create files with the following
    99         *  extensions:
   100         *  @p(dlist)
   101         *      - `".a<suffix>"`
   102         *              archive files (i.e., libraries)
   103         *      - `".o<suffix>"`
   104         *              object files
   105         *      - `".s<suffix>"`
   106         *              assembly language source (see `{@link #scompile()}`)
   107         *      - `".x<suffix>"`
   108         *              executable files
   109         *
   110         *  This suffix should be chosen to globally and uniquely identify the
   111         *  EABI (Embedded Application Binary Interface) of the objects produced
   112         *  by this target.  Targets with the same suffix should
   113         *  should produce 100% EABI compatible objects and, targets with different
   114         *  suffixes should produce objects with incompatible EABIs.
   115         *
   116         *  @see #scompile()
   117         */
   118        readonly config String suffix;
   119    
   120        /*!
   121         *  ======== compatibleSuffixes ========
   122         *  Array of suffixes used by targets compatible with this target
   123         *
   124         *  This array is used to identify a set of targets that produce
   125         *  code that can be linked with code produced by this target, where the
   126         *  order of suffixes defines the order of preferrence. This
   127         *  parameter is used by `findSuffixes()`.
   128         *
   129         *  For example, an Arm target which builds for v6 architecture might have
   130         *  the following values in its `compatibleSuffix`: ["v5T", "MV470"].
   131         *  This means that code produced by targets with suffixes "v5T' and
   132         *  "MV470" can be linked with code produced by that target, and that "v5T"
   133         *  code is more preferred than "MV470" code.
   134         */
   135        config String compatibleSuffixes[];
   136    
   137        /*!
   138         *  ======== isa ========
   139         *  CPU Instruction Set Architecture (ISA)
   140         *
   141         *  This parameter is used to identify a set of targets that produce
   142         *  code for a common ISA.  This is used by build scripts that need to
   143         *  build for all targets that support a particular device.
   144         *
   145         *  For example, the build script for a package that is designed for
   146         *  the TMS32064xx (and no other CPU) can easily specify that it
   147         *  should be built for all targets that generate code for the
   148         *  TMS320C64xx without having to specify a specific target.  This
   149         *  allows the user to add new targets (big endian, little endian,
   150         *  different compilers, etc.) that build for the TMS320C64xx without
   151         *  having to modify the package's build script.
   152         *
   153         *  Note that this field should not be confused with platform ISA
   154         *  names; this field is defined by target tool-chains and may differ
   155         *  from the names given by a CPU device.
   156         *
   157         *  @see xdc.platform.ICpuDataSheet
   158         */
   159        readonly config String isa;
   160    
   161        /*!
   162         *  ======== model ========
   163         *  Run-time model
   164         *
   165         *  This structure identifies a particular run-time model
   166         *  used by the compiler to generate instructions.
   167         */
   168        readonly config Model model;
   169    
   170        /*!
   171         *  ======== os ========
   172         *  Name of OS required to run programs built for this target.
   173         *
   174         *  Native executables are run by the host OS.  This OS often
   175         *  defines runtime interfaces that all executables (implicitly or
   176         *  explicitly) use.
   177         *
   178         *  If os is undefined, then no OS is required.
   179         */
   180        readonly config String os;
   181    
   182        /*!
   183         *  ======== rts ========
   184         *  Name of a run-time support package to include
   185         *
   186         *  Development environments often provide a set of common run-time
   187         *  support functions that all other code can easily utilize; e.g.,
   188         *  some means for performing a "printf", normal program termination
   189         *  with "exit status", etc.  If the `rts` parameter is non-`null`, it is
   190         *  the name of a package that is implicitly imported when building
   191         *  any executable that is built using this target.  If `rts` is
   192         *  undefined, no rts package is imported.
   193         *
   194         *  This parameter makes it possible for the target producer to name
   195         *  a package that provides a target-specific implementation of a runtime
   196         *  support interface.  Clients of a target do not need to explicitly
   197         *  name a target specific rts implementation; thus, it is not
   198         *  possible for the client to inadvertently name the wrong (or an
   199         *  incompatible) rts implementation.
   200         *
   201         *  Note: this package is *NOT* included if the executable's
   202         *  `{@link xdc.bld.Executable#attrs}.rtsName` attribute is set to `null`;
   203         *  see {@link xdc.bld.Executable#Attrs}.  It is also not included if the
   204         *  executable is a legacy DSP/BIOS program.
   205         */
   206        readonly config String rts;
   207    
   208        /*!
   209         *  ======== base ========
   210         *  A target that this target is based upon.
   211         *
   212         *  If non-`null`, this target shares the same tool-chain of the specified
   213         *  base target.  This parameter is used to determine various default
   214         *  values for target configuration parameters.  For example, the default
   215         *  setting of `{@link #rootDir}` is the value of the base's
   216         *  `{@link #rootDir}` setting.
   217         */
   218        readonly config ITarget.Module base;
   219        
   220        /*!
   221         *  ======== dllExt ========
   222         *  @_nodoc dlls are not yet fully supported
   223         */
   224        config String dllExt;
   225    
   226        /*!
   227         *  ======== execExt ========
   228         *  Extension for executables.
   229         *
   230         *  Operating systems and tools often have a strong preference for a
   231         *  specific extension for executables; e.g., Windows expects executables
   232         *  to have the extension "`.exe`".  If this parameter is set, executables
   233         *  will be given the specified extension instead of the default
   234         *  "`.x<suffix>`", where `<suffix>` is the target's suffix parameter.
   235         *
   236         *  The `execExt` is an expression that is expanded prior to use.
   237         *  Expressions of the form "`$(name)`" within the
   238         *  pattern string are expanded if "`name`" is one of the built-in
   239         *  variables listed below.
   240         *
   241         *  Built-in variables for `execExt`:
   242         *  @p(dlist)
   243         *      - `trgName`
   244         *              the target's `name` property
   245         *      - `trgSuffix`
   246         *              the target's `suffix` property
   247         *      - `platPName`
   248         *              the executable's platform package name
   249         *      - `platIName`
   250         *              the executable's platform instance name
   251         *  @p
   252         *
   253         *  @a(Example) If you want to build a portable executable for multiple
   254         *  targets side-by-side and you want (or need) to use a fixed extension
   255         *  such as ".out" for all executables, setting `execExt` to
   256         *  `"_$(trgSuffix).out"` for all targets ensures that all generated
   257         *  executables will have unique names and yet share a common extension
   258         *  of `".out"`.
   259         */
   260        config String execExt;
   261    
   262        /*!
   263         *  ======== platform ========
   264         *  The default platform name for this target
   265         *
   266         *  Build scripts often build for just one platform per target.  This
   267         *  parameter allows one to establish a default platform for each 
   268         *  target in a build.
   269         *
   270         *  If this parameter is `null` or `undefined` and `{@link #platforms}`
   271         *  array is non-empty, it is initialized to be the first element of the
   272         *  platforms array (i.e., `{@link #platforms[0]}`).
   273         */
   274        config String platform;
   275    
   276        /*!
   277         *  ======== platforms ========
   278         *  A set of platforms that can support this target
   279         *
   280         *  Some build scripts build executables for "all" platforms; e.g.,
   281         *  regression test suites.  This  parameter allows one to establish
   282         *  a set of platforms that build scripts can legitimately use to
   283         *  create executables, for example.
   284         *
   285         *  If this array is empty (i.e., has length 0) and `{@link #platform}`
   286         *  is non-`null`, platforms is initialized to an array of one element
   287         *  equal to `{@link #platform}`.
   288         */
   289        config String platforms[] = [];
   290    
   291        /*!
   292         *  ======== binaryParser ========
   293         *  The name of a object file parser
   294         *
   295         *  The value of this configuration parameter is the name of a
   296         *  module or Java class that implements the ?? interface.  This
   297         *  interface is used to extract information from the object files
   298         *  produced by this target.
   299         *
   300         *  @_nodoc object file readers are not yet fully supported
   301         */
   302        config String binaryParser;
   303        
   304        /*!
   305         *  ======== version ========
   306         *  The Compatibility Key associated with this target.
   307         *
   308         *  @a(Readonly) This value is automatically computed by the XDC Build
   309         *  Engine by executing the `{@link #getVersion()}` function after 
   310         *  `package.bld` completes but prior to generating `package.mak`.
   311         */
   312        config String version;
   313    
   314        /*!
   315         *  ======== versionRaw ========
   316         *  The unmodified version string associated with this target.
   317         *
   318         *  @a(Readonly) This value is automatically computed by the XDC Build
   319         *  Engine by executing the `{@link #getVersion()}` function after 
   320         *  `package.bld` completes but prior to generating `package.mak`.
   321         *
   322         *  @_nodoc
   323         */
   324        config String versionRaw;
   325    
   326        /*!
   327         *  ======== DebugGen ========
   328         *  Debugger integration support.
   329         *
   330         *  This structure specifies additional files that are generated
   331         *  in order to support integration with a debugger.  For example, the
   332         *  default setting for TI targets specifies the generation of CCS
   333         *  project files that allow one to easily debug executables that have
   334         *  been constructed from multiple packages.
   335         *
   336         *  There are two "types" of debug support files that are generated;
   337         *  one for the package as a whole, and one for each executable.
   338         *  Since packages may contain portable sources that are built for more
   339         *  than one target, a "package-level" file is generated for each target
   340         *  used in the package.  A separate file is generated for each
   341         *  executable built within the package.
   342         *
   343         *  The `execTemplate` and `packageTemplate` fields name a template that
   344         *  is expanded in the context of the config model and the build
   345         *  model, respectively.  These fields should be set to a file name
   346         *  string which is relative to the package path; e.g., the string
   347         *  "`ti/targets/cc_exec.xdt`" refers to the file "`cc_exec.xdt`" in the
   348         *  `ti.targets` package located along the package path.
   349         *
   350         *  Preconditions for the `execTemplate`:
   351         *  @p(dlist)
   352         *      - `this`
   353         *              the configured program object (`xdc.cfg.Program`);
   354         *              i.e., the program object *after* the program's
   355         *              configuration script completes.
   356         *      - `$args`
   357         *              array of arguments passed to the template
   358         *
   359         *      - `$args[1]`
   360         *              the name of the executable being produced for this
   361         *              configuration.
   362         *
   363         *      - `environment`
   364         *              hash table of XDC global parameters; e.g., `"xdc.path"`,
   365         *              `"xdc.root"`, ...
   366         *  @p
   367         *  Preconditions for the `packageTemplate`:
   368         *  @p(dlist)
   369         *      - `this`
   370         *              the "package contents" object (i.e.,
   371         *              `xdc.bld.PackageContents`) *after* the package's
   372         *              build script (`package.bld`) completes.
   373         *      - `$args`
   374         *              array of arguments passed to the template
   375         *
   376         *      - `$args[0]`
   377         *              the target (a module implementing the
   378         *              `{@link xdc.bld.ITarget}` interface)
   379         *
   380         *      - `$args[1]`
   381         *              hash-table of all package sources
   382         *
   383         *      - `environment`
   384         *              hash table of XDC global parameters; e.g., `"xdc.path"`,
   385         *              `"xdc.root"`, ...
   386         *  @p
   387         *  The `execPattern` and `packagePattern` fields are expressions that
   388         *  are expanded prior to template expansion to determine the name of
   389         *  the output file.  Expressions of the form "`$(name)`" within the
   390         *  pattern string are expanded if "`name`" is one of the built-in
   391         *  variables listed below.
   392         *
   393         *  Built-in variables for `execPattern`:
   394         *  @p(dlist)
   395         *      - `cfgName`
   396         *              the name of the generated configuration file (without
   397         *              any directory prefix);
   398         *      - `cfgDir`
   399         *              the name of the directory containing the config file;
   400         *      - `exeName`
   401         *              the name of the executable file (without any 
   402         *              directory prefix);
   403         *      - `exeDir`
   404         *              the directory containing the executable file.
   405         *  @p
   406         *  Both the `exeDir` and `cfgDir` are relative to the directory 
   407         *  containing the `package.bld` script.
   408         *
   409         *  Built-in variables for `packagePattern`:
   410         *  @p(dlist)
   411         *      - `pkgName`
   412         *              the package's name (e.g., `"ti.targets"`);
   413         *      - `trgName`
   414         *              the target's `name` property;
   415         *      - `trgSuffix`
   416         *              the target's `suffix` property.
   417         *
   418         * @see #debugGen
   419         */
   420        struct DebugGen {
   421            String execTemplate;    /*! debugger template for executable */
   422            String execPattern;     /*! exec file name pattern */
   423            String packageTemplate; /*! debugger template for package */
   424            String packagePattern;  /*! package file name pattern */
   425        }
   426        
   427        /*!
   428         *  ======== debugGen ========
   429         *  Debugger/IDE file generation support.
   430         *
   431         *  This parameter allows one to automatically generate files that
   432         *  can be used by an IDE to more easily debug (and possibly rebuild)
   433         *  specified goals.
   434         *
   435         *  To avoid unnecessary build time overhead, these files are not always
   436         *  generated; by default, they are only generated for "debug" profiles.
   437         *  The generation of these files is controlled by the
   438         *  `{@link xdc.cfg.Program#gen}` configuration parameter.  To force these
   439         *  files to be generated for a particular executable, add the following
   440         *  line to the executable's program configuration script:
   441         *  @p(code)
   442         *      Program.gen.debuggerFiles = true;
   443         *  @p
   444         *
   445         *  It is also possible to disable the generation of selected files by
   446         *  setting the appropriate fields of `{@link #DebugGen}` to `null` in
   447         *  your `config.bld` script.
   448         */
   449        config DebugGen debugGen;
   450        
   451        /*!
   452         *  ======== Extension ========
   453         *  File extension to file type association.
   454         *
   455         *  This structure is used by the Build Engine to determine whether a 
   456         *  file should be treated as C++, C, or assembly language source.
   457         *
   458         *  @field(suf) the file extension including any '.' characters
   459         *
   460         *  @field(typ) the type of the file having this extension.
   461         *              Allowable file type identifiers include:
   462         *              @p(dlist)
   463         *                 - `"c"`
   464         *                      C language source file
   465         *                 - `"asm"`
   466         *                      assembly language source file
   467         *                 - `"cpp"`
   468         *                      C++ language source file
   469         *
   470         *  @see #extensions
   471         */
   472        struct Extension {
   473            String suf;     /*! file extension (including any '.') */
   474            String typ;     /*! type of this file; e.g., `"c"`, `"asm"`, ... */
   475        };
   476        
   477        /*!
   478         *  ======== extensions ========
   479         *  File extensions recognized by this target.
   480         *
   481         *  This is a user modifiable table used to customize file extensions
   482         *  recognized by each target.
   483         *
   484         *  For example, to add a new assembly language extension, say "`.s64`",
   485         *  to the target `ti.targets.C64P`, add the following lines to the
   486         *  build model startup script:
   487         *  @p(code)
   488         *      var C64P = xdc.module('ti.targets.C64P');
   489         *      C64P.extensions[".s64"] = {
   490         *          suf: ".s64", typ: "asm"
   491         *      };
   492         *
   493         *  Note that individual targets may add additional language types.
   494         *
   495         *  It is also possible to remove default extensions.  For example, to
   496         *  remove the "`.asm`" extension from the target `ti.targets.C64P`, add
   497         *  the following lines to the build model startup script:
   498         *  @p(code)
   499         *      var C64P = xdc.module('ti.targets.C64P');
   500         *      delete C64P.extensions[".asm"];
   501         *  @p
   502         */
   503        config Extension extensions[string] = [
   504            [".asm", {suf: ".asm", typ: "asm"}],
   505            [".c",   {suf: ".c",   typ: "c"  }],
   506            [".cpp", {suf: ".cpp", typ: "cpp"}],
   507            [".cxx", {suf: ".cxx", typ: "cpp"}],
   508            [".C",   {suf: ".C",   typ: "cpp"}],
   509            [".cc",  {suf: ".cc",  typ: "cpp"}],
   510        ];
   511    
   512        /*!
   513         *  ======== versionMap ========
   514         *  Map of compiler version numbers to compatibility keys.
   515         *
   516         *  `versionMap` is a user modifiable table used to map tool-chain 
   517         *  version numbers to Compatibility Keys.
   518         *
   519         *  Each target defines the format of the tool-chain version obtained
   520         *  from the tool-chain.  The user can then map new tool-chain version
   521         *  strings to an appropriate compatibility key.  
   522         *
   523         *  Each target must respect the mapping defined by this table; i.e.,
   524         *  if the user supplies a compatibility key in this map, it must be
   525         *  returned when `{@link #getVersion()}` is called.
   526         *
   527         *  Thus, it is possible for the user to assert that any two compiler
   528         *  tool chains should be treated as equivalent (or incompatible) by
   529         *  mapping their version numbers to identical (incompatible)
   530         *  compatibility keys.
   531         *
   532         *  @see ti.targets.ITarget#versionMap
   533         */
   534        config String versionMap[string] = [
   535        ];
   536    
   537        /*!
   538         *  ======== alignDirectiveSupported ========
   539         *  The compiler supports an align directive.
   540         */
   541        readonly config Bool alignDirectiveSupported = false; 
   542        
   543        /*!
   544         *  ======== rootDir ========
   545         *  Installation directory for this target's code generation tools.
   546         *
   547         *  Since each target potentially "wraps" a different compiler tool-chain
   548         *  and each tool-chain will, in general, assume a different physical
   549         *  design for the installation of the compiler and its associated
   550         *  libraries and headers, one must consult each specific target to know
   551         *  how to set this parameter.
   552         *
   553         *  If the `{@link #base}` parameter is `null`, this parameter *must* be
   554         *  set by the user; otherwise, `rootDir` defaults to the value
   555         *  `base.rootDir`.
   556         */
   557        config String rootDir;
   558    
   559        /*!
   560         *  ======== CompileOptions ========
   561         *  Options passed to the compiler/assembler.
   562         *
   563         *  @field(aopts)   a string of target-specific assembler options
   564         *  @field(copts)   a string of target-specific C/C++ compiler options
   565         *  @field(cfgcopts)   a string of C/C++ compiler options for C config file,
   566         *                  includes 'copts' in addition to the value passed
   567         *  @field(defs)    a string of macro definitions each of the form
   568         *                  "`-Dname=value`" separated by white space
   569         *  @field(incs)    a string of include directories each of the form
   570         *                  "`-Idir`" separated by white space
   571         *
   572         *  @a(Predefined Macros)
   573         *  The XDC Build Engine automatically adds several predefined macros via
   574         *  `-D` definitions that enable conditional compilation of source files
   575         *  based on build-specific attributes.
   576         *  @p(dlist)
   577         *      - `xdc_bld__profile_`{profile_name}
   578         *          this symbol is always defined and {profile_name} is the
   579         *          compile goal's (see `{@link #CompileGoal}`) profile name.
   580         *  @p
   581         *
   582         *  In addition, each target defines a set of macros that enable clients
   583         *  to portably support big/little endian targets, for example.  These
   584         *  macros are indirectly included by sources that include `xdc/std.h`; 
   585         *  see `{@link xdc}`.
   586         *
   587         *  @see #OptionSet
   588         *  @see #CompileGoal
   589         *  @see xdc
   590         */
   591        struct CompileOptions {
   592            String aopts;       /*! goal specific ASM options */
   593            String copts;       /*! goal specific C compiler options */
   594            String cfgcopts;    /*! goal specific C config file options */
   595            String defs;        /*! goal specific C/ASM definition options */
   596            String incs;        /*! goal specific C/ASM include options */
   597        };
   598        
   599        /*!
   600         *  ======== OptionSet ========
   601         *  Collection of tool-chain options.
   602         *
   603         *  This structure is used to define a collection of tool-chain
   604         *  options that are used as a group to achieve some effect supported
   605         *  by the tool-chain.  For example, some compilers require that
   606         *  specific options be passed to the compiler *and* linker in order
   607         *  to generate execution profile information or code coverage
   608         *  statistics.
   609         *
   610         *  @field(compilerOptions) a set of compiler/assembler options
   611         *  @field(linkOpts)        a string of target-specific linker options
   612         *  @field(archiveOpts)     a string of target-specific archiver options
   613         *  @field(filters)         an array of filters applied (in order) to
   614         *                          tool-chain commands
   615         *
   616         *  @see #profiles
   617         */
   618        struct OptionSet {
   619            CompileOptions  compileOpts;    /*! profile-specific compiler opts */
   620            String          linkOpts;       /*! profile-specific linker opts */
   621            String          archiveOpts;    /*! profile-specific archiver opts */
   622    
   623            ITargetFilter.InstDesc  filters[]; /*! ITargetFilter instance descs */
   624        };
   625        
   626        /*!
   627         *  ======== profiles ========
   628         *  Profiles supported by this target.
   629         *
   630         *  A profile is a collection of tool options used to create a
   631         *  library or executable that supports a certain "flavor" of library
   632         *  or executable; e.g., "debug" or "release".
   633         *
   634         *  Some profile names are supported by all targets even though the
   635         *  targets use different compilers (and therefore different options).
   636         *  These profile names makes it possible for a package to build
   637         *  libraries or executables in a "debug" (or "release") profile
   638         *  independent of the target, for example.
   639         *
   640         *  All targets are required to support "debug" and "release" profile
   641         *  names.
   642         *
   643         *  Profile options are added to beginning of any goal specific options
   644         *  specified by the user before being passed to the target.
   645         */
   646        config OptionSet profiles[string] = [
   647            ["release", {}],
   648            ["debug", {}],
   649        ];
   650        
   651        /*!
   652         *  ======== CompileGoal ========
   653         *  The goal specification passed to the `{@link #compile}`
   654         *  function.
   655         *
   656         *  @see #compile
   657         *  @see #scompile
   658         */
   659        struct CompileGoal {
   660            String base;        /*! base name of the source and destination */
   661            String dstPrefix;   /*! directory prefix of destination file */
   662            String dstSuffix;   /*! suffix of destination file; e.g., ".o62" */
   663            String srcSuffix;   /*! optional suffix of source file; e.g., ".c" */
   664            String srcPrefix;   /*! optional directory prefix of source file */
   665            String profile;     /*! index into profiles map */
   666            CompileOptions opts;/*! goal specific compiler options */
   667            Bool configOpts;    /*! true if compiling the generated C config file */
   668        };
   669    
   670        /*!
   671         *  ======== LinkGoal ========
   672         *  The goal specification passed to the `{@link #link}` function.
   673         *
   674         *  @see #link
   675         */
   676        struct LinkGoal {
   677            String base;        /*! base name of the source and destination */
   678            String dstPrefix;   /*! directory prefix of destination file */
   679            String dstSuffix;   /*! suffix of destination file; e.g., ".x62" */
   680            String files;       /*! string of files to link with */
   681            String profile;     /*! index into profiles map */
   682            String opts;        /*! goal specific linker options */
   683            Bool dllMode;       /*! true if we're linking an assembly */
   684            Bool isRom;         /*! reflects the `isRom` attribute */
   685        };
   686        
   687        /*!
   688         *  ======== ArchiveGoal ========
   689         *  The goal specification passed to the `{@link #archive}`
   690         *  function.
   691         *
   692         *  @see #archive
   693         */
   694        struct ArchiveGoal {
   695            String base;        /*! base name of the source and destination */
   696            String dstPrefix;   /*! directory prefix of destination file */
   697            String dstSuffix;   /*! suffix of destination file; e.g., ".a62" */
   698            String files;       /*! String of files to archive */
   699            String profile;     /*! index into profiles map */
   700            String opts;        /*! goal specific archiver options */
   701        };
   702        
   703        /*!
   704         *  ======== CommandSet ========
   705         *  The commands necessary to create a specified goal.
   706         *
   707         *  This structure is the return value of the `{@link #compile}`,
   708         *  `{@link #link}` and `{@link #archive}` functions.  This value is then
   709         *  used to generate a makefile or any other files necessary to generate
   710         *  a specified goal.
   711         *
   712         *  @field(msg)     a brief synopsis of the commands specified by `cmds`;
   713         *                  this string is output in lieu of `cmds` when building
   714         *                  in "non-verbose" mode.
   715         *
   716         *  @field(cmds)    a single string of commands that must be executed
   717         *                  to complete the specified operation.  Multiple
   718         *                  commands may be specified by separating each command
   719         *                  with the '\n' character.
   720         *
   721         *                  To facilitate the creation of "portable" makefiles and
   722         *                  to simplify the implementation of targets, certain
   723         *                  distinguished "macros" may be embedded in this string.
   724         *                  The build engine replaces these macros with the
   725         *                  values described below.
   726         *                  @p(dlist)
   727         *                      - `$(rootDir)`
   728         *                          the target's `{@link #rootDir}` configuration
   729         *                          parameter
   730         *                      - `$(packageBase)`
   731         *                          the target package's
   732         *                          `{@link xdc.IPackage#packageBase}` property
   733         *                      - `$(XDCINCS)`
   734         *                          a set of "-I" options that names each
   735         *                          repository in the package path
   736         *                  @p
   737         *
   738         *  @field(envs)    an array of "name=value" strings that represent
   739         *                  environment variables that are defined prior to the
   740         *                  execution of the commands specified by `cmds`
   741         *
   742         *  @field(path)    an array of directory names that are used to compose
   743         *                  the PATH environment variable that is in effect when
   744         *                  the commands specified by `cmds` are run.
   745         *
   746         *  @see #archive
   747         *  @see #compile
   748         *  @see #scompile
   749         *  @see #link
   750         */
   751        struct CommandSet {
   752            String msg;         /*! brief message describing subsequent commands */
   753            String cmds;        /*! commands necessary to generate goal */
   754            String path[];      /*! host-independent representation of PATH */
   755            String envs[];      /*! environment variable settings for the cmds */
   756        };
   757    
   758        /*!
   759         *  ======== archive ========
   760         *  Create an archive.
   761         *
   762         *  This function is called during makefile generation to convert build
   763         *  goals into specific commands that generate the specified goal.
   764         *
   765         *  @param(goal) the `{@link #ArchiveGoal}` defining the archive to build.
   766         *
   767         *  @a(returns)
   768         *  This function returns a `{@link #CommandSet}`.  If non-`null`, this
   769         *  object defines the commands that must be executed to create the
   770         *  specified object file.  If `null`, then goal can not be achieved. 
   771         *
   772         *  @a(throws)  `Error` exceptions are thrown for fatal errors.
   773         */
   774        CommandSet* archive(ArchiveGoal *goal);
   775    
   776        /*!
   777         *  ======== compile ========
   778         *  Compile a source file into an object file.
   779         *
   780         *  This function is called during makefile generation to convert build
   781         *  goals into specific commands that generate the specified object
   782         *  file goal.
   783         *
   784         *  @param(goal) a `{@link #CompileGoal}` that specifies what file to
   785         *               compile, the output file name, and any goal-specific
   786         *               options to use
   787         *
   788         *  @a(returns)
   789         *  This function retuns a `{@link #CommandSet}`.  If non-`null`,
   790         *  this object defines the commands that must be executed to create the
   791         *  specified object file.  If `null`, then goal can not be achieved. 
   792         *
   793         *  @a(throws)  `Error` exceptions are thrown for fatal errors.
   794         */
   795        CommandSet* compile(CompileGoal *goal);
   796    
   797        /*!
   798         *  ======== scompile ========
   799         *  Compile a source file into an assembly language file.
   800         *
   801         *  This function is called during makefile generation to convert build
   802         *  goals into specific commands that generate the specified assembly
   803         *  language source goal.
   804         *
   805         *  @param(goal) a `{@link #CompileGoal}` that specifies what file to
   806         *               compile, the output file name, and any goal-specific
   807         *               options to use
   808         *
   809         *  @a(returns)
   810         * This function returns a `{@link #CommandSet}`.  If non-`null`, this
   811         * object defines the commands that must be executed to create the
   812         * specified assembly language file.  If `null`, then goal
   813         * can not be achieved or is unnecessary (e.g., because
   814         * the source file is already an asm file).
   815         *
   816         *  @a(throws)  `Error` exceptions are thrown for fatal errors.
   817         */
   818        CommandSet* scompile(CompileGoal *goal);
   819    
   820        /*!
   821         *  ======== link ========
   822         *  Link object files to produce an executable.
   823         *
   824         *  This function is called during makefile generation to convert build
   825         *  goals into specific commands that generate the specified goal.
   826         *
   827         *  @param(goal) a `{@link #LinkGoal}` that specifies the output file
   828         *               name, a list of files to link with, and any goal-specific
   829         *               options to use
   830         *
   831         *  @a(returns)
   832         *  This function returns a `{@link #CommandSet}`.  If non-`null`, this
   833         *  object defines the commands that must be executed to create the
   834         *  specified object file.  If `null`, then goal can not be
   835         *  achieved. 
   836         *
   837         *  @a(throws)  `Error` exceptions are thrown for fatal errors.
   838         */
   839        CommandSet* link(LinkGoal *goal);
   840    
   841        /*!
   842         *  ======== getVersion ========
   843         *  Get a target-specific Compatibility Key string
   844         *
   845         *  This function is called during makefile generation to obtain a 
   846         *  target-specific Compatibility Key string.  This string is of the
   847         *  form:
   848         *  @p(code)
   849         *      "<pkg>.<mod>{<d0>,<d1>,<d2>,<d3>"
   850         *  @p
   851         *  where, `<pkg>.<mod>` is the name of the target, and `<d0>`, `<d1>`,
   852         *  etc. forms a Compatibility Key.
   853         *
   854         *  @a(returns)
   855         *  This function returns a string that encodes the name of the target
   856         *  and its Compatibility Key.
   857         *
   858         *  @a(throws)  `Error` exceptions are thrown for fatal errors.
   859         */
   860        String getVersion();
   861    
   862        typedef String StringArray[];
   863    
   864        /*!
   865         *  ======== getISAChain ========
   866         *  Get this target's ISA "is compatible with" relation.
   867         *
   868         *  Returns an array of ISA names (including this target's ISA) that
   869         *  represents the "is a" relation between ISA's.  The array starts with
   870         *  the most general ISA and ends with this target's ISA or with the
   871         *  optionally specified argument.  This relation is used to:
   872         *  @p(nlist)
   873         *      - pre-define macro definitions that enable code to be
   874         *        conditionally compiled based on compatible versions of a
   875         *        target's ISA.
   876         *
   877         *      - locate appropriate source files during makefile generation;
   878         *        each ISA named in a chain causes the extensions ".s"isa to be
   879         *        added to the ITarget.extensions table (in the reverse order
   880         *        that they appear in the chain).  For example, if a target's
   881         *        ISA is "64P" and the returned chain is ["62", "64", "64P"],
   882         *        the following assembly language suffixes are added to
   883         *        the target's extensions table: ".s64P", ".s64", ".s62".
   884         *
   885         *      - determine the assembly language suffix used during legacy BIOS
   886         *        configuration; the first element of the target's ISA chain
   887         *        defines the suffix.  For example, if a target's ISA is "64P"
   888         *        and the returned chain is ["62", "64", "64P"], the assembly
   889         *        suffix is ".s62".
   890         *  @p
   891         *
   892         *  This relation may also be used in the future to help validate
   893         *  combinations of targets and platforms; a target's CPU ISA must
   894         *  appear on the chain specified by the platform's CPU ISA.
   895         *
   896         *  @param(isa) the ISA identifier string for the ISA to lookup; if null
   897         *              then the target's ISA is used (ITarget.isa).
   898         *
   899         *  @a(returns)
   900         *  This function returns an array of ISA strings where the last string
   901         *  is the optionally specified ISA string or this target's ISA,
   902         *  and the first string is the "base" ISA in the
   903         *  is source compatible" relationship.
   904         *  If the specified ISA string is not in this target's chain
   905         *  of compatible targets, `null` is returned.
   906         *
   907         *  @a(throws)  `Error` exceptions are thrown for fatal errors.
   908         *  
   909         */
   910        function getISAChain(isa);
   911        
   912        /*!
   913         *  ======== findSuffix ========
   914         *  Find the suffix that is compatible with this target.
   915         *
   916         *  This function determines the list of targets supported by the
   917         *  package given as the argument. From that list, this function
   918         *  returns the suffix of a target that is compatible with this target.
   919         *  Compatibility in this case means that object files created by a
   920         *  target having the suffix returned by this function can be linked
   921         *  into an executable produced using this target. In the case where more
   922         *  than one suffix is compatible, this function returns a suffix in the
   923         *  following order of preference:
   924         *  @p(nlist)
   925         *      - if this target's suffix is in the list, that suffix is returned.
   926         *
   927         *      - suffixes from `compatibleSuffixes` are matched against the list
   928         *        from the first to the last, and the first one with the match is
   929         *        returned.
   930         *  @p
   931         *
   932         *  @param(pkg) a package object or an array of target suffix strings
   933         *              (see `{@link #suffix}`).
   934         *
   935         *  @a(returns)
   936         *  This function returns the suffix string of a target compatible with
   937         *  this target or `null` if `pkg` does not support any target compatible
   938         *  with this target.
   939         *
   940         */
   941        function findSuffix(pkg);
   942    
   943        /*!
   944         *  ======== selectSuffix ========
   945         *  Select the suffix that is compatible with this target.
   946         *
   947         *  From a list of suffixes supplied as an argument, this function
   948         *  returns the suffix compatible with this target. Compatibility in
   949         *  this case means that object files created by a target having the
   950         *  suffix returned by this function can be linked into an executable
   951         *  produced using this target. In the case where more than one suffix
   952         *  is compatible, this function returns a suffix in the following order
   953         *  of preference:
   954         *  @p(nlist)
   955         *      - if this target's suffix is in the list, that suffix is returned.
   956         *
   957         *      - suffixes from `compatibleSuffixes` are matched against the list
   958         *        from the first to the last, and the first one with the match is
   959         *        returned.
   960         *  @p
   961         *
   962         *  @param(suffixList)      an array of target suffix strings
   963         *                          (see `{@link #suffix}`).
   964         *
   965         *  @a(returns)
   966         *  This function returns the suffix string of a target compatible with
   967         *  this target or `null` if no such suffix is found in the list of
   968         *  suffixes specified by the first argument.
   969         *
   970         */
   971        String selectSuffix(StringArray suffixList);
   972    
   973        /*!
   974         *  ======== sectMap ========
   975         *  Output section name to segment type mapping
   976         *
   977         *  This hash table is used to determine whether a particular object file
   978         *  output section (".text", ".stack", etc.) requires 'data', 'code' or
   979         *  'stack' memory segment.
   980         *
   981         *  This `sectMap` is referenced by linker command file templates during
   982         *  generation to create linker command files. The Platform defines the
   983         *  default memory segments for code and data, and based on this map and
   984         *  the default segments, the linker command file template places an
   985         *  output section into a physical memory segment.
   986         *
   987         *  Note that the `{@link xdc.cfg.Program}` object and the
   988         *  `{@link xdc.platform.IPlatform}` instance have a
   989         *  `sectMap` parameter. Both the `Program`'s and `IPlatform`'s `sectMap`
   990         *  can augment and/or override the placement for a section, but
   991         *  `{@link xdc.cfg.Program#sectMap}` takes precedence. Therefore, this
   992         *  `sectMap` and the default segments from the platform define an
   993         *  initial section map which is then augmented by the `Program`'s and
   994         *  `IPlatform`'s section map.
   995         */
   996        readonly config String sectMap[string];
   997    
   998        /*!
   999         *  ======== TypeInfo ========
  1000         *  @_nodoc
  1001         *
  1002         *  @see #StdTypes
  1003         */
  1004        struct TypeInfo {
  1005            int size;
  1006            int align;
  1007        }
  1008    
  1009        /*!
  1010         *  ======== StdTypes ========
  1011         *  Standard base types supported by all targets
  1012         *
  1013         *  @see #stdTypes
  1014         */
  1015        struct StdTypes {
  1016            TypeInfo t_IArg;
  1017            TypeInfo t_Char;
  1018            TypeInfo t_Double;
  1019            TypeInfo t_Float;
  1020            TypeInfo t_Fxn;
  1021            TypeInfo t_Int;
  1022            TypeInfo t_Int8;
  1023            TypeInfo t_Int16;
  1024            TypeInfo t_Int32;
  1025            TypeInfo t_Int40;
  1026            TypeInfo t_Int64;
  1027            TypeInfo t_Long;
  1028            TypeInfo t_LDouble;
  1029            TypeInfo t_LLong;
  1030            TypeInfo t_Ptr;
  1031            TypeInfo t_Short;
  1032            TypeInfo t_Size;
  1033        }
  1034    
  1035        /*!
  1036         *  ======== stdInclude ========
  1037         *  Standard C/C++ types header
  1038         *
  1039         *  This string identifies a header containing the C/C++ definitions
  1040         *  required to enable use of `xdc/std.h` in C/C++ sources; see
  1041         *  `{@link xdc}`.
  1042         *
  1043         *  The value of this string is used by `xdc/std.h` to include
  1044         *  target-specific definitions of the types `Int8`, `Int16`, etc.  In
  1045         *  addition, this header supplies target-specific definitions of the
  1046         *  predefined `xdc_target__*` macros required by `{@link xdc xdc/std.h}`.
  1047         *
  1048         *  Since this header must supply target-specific values for
  1049         *  target-independent names the structure of this header is usually of
  1050         *  the form:
  1051         *  @p(code)
  1052         *      // if target macros are not already defined, 
  1053         *      #if !defined(xdc_target_macros_include__)
  1054         *          // include target-specific definitions
  1055         *          #if defined(TARGET1)
  1056         *              #include "target1.h"
  1057         *          #elif defined(TARGET2)
  1058         *              #include "target2.h"
  1059         *          #elif ...
  1060         *              :
  1061         *          #else
  1062         *              #error unsupported target
  1063         *          #endif
  1064         *      #endif
  1065         *      // include common definitions
  1066         *          :
  1067         *  @p
  1068         *  The check of the symbol `xdc_target_macros_include__` exists to
  1069         *  allow others that define new targets to include this header to
  1070         *  get common definitions for a family of related targets.
  1071         *
  1072         *  To simplify the creation of the target-specific header files, the
  1073         *  template file `stddefs.xdt` in this package can be used to
  1074         *  automatically generate the required definitions from each target's
  1075         *  `.xdc` specification.
  1076         */
  1077        readonly config String stdInclude;
  1078        
  1079        /*!
  1080         *  ======== stdTypes ========
  1081         *  Size and alignment for standard base types
  1082         *
  1083         *  The values of size are the values returned by the 
  1084         *  target-specific `sizeof()` operator applied to the specified
  1085         *  type (as defined by the C language).  The align value is the number
  1086         *  of chars used in the alignment of the specified type.
  1087         */
  1088        readonly config StdTypes stdTypes = {
  1089            t_IArg          : { size: 0, align: 0 },
  1090            t_Char          : { size: 0, align: 0 },
  1091            t_Double        : { size: 0, align: 0 },
  1092            t_Float         : { size: 0, align: 0 },
  1093            t_Fxn           : { size: 0, align: 0 },
  1094            t_Int           : { size: 0, align: 0 },
  1095            t_Int8          : { size: 0, align: 0 },
  1096            t_Int16         : { size: 0, align: 0 },
  1097            t_Int32         : { size: 0, align: 0 },
  1098            t_Int40         : { size: 0, align: 0 },
  1099            t_Int64         : { size: 0, align: 0 },
  1100            t_Long          : { size: 0, align: 0 },
  1101            t_LDouble       : { size: 0, align: 0 },
  1102            t_LLong         : { size: 0, align: 0 },
  1103            t_Ptr           : { size: 0, align: 0 },
  1104            t_Short         : { size: 0, align: 0 },
  1105            t_Size          : { size: 0, align: 0 },
  1106        };
  1107    
  1108        /*!
  1109         *  ======== bitsPerChar ========
  1110         *  The number of bits in a variable of type `char`
  1111         *
  1112         *  This constant allows one to determine the precise number of bits in
  1113         *  each of the types specified in the stdTypes map.  For example, the
  1114         *  number of bits in the target `T`'s `int` type is
  1115         *  @p(code)
  1116         *      T.stdTypes.t_Int.size * T.bitsPerChar
  1117         *  @p
  1118         */
  1119        readonly config Int bitsPerChar = 8;
  1120    }
  1121    /*
  1122     *  @(#) xdc.bld; 1, 0, 2,384; 6-27-2012 10:24:45; /db/ztree/library/trees/xdc/xdc-y30x/src/packages/
  1123     */
  1124