1    /*
     2     *  Copyright 2012 by Texas Instruments Incorporated.
     3     *
     4     */
     5    
     6    /*!
     7     *  ======== Main ========
     8     *  Command-line tool for generating eclipse plugins for RTSC content
     9     *
    10     *  The `plugingen` tool allows RTSC content producers to
    11     *  create eclipse plugins that allows their content to be 
    12     *  integrated in the CCS4 environment. As input, the tool requires 
    13     *  @p(blist)
    14     *      - a RTSC module implementing {@link xdc.tools.product.IProduct}
    15     *  @p
    16     *  Refer to {@link ./doc-files/ExampleProduct.xdc ExampleProduct}
    17     *  for an implementation of {@link xdc.tools.product.IProduct IProduct}.
    18     *
    19     *  The tool may also be used to generate starter examples that will showup 
    20     *  in the new project wizard. This is accomplished by implementing
    21     *  {@link xdc.tools.product.IProductTemplate IProductTemplate} and setting
    22     *  the {@link xdc.tools.product.IProduct#templateModule templateModule} 
    23     *  configuration parameter of the {@link xdc.tools.product.IProduct IProduct} 
    24     *  implementation to the name of the implementation module. 
    25     *  Refer to {@link ./doc-files/Examples.xdc Examples}
    26     *  for a sample implementation of {@link
    27     *  xdc.tools.product.IProductTemplate IProductTemplate}.
    28     *  
    29     *  The XGCONF product view maybe developed by implementing
    30     *  {@link xdc.tools.product.IProductView IProductView} and setting
    31     *  the {@link xdc.tools.product.IProduct#productViewModule productViewModule} 
    32     *  configuration parameter of the {@link xdc.tools.product.IProduct IProduct} 
    33     *  implementation to the name of the implementation module.
    34     *  Refer to {@link ./doc-files/ProductView.xdc ProductView.xdc} and 
    35     *  {@link ./doc-files/ProductView.xs ProductView.xs}
    36     *  for a sample implementation of {@link
    37     *  xdc.tools.product.IProductView IProductView}.
    38     *
    39     *  The tool operates on a product that is either specified by the `-p`
    40     *  option or is present in the folder from which the tool is executed.
    41     *  The tool will create the plugin in a sub-folder named `eclipse`
    42     *  in the output directory specified with `-o` option. If the `-o`
    43     *  option is not specified the plugin is created in the product root
    44     *  directory. 
    45     *  The tool will search the repositories specified in the module
    46     *  implementing {@link xdc.tools.product.IProduct} for RTSC platforms.
    47     *  This search can be disabled by specifying the`--disable_repo_search` 
    48     *  option. The user needs to ensure that the repositories are installed 
    49     *  in the product root directory before using the tool.
    50     *
    51     *  @a(Example)
    52     *  @p(code)
    53     *      xs xdc.tools.product.plugingen 
    54     *                      -p exampleprod_1_0_0_00
    55     *                      -m xdc.tools.product.plugingen.examples.ExampleProduct
    56     *  @p
    57     */
    58    metaonly module Main inherits xdc.tools.ICmd
    59    {
    60        override config String usage[] = [
    61            '[-p product_root_directory]',
    62            ' -m module',
    63            '[-o outdir]',
    64            '[-f pluginFragment]',
    65            '[--suppress_product_type_info]',
    66            '[--disable_repo_search]'
    67        ];
    68    
    69    instance:
    70    
    71        /*!
    72         *  ======== productDir ========
    73         *  Product root directory
    74         *
    75         *  This option names the product root directory that is used by the 
    76         *  tool to generate the plugin.  For example, it's declared repositories
    77         *  are added to the package path and are searched for contributed
    78         *  platforms.
    79         *
    80         *  If the '-o' option is not specified, the tool generates the plugin
    81         *  in a sub-directory named `eclipse` in the product root directory.
    82         *
    83         *  If this option is not specified, the product root directory is
    84         *  assumed to be `./`.
    85         *
    86         */
    87        @CommandOption("p")
    88        config String productDir = "./";
    89    
    90        /*!
    91         *  ======== productModule ========
    92         *  Input description of the plug-in to be specified
    93         *
    94         *  This required option names a module that implements
    95         *  `{@link xdc.tools.product.IProduct}`.
    96         */
    97        @CommandOption("m")
    98        config String productModule;
    99    
   100        /*!
   101         *  ======== outputDir ========
   102         *  Output directory in which the plugin will be generated.
   103         *
   104         *  This option names the directory in which the plugin 
   105         *  will be generated in a sub-directory named `eclipse`.
   106         *  If this option is not specified the tool will generate
   107         *  the plugin in the product root directory specified with
   108         *  the '-p' option.
   109         */
   110        @CommandOption("o")
   111        config String outputDir = null;
   112    
   113        /*!
   114         *  ======== pluginFragment ========
   115         *  Text file containing plugin fragment
   116         *
   117         *  This option names the text file containing a plugin fragment.
   118         *  This allows users to contribute extensions to the UI plugins
   119         *  generated by the tool.
   120         *
   121         *  The tool does not perform syntax checking of the contributed
   122         *  fragment. Users need to ensure the correctness of the 
   123         *  contributed fragment. Note that syntactically incorrect 
   124         *  fragments can disable the plugin completely in the eclipse 
   125         *  platform.
   126         */
   127        @CommandOption("f")
   128        config String pluginFragment = null;
   129    
   130        /*!
   131         *  ======== generationFormat ========
   132         *  Plugin generation format
   133         */
   134        @CommandOption("generation_format")
   135        config String generationFormat = null;
   136    
   137        /*!
   138         *  ======== suppress_product_type_info ========
   139         *  Suppress generation of product type information 
   140         *
   141         *  This option generates eclipse plugin without the product
   142         *  type information. Should only be invoked to generate plugins 
   143         *  whose product type information was hard coded into CCS 4.x prior
   144         *  to the creation of this tool.
   145         *
   146         *  This option should not be used by _any_ new products.
   147         */
   148        @CommandOption("suppress_product_type_info")
   149        config Bool suppressProductTypeInfo = false;
   150    
   151        /*!
   152         *  ======== disable_repo_search ========
   153         *  Suppress search of product repositories
   154         *
   155         *  If this option is specified the tool does not
   156         *  search the product repositories for RTSC platforms.
   157         */
   158        @CommandOption("disable_repo_search")
   159        config Bool suppressSearch = false;
   160            
   161        /*!
   162         *  ======== run ========
   163         */
   164        override Any run(xdc.tools.Cmdr.Instance cmdr, String args[]);
   165    }
   166    /*
   167     *  @(#) xdc.tools.product.plugingen; 1, 0, 0,68; 4-30-2012 14:28:11; /db/ztree/library/trees/xdctools/xdctools-f11x/src/
   168     */
   169