1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== Utils.xdc ========
    14     */
    15    package xdc.bld
    16    
    17    /*!
    18     *  ======== Utils ========
    19     *  Utility functions to simplify creation of targets and platforms
    20     */
    21    metaonly module Utils
    22    {
    23        /*!
    24         *  ======== expandString ========
    25         *  Expand references within a string to specified values
    26         *
    27         *  All references of the form "`$(<name>)`" within the command string,
    28         *  `cmd` are replaced with the string value having key `<name>` in the
    29         *  hashtable `values`.
    30         *
    31         *  If `<name>` appears in values and its value is `null` or `undefined`,
    32         *  then `$(<name>)` is replaced with the empty string.  If `<name>` does
    33         *  not appear in `values`, then `$(<name>)` is not replaced.
    34         *
    35         *  @param(cmd)     a string with embeded references to values defined in
    36         *                  the values hashtable parameter
    37         *  @param(values)  an arbitrary hash of name-value pairs; these values
    38         *                  are used to substitute for references of the form
    39         *                  `$(name)` that appear within `cmd`.
    40         *
    41         *  @a(returns)     string with references replaced as specified by the
    42         *                  `values` hash.
    43         *
    44         *  @a(throws)      `Error` exceptions are thrown for fatal errors
    45         */
    46        String expandString(String cmd, Any values);
    47    
    48        /*!
    49         *  ======== expandDbgName ========
    50         *  Generate name of a debug support output file
    51         *
    52         *  @param(cfgName) the name of the generated configuration script
    53         *                  without the ".cfg" extension
    54         *  @param(exeName) the name of the output executable
    55         *  @param(pattern) file name pattern
    56         *
    57         *  Both cfgName and exeName are relative to the directory containing
    58         *  package.bld.
    59         *
    60         *  @_nodoc this function is an internal method shared between xdc.bld
    61         *  and xdc.cfg and has little value outside this context.
    62         */
    63        function expandDbgName(cfgName, exeName, pattern);
    64        
    65        /*!
    66         *  ======== parsePlatName ========
    67         *  Parse platform instance name into platform package name and short
    68         *  instance name
    69         *
    70         *  @param(platInstName)     the name of a platform instance
    71         *
    72         *  @a(returns)
    73         *  returns object with the following fields:
    74         *  @p(dlist)
    75         *      - `platPkgName`
    76         *              name of the platform package name
    77         *      - `instName`
    78         *              name of the platform instance
    79         *      - `instMod`
    80         *              module object specifying platform instances (if it exists)
    81         * @p
    82         *
    83         *  @a(throws)      `Error` exceptions are thrown for fatal errors
    84    
    85         *  @_nodoc this function is an internal method shared between xdc.bld
    86         *  and xdc.cfg and has little value outside this context.
    87         */
    88        function parsePlatName(platInstName);
    89    
    90        /*!
    91         *  ======== display ========
    92         *  Recursively print arbitrary object
    93         *
    94         *  @param(msg)  a string to print before printing the object
    95         *  @param(obj)  an arbitrary object to display
    96         */
    97        Void display(String msg, Any obj);
    98    }
    99    /*
   100     *  @(#) xdc.bld; 1, 0, 2,384; 6-27-2012 10:24:46; /db/ztree/library/trees/xdc/xdc-y30x/src/packages/
   101     */
   102