1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== ITimestampClient.xdc ========
15 */
16 package xdc.runtime;
17
18 /*!
19 * ======== ITimestampClient ========
20 * Timestamp Client Interface
21 *
22 * This interface defines the methods used by client applications to
23 * get timestamp values. It is implemented by the
24 * `{@link xdc.runtime.Timestamp Timestamp}` module.
25 */
26 interface ITimestampClient {
27
28 /*!
29 * ======== get32 ========
30 * Return a 32-bit timestamp
31 *
32 * @a(returns) 33 * Returns a 32-bit timestamp value.
34 * Use `{@link #getFreq}` to convert this value into units of real time.
35 *
36 * @see #get64
37 */
38 Bits32 get32();
39
40 /*!
41 * ======== get64 ========
42 * Return a 64-bit timestamp
43 *
44 * @param(result) pointer to 64-bit result
45 *
46 * This parameter is a pointer to a structure representing a 64-bit
47 * wide timestamp value where the current timestamp is written.
48 *
49 * If the underlying hardware does not support 64-bit resolution, the
50 * `hi` field of `result` is always set to 0; see
51 * `{@link xdc.runtime.Types#Timestamp64}`. So, it is possible for
52 * the `lo` field to wrap around without any change to the `hi` field.
53 * Use `{@link #getFreq}` to convert this value into units of real
54 * time.
55 *
56 * @see #get32
57 */
58 Void get64(Types.Timestamp64 *result);
59
60 /*!
61 * ======== getFreq ========
62 * Get the timestamp timer's frequency (in Hz)
63 *
64 * @param(freq) pointer to a 64-bit result
65 *
66 * This parameter is a pointer to a structure representing a 64-bit
67 * wide frequency value where the timer's frequency (in Hz)
68 * is written; see `{@link xdc.runtime.Types#FreqHz}`.
69 * This function provides a way of converting timestamp
70 * values into units of real time.
71 *
72 * @see #get32
73 * @see #get64
74 */
75 Void getFreq(Types.FreqHz *freq);
76 }
77 /*
78 * @(#) xdc.runtime; 2, 1, 0,375; 4-27-2012 14:30:33; /db/ztree/library/trees/xdc/xdc-y25x/src/packages/
79 */
80