1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*!
14 * ======== IInstance ========
15 * Common instance params
16 *
17 * Every module's instance parameter structure contains a pointer to an
18 * `IInstance.Params` structure named `instance`. So, every instance
19 * parameter defined in this interface may optionally be set when
20 * creating (or constructing) any module's instances.
21 */
22 interface IInstance {
23
24 instance:
25
26 /*!
27 * ======== name ========
28 * Name of the instance
29 *
30 * It is possible to "bind" a name to each instance of any module
31 * at the time the instance is created (or constructed).
32 * @p(code) 33 * ModA_Params params;
34 * ModA_Params_init(¶ms);
35 * params.instance->name = "myInstance";
36 * ModA_create(¶ms, NULL);
37 * @p 38 *
39 * The name field must be assigned a pointer to a buffer that persists
40 * as long as the instance that it names exists. Only a reference to
41 * the name is retained in the instance, the name is not copied to a
42 * secondary buffer.
43 *
44 * The configuration parameters that controls if instance names are
45 * supported is `common$.namedInstance`. The parameter is a member of the
46 * structure `{@link xdc.runtime.Types#Common$ common$}`, available in each
47 * module. By default, this parameter is set to `false`, which disables
48 * support for instance names.
49 * Therefore, to enable instance names for a given module `Mod`, configure
50 * the module as follows in your configuration script:
51 * @p(code) 52 * var Mod = xdc.useModule('pkg.Mod');
53 * ModA.common$.namedInstance = true;
54 * @p 55 *
56 * Here is how the static instances are given names at the configuration
57 * time:
58 * @p(code) 59 * var inst = Mod.create();
60 * inst.instance.name = "myInstance";
61 * @p 62 *
63 * At runtime, assign your instance a name:
64 * @p(code) 65 * #include <package/name/Mod.h>
66 * Mod_Params params;
67 * Mod_Params_init(¶ms);
68 * params.instance->name = "myInstance";
69 * Mod_create(¶ms, NULL);
70 * @p 71 *
72 * If instances have been configured to not support names, it is still
73 * possible to assign to the `instance.name` field of the parameter
74 * structure (as shown above). However, the pointer is not retained
75 * and methods that normally return an instance's name will return
76 * `NULL` instead.
77 */
78 config String name = null;
79 }
80 /*
81 * @(#) xdc.runtime; 2, 1, 0,375; 4-27-2012 14:30:33; /db/ztree/library/trees/xdc/xdc-y25x/src/packages/
82 */
83