1 /*
2 * Copyright (c) 2012 by Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12
13 /*
14 * ======== Boot.xdc ========
15 *
16 */
17
18 package ti.catalog.c2800.init;
19
20 import xdc.rov.ViewInfo;
21
22 /*!
23 * ======== Boot ========
24 * 28x Boot Support.
25 *
26 * The Boot module supports boot initialization for the 28x devices.
27 * A special boot init function is created based on the configuration
28 * settings for this module. This function is hooked into the
29 * xdc.runtime.Reset.fxns[] array and called very early at boot time (prior
30 * to cinit processing).
31 *
32 * The code to support the boot module is placed in a separate section
33 * named `".text:.bootCodeSection"` to allow placement of this section in
34 * the linker .cmd file if necessary. This section is a subsection of the
35 * `".text"` section so this code will be placed into the .text section unless
36 * explicitly placed, either through
37 * `{@link xdc.cfg.Program#sectMap Program.sectMap}` or through a linker
38 * command file.
39 */
40 @Template("./Boot.xdt")
41 @NoRuntime
42 module Boot
43 {
44 /*! PLL type */
45 metaonlyenum Type {
46 Type_280x, /*! 280x (PLL configuration not supported for this type) */
47 Type_281x, /*! 281x (PLL configuration not supported for this type) */
48 Type_282xx_283xx, /*! 282xx or 283xx */
49 Type_2802x_2803x_2806x, /*! 2802x or 2803x or 2806x */
50 Type_2834x /*! 2834x */
51 };
52
53 metaonlystruct ModuleView {
54 Bool disableWatchdog;
55 Bool configurePll;
56 UInt pllcrDIV;
57 UInt pllstsDIVSEL;
58 }
59
60 @Facet
61 metaonlyconfig ViewInfo.Instance rovViewInfo =
62 ViewInfo.create({
63 viewMap: [
64 [
65 'Module',
66 {
67 type: ViewInfo.MODULE,
68 viewInitFxn: 'viewInitModule',
69 structName: 'ModuleView'
70 }
71 ],
72 ]
73 });
74
75 /*!
76 * Watchdog disable flag, default is false.
77 *
78 * Set to true to disable the watchdog timer.
79 */
80 metaonlyconfig Bool disableWatchdog = false;
81
82 /*!
83 * PLL type.
84 *
85 * The default will be determined by platform specification, or by the
86 * device ID for the generic (tms320c28) platform.
87 */
88 metaonlyconfig Type pllType;
89
90 /*!
91 * PLL configuration flag, default is false.
92 *
93 * Set to true to configure the PLL.
94 */
95 metaonlyconfig Bool configurePll = false;
96
97 /*!
98 * OSCCLK input frequency to PLL, in MHz. Default is 10 MHz.
99 *
100 * This is the frequency of the oscillator clock (OSCCLK) input to the
101 * PLL. On some devices (e.g., TMS320C28346) this will correspond to the
102 * frequency of an external crystal or clock input. On others
103 * (e.g., TMS320F28069) this will correspond to the frequency of an
104 * internal oscillator which is the default OSCCLK coming out of reset.
105 */
106 metaonlyconfig UInt pllOSCCLK = 10;
107
108 /*!
109 * PLLCR[DIV] clocking ratio value. Default is 10.
110 *
111 * This is the actual value written to the DIV bits in
112 * the PLL Control Register (PLLCR)
113 */
114 metaonlyconfig UInt pllcrDIV = 10;
115
116 /*!
117 * PLLSTS[DIVSEL] divide select value. Default is 2.
118 *
119 * This is the actual value written to the DIVSEL bits in
120 * the PLL Status Register (PLLSTS).
121 *
122 * This configuration parameter applies for all of the
123 * enumerated PLL types, except for "Type_280x".
124 */
125 metaonlyconfig UInt pllstsDIVSEL = 2;
126
127 /*!
128 * Function to be called when Limp mode is detected.
129 *
130 * This function is called when the Boot module is about to configure
131 * the PLL, but finds the device operating in Limp mode (i.e., the mode
132 * when a missing OSCCLK input has been detected).
133 *
134 * If this function is not specified by the application, a default
135 * function will be used, which does an ESTOP0 and then enters an
136 * infinite loop.
137 */
138 metaonlyconfig Fxn limpAbortFunction;
139
140 /*!
141 * Boot from FLASH flag, default is false.
142 *
143 * Set to true to enable booting from FLASH. When set to true,
144 * a long branch (LB) to the c_int00 entry point will be placed at
145 * the BEGIN section address defined in the linker command file.
146 */
147 metaonlyconfig Bool bootFromFlash = false;
148
149 /*!
150 * Configure the external memory interface (XINTF) for eZdsp283xx
151 * boards.
152 *
153 * This external memory interface configuration is applicable only for
154 * eZdsp283xx boards; it should not be enabled for any other boards.
155 */
156 metaonlyconfig Bool enableEzdspXintfConfig = false;
157
158 /*!
159 * @_nodoc 160 * Default abort function to be called when PLL Limp mode is detected
161 */
162 metaonly Void defaultLimpAbort();
163
164 /*!
165 * ======== getFrequency ========
166 * Gets the resulting output frequency (in Hz) given the PLL configuration
167 * parameters.
168 */
169 metaonly UInt32 getFrequency();
170
171 /*!
172 * ======== registerFreqListener ========
173 * Register a module to be notified whenever the frequency changes.
174 *
175 * The registered module must have a function named 'fireFrequencyUpdate'
176 * which takes the new frequency as an argument.
177 */
178 metaonlyfunction registerFreqListener(listener);
179
180 internal:
181
182 /* Used to display the computed frequency value in the Grace page. */
183 metaonlyconfig String displayFrequency;
184
185 /* Used to indicate if using on a Concerto device */
186 metaonlyconfig Bool concertoDevice = false;
187
188 };
189 /*
190 * @(#) ti.catalog.c2800.init; 1, 0, 0,243; 4-24-2012 14:55:58; /db/ztree/library/trees/platform/platform-n20x/src/
191 */
192