1 /*
2 * Copyright (c) 2008 Texas Instruments. All rights reserved.
3 * This program and the accompanying materials are made available under the
4 * terms of the Eclipse Public License v1.0 and Eclipse Distribution License
5 * v. 1.0 which accompanies this distribution. The Eclipse Public License is
6 * available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
7 * Distribution License is available at
8 * http://www.eclipse.org/org/documents/edl-v10.php.
9 *
10 * Contributors:
11 * Texas Instruments - initial implementation
12 * */
13 /*
14 * ======== Log.xdc ========
15 */
16
17 /*!
18 * ======== Log ========
19 * Event logging manager
20 *
21 * RTSC modules and the application code generate `{@link #Event Log_Event}`
22 * events by calling the `Log` module's functions. The `Log` module then
23 * passes those events to an `{@link ILogger}` instance assigned to the event
24 * originating module, specified by that module's configuration parameter
25 * `common$.logger`. `ILogger` instances handle events, usually converting
26 * events to `{@link #EventRec Log_EventRec}` records prior to recording,
27 * transmitting, or displaying them.
28 *
29 * All events generated by a target module are stored and displayed by an
30 * `ILogger`, examples of which are instances of
31 * `{@link LoggerBuf xdc.runtime.LoggerBuf}` or
32 * `{@link LoggerSys xdc.runtime.LoggerSys}`. At runtime, modules
33 * generate events through this module, rather than invoking directly their
34 * `ILogger`s. By doing so, modules can be configured to use different
35 * `ILogger` implementations without any changes to their source code.
36 *
37 * A logger instance can accept `Log` events from any module, but a module
38 * can put `Log` events to only one logger instance. There can be one or
39 * more logger instances in a system. All `Log` calls that are not in a
40 * module are controlled by the module `{@link Main xdc.runtime.Main}`.
41 * For example, top-level application code or any existing sources that
42 * simply call the `Log` or `Assert` methods implicitly use the logger
43 * associated with the `Main` module.
44 *
45 * The generation of a `Log` event is controlled by a module's diagnostics
46 * mask, which is described in details in `{@link Diags}`. Each `Log` event
47 * is associated with a mask. `Log` events are generated only when a
48 * particular bit is set in both the `Log` event mask
49 * and the module's diagnostics mask. For example, a `Log` event mask with
50 * the `{@link Diags#USER1 USER1}` bit set is generated only when the `USER1`
51 * bit is also set in the module's diagnostics mask.
52 *
53 * There are two ways to generate `Log` events:
54 *
55 * @p(blist) 56 * - `{@link #write8 Log_write()}`, which is tailored for module writers
57 * and takes full advantage of the XDC configuration model. For example,
58 * the message string associated with the `Log` event need not be a part of
59 * the final application, significantly reducing the "footprint overhead"
60 * of embedding diagnostics in deployed systems. The `Log_write[0-8]()`
61 * functions allow up to 8 values to be passed to the logger. They expect
62 * the logger to handle any formatting. A `Log` event type allows you to
63 * specify the type of event.
64 * - `{@link #print6 Log_print()}`, which is designed for arbitrary C code.
65 * The `Log_print[0-6]()` functions allow up to 6 values to be passed along
66 * with a printf-like format string to the logger. They handle printf-style
67 * formatting.
68 * @p 69 *
70 * Both functions are controlled by the module's diagnostics mask. Their
71 * storage or output is defined by the logger that is assigned to the
72 * module that calls the `Log` methods or to the
73 * `{@link Main xdc.runtime.Main}` module if the caller is not part of a
74 * module.
75 *
76 * The `Log` function call sites are implemented in such a way that an
77 * optimizer can completely eliminate `Log` code from the program if the
78 * `Log` functions have been permanently disabled at configuration time. If
79 * the `Log` functions are permanently turned on at configuration time,
80 * then the optimizer can eliminate all runtime conditional checking and
81 * simply invoke the `Log` functions directly. Runtime checking is performed
82 * only when the `Log` functions are configured to be runtime modifiable.
83 *
84 * The Log calls can also be completely removed by defining the symbol
85 * `xdc_runtime_Log_DISABLE_ALL`. This can be done on the compile line, e.g.
86 * `-Dxdc_runtime_Log_DISABLE_ALL`. This will completely remove the `Log`
87 * statements from any code compiled with this flag, regardless of the
88 * application's logging configuration or your compiler's optimization
89 * settings.
90 *
91 * It is also possible to remove all logging except for
92 * `{@link #error Log_error}`, `{@link #warning Log_warning}`, or
93 * `{@link #info Log_info}` statements. This is done by first defining
94 * `xdc_runtime_Log_DISABLE_ALL`, followed by defining one or more of the
95 * symbols below to leave that type of logging enabled:
96 * @p(blist) 97 * - `xdc_runtime_Log_ENABLE_ERROR`
98 * - `xdc_runtime_Log_ENABLE_WARNING`
99 * - `xdc_runtime_Log_ENABLE_INFO`
100 * @p 101 * For example, to disable all `Log` statements except for `Log_error`, add
102 * the following to the compile line:
103 * @p(code) 104 * -Dxdc_runtime_Log_DISABLE_ALL -Dxdc_runtime_Log_ENABLE_ERROR
105 * @p 106 *
107 * @a(Examples) 108 * Example 1: The following example defines a `Log` event, uses that `Log`
109 * event in a module, and configures the program to generate the `Log`
110 * event. In this example, both `USER1` and `USER2` bits are set in the
111 * event mask. This means that if either bit is set in the module's
112 * diagnostics mask, then the `Log` event will be generated.
113 *
114 * This is a part of the XDC specification file for the `Mod` module
115 * (Mod.xdc):
116 *
117 * @p(code) 118 * import xdc.runtime.Diags;
119 * import xdc.runtime.Log;
120 *
121 * config Log.Event L_someEvent = {
122 * mask: Diags.USER1 | Diags.USER2,
123 * level: Diags.LEVEL1,
124 * msg: "my log event message, arg1: 0x%x, arg2: 0x%x"
125 * };
126 * @p 127 *
128 * This is a part of the C code implementation of the Mod module:
129 *
130 * @p(code) 131 * #include <xdc/runtime/Log.h>
132 * UInt x, y;
133 *
134 * Log_write2(Mod_L_someEvent, (IArg)x, (IArg)y);
135 * @p 136 *
137 * The following configuration script demonstrates how the application might
138 * control the `Log` statements embedded in the `Mod` module at configuration
139 * time. In this case, the configuration script arranges for the `Log`
140 * statements within the `Mod` module (shown above) to always generate events.
141 * Without these configuration statements, no `Log` events would be generated
142 * by this module.
143 *
144 * This is part of the XDC configuration file for the application:
145 *
146 * @p(code) 147 * var Diags = xdc.useModule('xdc.runtime.Diags');
148 * var LoggerSys = xdc.useModule('xdc.runtime.LoggerSys');
149 * var Mod = xdc.useModule('my.pkg.Mod');
150 * Mod.common$.diags_USER1 = Diags.ALWAYS_ON;
151 * Mod.common$.logger = LoggerSys.create();
152 * @p 153 *
154 * @p(html) 155 * <hr />
156 * @p 157 *
158 * Example 2: The following XDC configuration statements turn on enter
159 * and exit logging at configuration time for a module. Without any other
160 * changes in the runtime code, every time a module `Mod`'s function is
161 * being called or exits, an event will be logged.
162 *
163 * @p(code) 164 * var Diags = xdc.useModule('xdc.runtime.Diags');
165 * var Mod = xdc.useModule('my.pkg.Mod');
166 *
167 * Mod.common$.diags_ENTER = Diags.ALWAYS_ON;
168 * Mod.common$.diags_EXIT = Diags.ALWAYS_ON;
169 * @p 170 *
171 * @p(html) 172 * <hr />
173 * @p 174 *
175 * Example 3: The following example configures a module to support enter and
176 * exit logging, but defers the actual activation and deactivation of the
177 * logging until runtime. See the `{@link Diags#setMask Diags_setMask()}`
178 * function for details on specifying the control string.
179 *
180 * This is a part of the XDC configuration file for the application:
181 *
182 * @p(code) 183 * var Diags = xdc.useModule('xdc.runtime.Diags');
184 * var Mod = xdc.useModule('my.pkg.Mod');
185 *
186 * Mod.common$.diags_ENTER = Diags.RUNTIME_OFF;
187 * Mod.common$.diags_EXIT = Diags.RUNTIME_OFF;
188 * @p 189 *
190 * This is a part of the C code for the application:
191 *
192 * @p(code) 193 * // turn on enter and exit logging in the module
194 * Diags_setMask("my.pkg.Mod+EX");
195 *
196 * // turn off enter and exit logging in the module
197 * Diags_setMask("my.pkg.Mod-EX");
198 * @p 199 */
200
201 @CustomHeader
202
203 module Log {
204
205 /*!
206 * ======== NUMARGS ========
207 * Maximum number of arguments supported in `Log` events.
208 */
209 const Int NUMARGS = 8;
210
211 /*!
212 * ======== PRINTFID ========
213 * The `EventId` for `Log_print()` events
214 */
215 const EventId PRINTFID = 0;
216
217 /*!
218 * ======== EventDesc ========
219 * `Log` event descriptor
220 *
221 * Each `Log` event is defined by a `Log` event descriptor.
222 *
223 * The `mask` defines which bits in the module's diagnostics mask
224 * enable this `Log` event. Events "posted" via `Log_write` are only
225 * written to the underlying logger if one of the mask's bits matches
226 * the caller's module diagnostics settings (see
227 * `{@link xdc.runtime.Types#common$}`).
228 *
229 * The 'level' defines the event level of the event. While the diags
230 * bits selected in the 'mask' signify the "category" of the event (e.g.
231 * Entry/Exit, Analysis, Info), the 'level' field allows you to assign
232 * a "priority" or "detail level" to the event relative to other events in
233 * that category. There are four event levels defined by
234 * '{@link xdc.runtime.Diags#EventLevel}'.
235 *
236 * Filtering of events by level is handled by the ILogger implementation.
237 * ILogger implementations which also implement the {@link IFilterLogger}
238 * interface support filtering of events based on priority level.
239 *
240 * Specifying an event level is optional. Events that don't specify a
241 * level will receive Diags.LEVEL1 by default, making them the highest
242 * priority and ensuring that they will not inadvertently be filtered out
243 * by level-based filtering.
244 *
245 * The `msg` defines a printf style format string that defines how to
246 * render the arguments passed along the event in a `Log_write` call.
247 * For a description of the allowable format strings see
248 * `{@link #print6}`.
249 *
250 * @see #write8
251 * @see #print6
252 */
253 metaonlystruct EventDesc {
254 Diags.Mask mask; /*! event enable mask */
255 Diags.EventLevel level; /*! event level relative to other events */
256 String msg; /*! event "printf" message format string */
257 };
258
259 /*!
260 * ======== EventRec ========
261 * The target representation of a recorded event
262 *
263 * This structure defines how events are recorded on the target.
264 */
265 struct EventRec {
266 Types.Timestamp64 tstamp; /*! time event was written */
267 Bits32 serial; /*! serial number of event */
268 Types.Event evt; /*! target encoding of an Event */
269 IArg arg[NUMARGS]; /*! arguments passed via Log_write/print */
270 }
271
272 /*!
273 * ======== Event ========
274 * `Log` event type
275 *
276 * An `Event` is represented on the target as a 32-bit value that can
277 * be decoded offline to recover the `Event` information defined in
278 * a corresponding metaonly `EventDesc`. In addition, `Event`s may be
279 * decoded at runtime via methods provided in this module; see
280 * `{@link #getMask}` and `{@link #getEventId}`.
281 *
282 * When an event is "raised" a `{@link Types#Event Types_Event}` is
283 * created which has the same event ID as the `Log_Event` but also
284 * encodes the module ID of the caller. This new event is passed to
285 * the underlying `{@link ILogger}` module along with any arguments
286 * associated with the event.
287 *
288 * @see #getMask
289 * @see #getEventId
290 */
291 @Encoded typedef EventDesc Event;
292
293 /*!
294 * ======== EventId ========
295 * Unique ID embedded in each `{@link #Event}`
296 *
297 * This ID must be used to compare two `Event`s for equality. Event
298 * ids are not guaranteed to remain constant between different
299 * configurations of an application. For example, adding a module
300 * may cause the event ids of another module to change.
301 *
302 * However, event ids declared by a module are guaranteed to be
303 * consecutive values starting from the first declared
304 * `{@link #Event Log_Event}` and increasing to the last declared
305 * event. As a result, clients of a module can efficiently test ranges
306 * of events and modules can add new events, such as internal trace
307 * events, without breaking clients; simply be careful to add new events
308 * after any existing events in you module's `.xdc` specification.
309 *
310 * @see #getEventId
311 * @see #Event
312 */
313 typedef Types.RopeId EventId;
314
315 /*!
316 * ======== L_construct ========
317 * Lifecycle event posted when an instance is constructed
318 */
319 config Log.Event L_construct = {
320 mask: Diags.LIFECYCLE,
321 msg: "<-- construct: %p('%s')"
322 };
323
324 /*!
325 * ======== L_create ========
326 * Lifecycle event posted when an instance is created
327 */
328 config Log.Event L_create = {
329 mask: Diags.LIFECYCLE,
330 msg: "<-- create: %p('%s')"
331 };
332
333 /*!
334 * ======== L_destruct ========
335 * Lifecycle event posted when an instance is destructed
336 */
337 config Log.Event L_destruct = {
338 mask: Diags.LIFECYCLE,
339 msg: "--> destruct: (%p)"
340 };
341
342 /*!
343 * ======== L_delete ========
344 * Lifecycle event posted when an instance is deleted
345 */
346 config Log.Event L_delete = {
347 mask: Diags.LIFECYCLE,
348 msg: "--> delete: (%p)"
349 };
350
351 /*!
352 * ======== L_error ========
353 * Error event posted by Log_errorX API
354 *
355 * This event is marked as a STATUS event and given the priority level
356 * of ERROR.
357 *
358 * This event prints the Log call site (%$F) and a format string (%$S)
359 * which is recursively formatted with any additional arguments.
360 */
361 config Log.Event L_error = {
362 mask: Diags.STATUS,
363 level: Diags.ERROR,
364 msg: "ERROR: %$F%$S"
365 };
366
367 /*!
368 * ======== L_warning ========
369 * Warning event posted by Log_warningX API
370 *
371 * This event is marked as a STATUS event and given the priority level of
372 * WARNING.
373 *
374 * This event prints the Log call site (%$F) and a format string (%$S)
375 * which is recursively formatted with any addition arguments.
376 */
377 config xdc.runtime.Log.Event L_warning = {
378 mask: Diags.STATUS,
379 level: Diags.WARNING,
380 msg: "WARNING: %$F%$S"
381 };
382
383 /*!
384 * ======== L_info ========
385 * Info event posted by Log_infoX API
386 *
387 * This event is marked as an INFO event. The event priority is not
388 * specified in the event definition. Rather, it is specified as an
389 * argument to the Log_infoX APIs.
390 *
391 * This event prints the Log call site (%$F) and a format string (%$S)
392 * which is recursively formatted with any addition arguments.
393 */
394 config xdc.runtime.Log.Event L_info = {
395 mask: Diags.INFO,
396 msg: "%$F%$S"
397 };
398
399 /*!
400 * ======== L_start ========
401 * Benchmark event used to log the start of an operation
402 * @_nodoc 403 *
404 * @a(Example) 405 * The following C code shows how to log a simple
406 * benchmark 'start' event along with a user-specified
407 * format string describing the event.
408 *
409 * @p(code) 410 * #include <xdc/runtime/Log.h>
411 * ...
412 * Log_write2(Log_L_start, (IArg)"My benchmark event", (IArg)myUniqueId);
413 * Log_write2(Log_L_stop, (IArg)"My benchmark event", (IArg)myUniqueId);
414 * @p 415 * @param(fmt) a constant string that provides format specifiers for up to 6 additional parameters
416 * @param(id) a unique ID used to match benchmark start and stop events
417 */
418 config xdc.runtime.Log.Event L_start = {
419 mask: Diags.ANALYSIS,
420 msg: "Start: %$S"};
421
422 /*!
423 * ======== L_stop ========
424 * Benchmark event used to log the end of an operation
425 * @_nodoc 426 *
427 * @a(Example) 428 * The following C code shows how to log a simple
429 * benchmark 'stop' event along with a user-specified
430 * format string describing the event.
431 *
432 * @p(code) 433 * #include <xdc/runtime/Log.h>
434 * ...
435 * Log_write2(Log_L_start, (IArg)"My benchmark event", (IArg)myUniqueId);
436 * Log_write2(Log_L_stop, (IArg)"My benchmark event", (IArg)myUniqueId);
437 * @p 438 * @param(fmt) a constant string that provides format specifiers for up to 6 additional parameters
439 * @param(id) a unique ID used to match benchmark start and stop events
440 */
441 config xdc.runtime.Log.Event L_stop = {
442 mask: Diags.ANALYSIS,
443 msg: "Stop: %$S"};
444
445 /*!
446 * ======== L_startInstance ========
447 * Benchmark event used to log the start of an operation instance
448 * @_nodoc 449 *
450 * Event parameter provides instance data to differentiate
451 * between multiple instances that can run in parallel.
452 *
453 * @a(Example) 454 * The following C code shows how to log a benchmark
455 * 'startInstance' event along with a user-specified
456 * instance identifier and a format string describing the event.
457 *
458 * @p(code) 459 * #include <xdc/runtime/Log.h>
460 * ...
461 * Log_write3(Log_L_startInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
462 * ...
463 * Log_write3(Log_L_stopInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
464 * @p 465 * @param(fmt) a constant string that provides format specifiers for up to 6 additional parameters
466 * @param(id) a unique ID used to match benchmark start and stop events
467 * @param(instId) a unique instance ID that can be used to match and instance
468 */
469 config xdc.runtime.Log.Event L_startInstance = {
470 mask: Diags.ANALYSIS,
471 msg: "StartInstance: %$S"
472 };
473
474 /*!
475 * ======== L_stopInstance ========
476 * Benchmark event used to log the end of an operation instance
477 * @_nodoc 478 *
479 * Event parameter provides instance data to differentiate
480 * between multiple instances that can run in parallel.
481 *
482 * @a(Example) 483 * The following C code shows how to log a benchmark
484 * 'stopInstance' event along with a user-specified
485 * instance identifier and a format string describing the event.
486 *
487 * @p(code) 488 * #include <xdc/runtime/Log.h>
489 * ...
490 * Log_write3(Log_L_startInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
491 * ...
492 * Log_write3(Log_L_stopInstance, (IArg)"My benchmark event", (IArg)uniqueId, (IArg)instId);
493 * @p 494 * @param(fmt) a constant string that provides format specifiers for up to 6 additional parameters
495 * @param(id) a unique ID used to match benchmark start and stop events
496 * @param(instId) a unique instance ID that can be used to match and instance
497 */
498 config xdc.runtime.Log.Event L_stopInstance = {
499 mask: Diags.ANALYSIS,
500 msg: "StopInstance: %$S"
501 };
502
503 /*!
504 * ======== getMask ========
505 * Get the `Diags` mask for the specified (encoded) event
506 *
507 * @param(evt) the `Log` event encoding a mask and event ID
508 *
509 * @a(returns) `Diags` mask for the specified event
510 */
511 @Macro Diags.Mask getMask(Event evt);
512
513 /*!
514 * ======== getRope ========
515 * Get RopeId of the Event.msg for the specified (encoded) event
516 * @_nodoc 517 */
518 @Macro Text.RopeId getRope(Event evt);
519
520 /*!
521 * ======== getEventId ========
522 * Get event ID of the specified (encoded) event
523 *
524 * This method is used to compare "known" `Log` events with
525 * "raised" `{@link Types#Event Types_Event}`.
526 *
527 * @param(evt) the `Log` event encoding a mask and event ID
528 *
529 * @a(returns) event ID of the specified event
530 *
531 * @see Types#getEventId
532 */
533 @Macro EventId getEventId(Event evt);
534
535 /*!
536 * ======== print0 ========
537 * Generate a `Log` "print event" with 0 arguments
538 *
539 * @see #print6
540 */
541 @Macro Void print0(Diags.Mask mask, String fmt);
542
543 /*!
544 * ======== print1 ========
545 * Generate a `Log` "print event" with 1 argument
546 *
547 * @see #print6
548 */
549 @Macro Void print1(Diags.Mask mask, String fmt, IArg a1);
550
551 /*!
552 * ======== print2 ========
553 * Generate a `Log` "print event" with 2 arguments
554 *
555 * @see #print6
556 */
557 @Macro Void print2(Diags.Mask mask, String fmt, IArg a1, IArg a2);
558
559 /*!
560 * ======== print3 ========
561 * Generate a `Log` "print event" with 3 arguments
562 *
563 * @see #print6
564 */
565 @Macro Void print3(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3);
566
567 /*!
568 * ======== print4 ========
569 * Generate a `Log` "print event" with 4 arguments
570 *
571 * @see #print6
572 */
573 @Macro Void print4(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3,
574 IArg a4);
575
576 /*!
577 * ======== print5 ========
578 * Generate a `Log` "print event" with 5 arguments
579 *
580 * @see #print6
581 */
582 @Macro Void print5(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3,
583 IArg a4, IArg a5);
584
585 /*!
586 * ======== print6 ========
587 * Generate a `Log` "print event" with 6 arguments
588 *
589 * As a convenience to C (as well as assembly language) programmers,
590 * the `Log` module provides a variation of the ever-popular `printf`
591 * function.
592 * The `print[0-6]` functions generate a `Log` "print event" and route
593 * it to the current module's logger.
594 *
595 * The arguments passed to `print[0-6]` may be characters, integers,
596 * strings, or pointers. However, because the declared type of the
597 * arguments is `{@link xdc IArg}`, all pointer arguments must be cast
598 * to an `IArg` type. `IArg` is an integral type large enough to hold
599 * any pointer or an `int`. So, casting a pointer to an `IArg` does
600 * not cause any loss of information and C's normal integer conversions
601 * make the cast unnecessary for integral arguments.
602 *
603 * The format string can use the following conversion characters.
604 * However, it is important to recall that all arguments referenced by
605 * these conversion characters have been converted to an `IArg`
606 * prior to conversion; so, the use of "length modifiers" should be
607 * avoided.
608 *
609 * @p(code) 610 * Conversion Character Description
611 * ------------------------------------------------
612 * %c Character
613 * %d Signed integer
614 * %u Unsigned integer
615 * %x Unsigned hexadecimal integer
616 * %o Unsigned octal integer
617 * %s Character string
618 * %p Pointer
619 * %f Single precision floating point (float)
620 * @p 621 *
622 * Format strings, while very convenient, are a well known source of
623 * portability problems: each format specification must precisely match
624 * the types of the arguments passed. Underlying "printf" functions use
625 * the format string to determine how far to advance through their
626 * argument list. For targets where pointer types and integers are the
627 * same size there are no problems. However, suppose a target's pointer
628 * type is larger than its integer type. In this case, because integer
629 * arguments are widened to be of type `IArg`, a format specification of
630 * "%d" causes an underlying `printf()` implementation to read the
631 * extended part of the integer argument as part of the next argument(!).
632 *
633 * To get around this problem and still allow the use of "natural"
634 * format specifications (e.g., `%d` and `%x` with optional width
635 * specifications), `{@link System#aprintf()}` is used which assumes
636 * that all arguments have been widened to be of type `IArg`.
637 *
638 * See `{@link System#printf}` for complete details.
639 *
640 * The `%f` format specifier is used to print a single precision float
641 * value. Note that `%f` assumes that sizeof(Float) <= sizeof(IArg).
642 * Most clients that interpret float values expect that they are
643 * represented in IEEE 754 floating point format. Therefore, it is
644 * recommended that the float values be converted into that format prior
645 * to supplying the values to `Log` functions in cases where targets do
646 * not generate the float values in IEEE 754 floating point format by
647 * default.
648 *
649 * The first argument to a `Log_print` call is the diags category to be
650 * associated with the event.
651 *
652 * It is also possible to associate an event level with the event to
653 * enable filtering of events based on event level. Conceptually, it is
654 * best to regard the event level as completely separate from the event's
655 * diags category; however, the priority value actually occupies a part
656 * of the diags mask. For this reason, it is possible to specify an event
657 * level by OR'ing the level with the diags mask. For example, to print
658 * an `Diags_INFO` event of `Diags_LEVEL2`, you'd simply write:
659 * (Diags_INFO | Diags_LEVEL2)
660 *
661 * Specifying an event level is optional. `Log_print` calls which do not
662 * specify a level will receive the highest priority by default.
663 *
664 * @param(mask) enable bits and optional detail level for this event
665 * @param(fmt) a `printf` style format string
666 * @param(a1) value for first format conversion character
667 * @param(a2) value for second format conversion character
668 * @param(a3) value for third format conversion character
669 * @param(a4) value for fourth format conversion character
670 * @param(a5) value for fifth format conversion character
671 * @param(a6) value for sixth format conversion character
672 *
673 * @a(Examples) 674 * The following example demonstrates a typical usage.
675 * @p(code) 676 * String list[];
677 * UInt i;
678 *
679 * Log_print2(Diags_USER2, "list[%u] = %s\n", i, (IArg)list[i]);
680 * @p 681 * Note that the `IArg` cast above is only necessary for pointer
682 * arguments; C's normal parameter conversions implicitly convert
683 * integral arguments.
684 *
685 * To simplify the conversion from `float` arguments to `IArg`,
686 * the standard header `xdc/std.h` provides a macro, named floatToArg(),
687 * to do this conversion in a type safe manner. So, the following
688 * statement will print "`float = 2.3456`":
689 * @p(code) 690 * Log_print1(Diags_USER1, "float = %f", floatToArg(2.34567));
691 * @p 692 *
693 * Note that, if you are formatting events on the target, you must
694 * also add support for floating point to ASCII conversion to
695 * `{@link System#printf}`; for more information, see the
696 * `{@link System#extendedFormats}` reference documenation. For example:
697 * @p(code) 698 * var System = xdc.useModule('xdc.runtime.System');
699 * System.extendedFormats = "%f";
700 * @p 701 */
702 @Macro Void print6(Diags.Mask mask, String fmt, IArg a1, IArg a2, IArg a3,
703 IArg a4, IArg a5, IArg a6);
704
705 /*!
706 * ======== error0 ========
707 * Generate a `Log` "error event" with 0 arguments
708 *
709 * @see #error5
710 */
711 @Macro Void error0(String fmt);
712
713 /*!
714 * ======== error1 ========
715 * Generate a `Log` "error event" with 1 argument
716 *
717 * @see #error5
718 */
719 @Macro Void error1(String fmt, IArg a1);
720
721 /*!
722 * ======== error2 ========
723 * Generate a `Log` "error event" with 2 arguments
724 *
725 * @see #error5
726 */
727 @Macro Void error2(String fmt, IArg a1, IArg a2);
728
729 /*!
730 * ======== error3 ========
731 * Generate a `Log` "error event" with 3 arguments
732 *
733 * @see #error5
734 */
735 @Macro Void error3(String fmt, IArg a1, IArg a2, IArg a3);
736
737 /*!
738 * ======== error4 ========
739 * Generate a `Log` "error event" with 4 arguments
740 *
741 * @see #error5
742 */
743 @Macro Void error4(String fmt, IArg a1, IArg a2, IArg a3,
744 IArg a4);
745
746 /*!
747 * ======== error5 ========
748 * Generate a `Log` "error event" with 5 arguments
749 *
750 * The Log_error APIs are intended to allow users to easily log error
751 * events in their code. Similar to the Log_print APIs, Log_error does not
752 * require that you define an event. You simply pass an informative error
753 * string which can optionally be formatted with additional arguments. The
754 * error is logged with the predefined event {@link #L_error}.
755 *
756 * Log_error prepends a string to the message which identifies it as an
757 * ERROR and specifies the filename and line number of the Log_error call
758 * site. A simple example:
759 *
760 * @p(code) 761 * Log_error0("Invalid argument");
762 * @p 763 * This event will be formatted as (assuming that the above call was line
764 * 35 of "MyCode.c")
765 * @p(code) 766 * ERROR at "MyCode.c", line 35: Invalid argument
767 * @p 768 *
769 * Users may provide additional information in the error event, such as
770 * a predefined error code or details of the error. These additional
771 * values will be used to format the string passed to Log_error.
772 * @see #print6 for information about format strings.
773 *
774 * Log_error does not use a variable length argument list--you must call
775 * the appropriate Log_errorX API based on the number of arguments.
776 *
777 * @param(fmt) a reference to a constant error string / fmt string
778 * @param(a1) value for an additional parameter (e.g. an error code)
779 * @param(a2) value for an additional parameter
780 * @param(a3) value for an additional parameter
781 * @param(a4) value for an additional parameter
782 * @param(a5) value for an additional parameter
783 *
784 * @a(Examples) 785 * The following example demonstrates a typical usage.
786 * @p(code) 787 * Int myArg;
788 *
789 * Log_error1("Invalid argument: %d", myArg);
790 * @p 791 * The above event is formatted as, for example:
792 * @p(code) 793 * ERROR: "MyCode.c", line 35: Invalid argument: -1
794 * @p 795 */
796 @Macro Void error5(String fmt, IArg a1, IArg a2, IArg a3,
797 IArg a4, IArg a5);
798
799 /*!
800 * ======== warning0 ========
801 * Generate a `Log` "warning event" with 0 arguments
802 *
803 * @see #warning5
804 */
805 @Macro Void warning0(String fmt);
806
807 /*!
808 * ======== warning1 ========
809 * Generate a `Log` "warning event" with 1 argument
810 *
811 * @see #warning5
812 */
813 @Macro Void warning1(String fmt, IArg a1);
814
815 /*!
816 * ======== warning2 ========
817 * Generate a `Log` "warning event" with 2 arguments
818 *
819 * @see #warning5
820 */
821 @Macro Void warning2(String fmt, IArg a1, IArg a2);
822
823 /*!
824 * ======== warning3 ========
825 * Generate a `Log` "warning event" with 3 arguments
826 *
827 * @see #warning5
828 */
829 @Macro Void warning3(String fmt, IArg a1, IArg a2, IArg a3);
830
831 /*!
832 * ======== warning4 ========
833 * Generate a `Log` "warning event" with 4 arguments
834 *
835 * @see #warning5
836 */
837 @Macro Void warning4(String fmt, IArg a1, IArg a2, IArg a3,
838 IArg a4);
839
840 /*!
841 * ======== warning5 ========
842 * Generate a `Log` "warning event" with 5 arguments
843 *
844 * The Log_warning APIs provide the same features as the Log_error APIs,
845 * but are used to specifically log "warning" events.
846 * @see #error5
847 *
848 * The Log_warning APIs are equivalent to the Log_error APIs except that
849 * they use the predefined {@link #L_warning} event. Log_warning prepends
850 * a string to the message which identifies it as a WARNING and specifies
851 * the filename and line number of the Log_warning call site.
852 *
853 * @param(fmt) reference to a constant warning string / fmt string
854 * @param(a1) value for an additional parameter (e.g. a warning code)
855 * @param(a2) value for an additional parameter
856 * @param(a3) value for an additional parameter
857 * @param(a4) value for an additional parameter
858 * @param(a5) value for an additional parameter
859 *
860 * @a(Examples) 861 * The following example demonstrates a typical usage.
862 * @p(code) 863 * Int myArg;
864 *
865 * Log_warning1("Value may be too high: %d", myArg);
866 * @p 867 * The above event is formatted as:
868 * @p(code) 869 * WARNING: "MyCode.c", line 50: Value may be too high: 4096
870 * @p 871 */
872 @Macro Void warning5(String fmt, IArg a1, IArg a2, IArg a3,
873 IArg a4, IArg a5);
874
875 /*!
876 * ======== info0 ========
877 * Generate a `Log` "info event" with 0 arguments
878 *
879 * @see #info5
880 */
881 @Macro Void info0(String fmt);
882
883 /*!
884 * ======== info1 ========
885 * Generate a `Log` "info event" with 1 argument
886 *
887 * @see #info5
888 */
889 @Macro Void info1(String fmt, IArg a1);
890
891 /*!
892 * ======== info2 ========
893 * Generate a `Log` "info event" with 2 arguments
894 *
895 * @see #info5
896 */
897 @Macro Void info2(String fmt, IArg a1, IArg a2);
898
899 /*!
900 * ======== info3 ========
901 * Generate a `Log` "info event" with 3 arguments
902 *
903 * @see #info5
904 */
905 @Macro Void info3(String fmt, IArg a1, IArg a2, IArg a3);
906
907 /*!
908 * ======== info4 ========
909 * Generate a `Log` "info event" with 4 arguments
910 *
911 * @see #info5
912 */
913 @Macro Void info4(String fmt, IArg a1, IArg a2, IArg a3, IArg a4);
914
915 /*!
916 * ======== info5 ========
917 * Generate a `Log` "info event" with 5 arguments
918 *
919 * The Log_info APIs are provided for easily logging generic
920 * "informational" events with call site information. They are similar to
921 * the Log_print APIs in that they do not require you to define an event--
922 * you simply pass an informative printf-style string which can optionally
923 * be formatted with additional arguments. The info record is logged with
924 * the predefined event '{@link #L_info}'.
925 *
926 * The Log_info APIs log the {@link #L_info} event which uses the 'INFO'
927 * diags category. They do not allow you to specify an event priority.
928 *
929 * Log_info prepends the filename and line number of the call site to the
930 * message.
931 *
932 * @param(fmt) reference to a constant event string / fmt string
933 * @param(a1) value for an additional parameter (e.g. an event code)
934 * @param(a2) value for an additional parameter
935 * @param(a3) value for an additional parameter
936 * @param(a4) value for an additional parameter
937 * @param(a5) value for an additional parameter
938 *
939 * @a(Examples) 940 * The following example demonstrates a typical usage.
941 * @p(code) 942 * Int load;
943 *
944 * Log_info1("Current load: %d", load);
945 * @p 946 * The above event is formatted as, for example:
947 * @p(code) 948 * "MyCode.c", line 15: Current load: 25
949 * @p 950 */
951 @Macro Void info5(String fmt, IArg a1, IArg a2, IArg a3, IArg a4, IArg a5);
952
953 /*!
954 * ======== put0 ========
955 * Unconditionally put the specified Log event with 0 arguments
956 *
957 * @see #put4
958 */
959 @Macro Void put0(Log.Event evt, Types.ModuleId mid);
960
961 /*!
962 * ======== put1 ========
963 * Unconditionally put the specified Log event and 1 argument
964 *
965 * @see #put4
966 */
967 @Macro Void put1(Log.Event evt, Types.ModuleId mid, IArg a1);
968
969 /*!
970 * ======== put2 ========
971 * Unconditionally put the specified Log event and 2 arguments
972 *
973 * @see #put4
974 */
975 @Macro Void put2(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2);
976
977 /*!
978 * ======== put4 ========
979 * Unconditionally put the specified Log event
980 *
981 * This method unconditionally puts the specified `{@link Event}`
982 * `evt` into the log. The `{@link Types#ModuleId}` `mid` should be the
983 * module ID of the module which is putting the event.
984 *
985 * @param(evt) the Log event to put into the log
986 * @param(mid) module ID of the module putting the event
987 * @param(a1) value for first format conversion character
988 * @param(a2) value for second format conversion character
989 * @param(a3) value for third format conversion character
990 * @param(a4) value for fourth format conversion character
991 *
992 * @see #put8
993 */
994 @Macro Void put4(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
995 IArg a3, IArg a4);
996
997 /*!
998 * ======== put8 ========
999 * Unconditionally put the specified Log event and 8 arguments
1000 *
1001 * @see #put4
1002 */
1003 @Macro Void put8(Log.Event evt, Types.ModuleId mid, IArg a1, IArg a2,
1004 IArg a3, IArg a4, IArg a5, IArg a6, IArg a7, IArg a8);
1005
1006 /*!
1007 * ======== write0 ========
1008 * Generate a `Log` event with 0 arguments
1009 *
1010 * @see #write8
1011 */
1012 @Macro Void write0(Event evt);
1013
1014 /*!
1015 * ======== write1 ========
1016 * Generate a `Log` event with 1 argument
1017 *
1018 * @see #write8
1019 */
1020 @Macro Void write1(Event evt, IArg a1);
1021
1022 /*!
1023 * ======== write2 ========
1024 * Generate a `Log` event with 2 arguments
1025 *
1026 * @see #write8
1027 */
1028 @Macro Void write2(Event evt, IArg a1, IArg a2);
1029
1030 /*!
1031 * ======== write3 ========
1032 * Generate a `Log` event with 3 arguments
1033 *
1034 * @see #write8
1035 */
1036 @Macro Void write3(Event evt, IArg a1, IArg a2, IArg a3);
1037
1038 /*!
1039 * ======== write4 ========
1040 * Generate a `Log` event with 4 arguments
1041 *
1042 * @see #write8
1043 */
1044 @Macro Void write4(Event evt, IArg a1, IArg a2, IArg a3, IArg a4);
1045
1046 /*!
1047 * ======== write5 ========
1048 * Generate a `Log` event with 5 arguments
1049 *
1050 * @see #write8
1051 */
1052 @Macro Void write5(Event evt, IArg a1, IArg a2, IArg a3, IArg a4, IArg a5);
1053
1054 /*!
1055 * ======== write6 ========
1056 * Generate a `Log` event with 6 arguments
1057 *
1058 * @see #write8
1059 */
1060 @Macro Void write6(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
1061 IArg a5, IArg a6);
1062
1063 /*!
1064 * ======== write7 ========
1065 * Generate a `Log` event with 7 arguments
1066 *
1067 * @see #write8
1068 */
1069 @Macro Void write7(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
1070 IArg a5, IArg a6, IArg a7);
1071
1072 /*!
1073 * ======== write8 ========
1074 * Generate a `Log` event with 8 arguments
1075 *
1076 * If the mask in the specified `Log` event has any bit set which is
1077 * also set in the current module's diagnostics mask, then this call to
1078 * write will "raise" the given `Log` event.
1079 *
1080 * @param(evt) the `Log` event to write
1081 * @param(a1) value for first format conversion character
1082 * @param(a2) value for second format conversion character
1083 * @param(a3) value for third format conversion character
1084 * @param(a4) value for fourth format conversion character
1085 * @param(a5) value for fifth format conversion character
1086 * @param(a6) value for sixth format conversion character
1087 * @param(a7) value for seventh format conversion character
1088 * @param(a8) value for eighth format conversion character
1089 */
1090 @Macro Void write8(Event evt, IArg a1, IArg a2, IArg a3, IArg a4,
1091 IArg a5, IArg a6, IArg a7, IArg a8);
1092
1093 /*!
1094 * ======== doPrint ========
1095 * Render an event as text via `{@link System#printf System_printf}`
1096 *
1097 * This method is not gated and may make more than one call to
1098 * `System_printf`. This utility method is typically used within the
1099 * implementation of a logger which initializes
1100 * `{@link #EventRec Log_EventRec}` structures based on `Log` events
1101 * produced by the application.
1102 *
1103 * @param(evRec) a non`NULL` pointer to an initialized `Log_EventRec`
1104 * structure to be formated via
1105 * `{@link System#printf System_printf}`.
1106 */
1107 Void doPrint(EventRec *evRec);
1108
1109 /*!
1110 * @_nodoc 1111 * ======== lookupEventMessage ========
1112 * Returns the format string for the event with the given id.
1113 */
1114 function lookupEventMessage(eventId);
1115
1116 /*!
1117 * @_nodoc 1118 * ======== getTargetArgSize ========
1119 * Returns the target size of a record argument in bytes (not MAUs).
1120 */
1121 function getTargetArgSize();
1122
1123 /*!
1124 * @_nodoc 1125 * ======== lookupEventName ========
1126 */
1127 function lookupEventName(eventId);
1128
1129 /*!
1130 * @_nodoc 1131 * ======== lookupModuleName ========
1132 */
1133 function lookupModuleName(modId);
1134
1135 /*!
1136 * @_nodoc 1137 * ======== getTargetEventRecSize ========
1138 * Returns the record size in bytes (not MAUs).
1139 */
1140 function getTargetEventRecSize();
1141
1142 internal:
1143
1144 /*
1145 * ======== idToInfo ========
1146 * Map event ID strings into a string of the form <eventName>::<eventMsg>
1147 */
1148 metaonlyconfig String idToInfo[string] = [];
1149
1150 }
1151 /*
1152 * @(#) xdc.runtime; 2, 1, 0,359; 11-16-2011 11:00:16; /db/ztree/library/trees/xdc/xdc-y13x/src/packages/
1153 */
1154