1 /*
2 * Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*
13 * ======== Program.xdc ========
14 */
15 package xdc.cfg;
16
17 /*!
18 * ======== Program ========
19 * The Program object for the configuration object model.
20 *
21 * This module defines the "root" of the configuration object model; all
22 * "top-level" configuration settings for the executable are provided by
23 * this object. Program configuration scripts reference this module via the
24 * global variable `Program`; i.e., `Program` is implicitly initialized as
25 * follows:
26 * @p(code) 27 * var Program = xdc.useModule('xdc.cfg.Program');
28 * @p 29 *
30 * After a configuration script completes successfully, the following files
31 * are generated:
32 * @p(nlist) 33 * - package/cfg/<exe_name>.c
34 * - package/cfg/<exe_name>.xdl
35 * @p 36 * where `<exe_name>` is the name of the executable with the final '.'
37 * character replaced with an '_'.
38 *
39 * The generated C file contains code and data from each module used by the
40 * program and must be compiled and linked with the other sources to
41 * produce the final executable. The generated linker command file must also
42 * be added during this final link step.
43 *
44 * The linker command file is produced by expanding a template
45 * provided by the platform specifed during configuration and contains
46 * hardware and compiler specific directives required by the target modules
47 * that are part of the program's configuration. This template expands
48 * other templates specified by each imported package's
49 * `{@link xdc.IPackage#getSects getSects}` method, for example. This allows
50 * each package participating in the configuration executable to
51 * automatically contribute a portion of the executable's linker command
52 * file.
53 *
54 * You can modify or augment the contents of this file via
55 * `{@link xdc.cfg.Program#sectionsExclude sectionsExclude}` and
56 * `{@link xdc.cfg.Program#sectionsTemplate sectionsTemplate}`. It is even
57 * possible to completely replace the template used to generate this file via
58 * `{@link xdc.cfg.Program#linkTemplate linkTemplate}`. These configuration
59 * options provide the user complete control of the linker command file
60 */
61
62 @Template("./Program.xdt")
63
64 metaonlymodule Program {
65
66 /*!
67 * ======== GenerationOptions ========
68 * Options that control the files generated as part of program
69 * configuration.
70 *
71 * @field(debuggerFiles) If set to `true` in a configuration script,
72 * debugger project files will be generated as part of the
73 * configuration step. If set to `false`, these files will not
74 * be generated.
75 *
76 * If it is not set (or set to undefined) and the environment
77 * variable `environment["xdc.cfg.gen.debuggerFiles"]` is
78 * non-`null`, then the default value of this parameter is taken
79 * to be the value of the following expression:
80 * @p(code) 81 * environment["xdc.cfg.gen.debuggerFiles"] == "true"
82 * @p 83 * This makes it is possible to enable the generation of
84 * debugger project files from build scripts by passing
85 * the option `-Dxdc.cfg.gen.debuggerFiles=true` to the
86 * configuration tool (see
87 * `{@link xdc.bld.Executable#Attrs.xsopts}` or
88 * `{@link xdc.bld.PackageContents#Attrs.xsopts}`).
89 *
90 * Finally, if `debuggerFiles` is not set (or set to `undefined`)
91 * and the environment variable above is not defined,
92 * the generation of debugger project files occurs only if
93 * `{@link xdc.cfg.Program#build.profile}` contains
94 * the string `"debug"`. So, unless otherwise specified, debug
95 * profiles result in debugger project files being generated.
96 */
97 struct GenerationOptions {
98 Bool debuggerFiles; /*! if `true`, generate debugger "project" files */
99 };
100
101 /*!
102 * ======== SectionSpec ========
103 * Map that instructs the linker where to place output sections.
104 *
105 * This structure contains some fields that are specific to TI targets.
106 * On non-TI targets, such fields are ignored.
107 *
108 * @field(runSegment) Defines the memory segment where the section is
109 * to be run.
110 *
111 * @field(loadSegment) Defines the memory segment where the section is
112 * to be loaded. If 'runSegment' or 'loadSegment' is defined,
113 * but not both, the linker is instructed to use the defined
114 * field as the load and run allocation for the section.
115 *
116 * @field(runAddress) Defines the memory address where the section is
117 * to be run. It is an error if both 'runSegment' and 'runAddress'
118 * are specified.
119 *
120 * @field(loadAddress) Defines the memory address where the section is
121 * to be loaded. It is an error if both 'loadSegment' and
122 * 'loadAddress' are specified. If 'runAddress' or 'loadAddress'
123 * is defined, but not both, the linker is instructed to use the
124 * defined field as the load and run address for the section.
125 *
126 * @field(runAlign) If runSegment is specified, runAlign determines the
127 * alignment. It is an error if both 'runAlign' and 'runAddress'
128 * are specified.
129 *
130 * @field(loadAlign) If runSegment is specified, runAlign determins the
131 * alignment. It is an error if both 'loadAlign' and 'loadAddress'
132 * are specified.
133 *
134 * @field(type) Defines flags for special section types (COPY, DSECT,
135 * NOLOAD).
136 *
137 * @field(fill) Defines the value to initialize an uninitialized
138 * section.
139 */
140 struct SectionSpec {
141 String runSegment; /*! segment where section contents are run */
142 String loadSegment; /*! segment where section contents are loaded */
143 UInt runAddress; /*! start address of section when run */
144 UInt loadAddress; /*! start address of section when loaded */
145 UInt runAlign; /*! alignment of section within runSegment */
146 UInt loadAlign; /*! alignment of section within loadSegment */
147 String type; /*! target-specific flags */
148 UInt fill; /*! fill value */
149 };
150
151 /*!
152 * ======== gen ========
153 * Generation options for this executable
154 *
155 * This configuration parameter allows the program configuration script
156 * to control (to some extent) what files are generated as part of the
157 * configuration process.
158 */
159 config GenerationOptions gen;
160
161 /*!
162 * ======== globalSection ========
163 * UNDER CONSTRUCTION
164 * @_nodoc 165 *
166 * Section where `{@link #globals}` are placed.
167 *
168 * All globals specified in the application configuration file
169 * are placed into this section.
170 *
171 * The default is `null`, which means the `{@link #dataSection}` is used.
172 */
173 config String globalSection = null;
174
175 /*!
176 * ======== sysStack ========
177 * The size of the executable's initial system stack
178 *
179 * On architectures that maintain a separate "system stack" in addition
180 * to the normal `{@link #stack}`, this parameter sets its initial size
181 * (in units of chars). This parameter is ignored for those
182 * architectures for which there is just a single stack; in other
183 * words, almost all known architectures.
184 *
185 * This parameter is used on later generation TI/C55 16-bit DSPs where,
186 * in order to compatibly support 24-bit addresses, a separate
187 * system call/return stack that stores the upper address bits is
188 * employed.
189 */
190 config UInt sysStack = 0x1000;
191
192 /*!
193 * ======== stack ========
194 * The size of the executable's initial stack
195 *
196 * On platforms that enable control of the initial stack size (the
197 * stack that exists immediately after reset), this parameter specifies
198 * its initial size (in units of chars).
199 */
200 config UInt stack = 0x1000;
201
202 /*!
203 * ======== heap ========
204 * The size of the executable's initial heap
205 *
206 * On platforms that enable control of the size of the heap managed by
207 * the run-time support function malloc(), this parameter specifies
208 * its initial size (in units of chars).
209 */
210 config UInt heap = 0x1000;
211
212 /*!
213 * ======== argSize ========
214 * The size allocated for command line args to the executable
215 *
216 * On platforms that require static allocation of space to hold
217 * command line arguments, this parameter specifies its maximum size
218 * (in units of chars).
219 *
220 * Command line arguments are passed to C's `main` function when it's
221 * declared via the prototype: `int main(int argc, char *argv[])`. the
222 * `argv` array points to an array of strings allocated from the
223 * memory block whose size is controlled by `argSize`.
224 *
225 * Setting `argSize` to 0 means that no `argv` array will be allocated
226 * and the application `main()` function should be declared as
227 * `int main(void)`.
228 */
229 config UInt argSize = 0x200;
230
231 /*!
232 * ======== execCmd ========
233 * The command used to run this executable
234 *
235 * This string is used to create a command that runs the executable
236 * from the command line. If it is not set by the configuration script,
237 * it is set by the program's platform package (during program
238 * configuration).
239 *
240 * This command is run as follows:
241 * @p(code) 242 * execCmd <prog> <args>
243 * @p 244 * where, `<prog>` is the name of the executable and `<args>` are
245 * the arguments specified in the test (if any).
246 *
247 * @a(Note) 248 * This parameter is ignored if the exec command is specified as part
249 * of the test; see `{@link xdc.bld.Test#Attrs}`.
250 */
251 config String execCmd;
252
253 /*!
254 * ======== linkTemplate ========
255 * The template for the Program's linker command file
256 *
257 * A template is used to create the linker command file for each
258 * program. It can be optionally specified by setting this
259 * configuration parameter in the program's configuration script. If
260 * `linkTemplate` it is not set or set to `null`, the template is
261 * obtained from the platform associated with this program (i.e., the
262 * platform named by the `{@link #platform}` config in this module).
263 * See `{@link xdc.platform.IPlatform#getLinkTemplate IPlatform.getLinkTemplate}`.
264 *
265 * The `linkTemplate` string names a package path relative path; e.g.,
266 * if the linker template you want to specify is
267 * `"templates/big_n_hairy.xdt"` in the package `myCompany.myPackage`,
268 * `linkTemplate` should be set to:
269 * @p(code) 270 * "myCompany/myPackage/templates/big_n_hairy.xdt"
271 * @p 272 * If `linkTemplate` begins with the string `"./"`, the file is NOT
273 * searched for along the package path; instead the file name is taken
274 * to specify a file relative to the current working directory.
275 *
276 * In any case, if `linkTemplate` is non-`null`, the file must exist;
277 * otherwise, the configuration step will fail.
278 */
279 config String linkTemplate = null;
280
281 /*!
282 * ======== main ========
283 * The main entry point for the program
284 *
285 * This parameter is optionally set by the user's program
286 * configuration script. If it is not set, then a "legacy" `main()`
287 * function is assumed to be linked into the program; otherwise,
288 * the value of `main` is used as the "main" entry point to the
289 * program.
290 */
291 config Int (*main)(Int, Char*[]);
292
293 /*!
294 * ======== sectMap ========
295 * A section name to SectionSpec mapping
296 *
297 * This is a program specific mapping of output section names to
298 * {@link #SectionSpec} objects. The map supports mapping of section
299 * names to memory names; see {@link xdc.platform.IPlatform#sectMap}.
300 *
301 * This parameter enables program configurations to place named
302 * sections in platform specific memory regions. During generation of
303 * the linker command file, sections are mapped to named memories by
304 * first consulting this table; if the table does not contain a mapping,
305 * the target classifies each section as either "code", "data" or
306 * "stack" {@link xdc.bld.ITarget#sectMap} and the platform defines a
307 * memory region for each of these section types
308 * ({@link xdc.platform.IPlatform#codeMemory}/
309 * {@link xdc.platform.IPlatform#dataMemory}). If
310 * this does not produce a result, an error is generated.
311 * It is important to note that `sectMap` does not contain the complete
312 * section allocation for the program. It only contains the entries
313 * explicitly added to `sectMap`. To get the complete section
314 * allocation, a user should call {@link #getSectMap}.
315 *
316 * Suppose for example that the platform defines a memory segment
317 * named "DDR2". The following configuration statement places
318 * everything from the ".text" section into the "DDR2" segment.
319 *
320 * @p(code) 321 * Program.sectMap[".text"] = new Program.SectionSpec();
322 * Program.sectMap[".text"].loadSegment = "DDR2";
323 * @p 324 *
325 * @a(Note) 326 * If BIOS 5 configuration script (Tconf script) is executed, the
327 * section allocations configured in the Tconf script take precedence
328 * over any settings for the same sections in this parameter.
329 *
330 * @see #SectionSpec
331 * @see xdc.platform.IPlatform#sectMap
332 * @see xdc.bld.ITarget#sectMap
333 */
334 config Any sectMap[string]; /* section name => SectionSpec */
335
336 /*!
337 * ======== sectionsExclude ========
338 * Sections to exclude from linker command file generation
339 *
340 * The `sectionsExclude` string is a JavaScript regular expression
341 * that is used to identify names of sections that should NOT be
342 * be handled by the normal linker command file generation process.
343 *
344 * Sections whose name matches `sectionsExclude` must be handled
345 * using a custom linker command file or by specifying a custom template
346 * (see `{@link #sectionsTemplate}` or `{@link #linkTemplate}`).
347 * @a(Examples) 348 * To completely override the placement of all output sections you can
349 * define `sectionsExclude` to match any string.
350 * @p(code) 351 * // Note: the '.' below represents _any_ character, not just "."
352 * Program.sectionsExclude = ".*";
353 * @p 354 * To override output sections that begin with '.' you must specify
355 * the literal character '.' and use the '^' character to match the
356 * beginning of the string.
357 * @p(code) 358 * // the sequence '^\.' matches just "." at the start of the name
359 * Program.sectionsExclude = "^\.";
360 * @p 361 * To override a specific sections you should be careful to supply a
362 * regular expression that matches the entire section name. You can
363 * use '$' to match the end of the name.
364 * @p(code) 365 * // match only ".const" or ".text"
366 * Program.sectionsExclude = "^\.const$|^\.text$";
367 * @p 368 */
369 config String sectionsExclude = null;
370
371 /*!
372 * ======== sectionsTemplate ========
373 * Replace the sections portion of the generated linker command file
374 *
375 * The `sectionsTemplate` string names a template that is used to replace
376 * the "`SECTIONS`" content to the generated linker command file. This
377 * is useful especially when excluding specific sections via
378 * `{@link #sectionsExclude}` or when taking full control of the linker
379 * command file via `{@link #linkTemplate}` is unnecessary. The original
380 * "`SECTIONS`" content is computed and passed as an argument to this
381 * template, which makes it relatively simple to perform small changes to
382 * the "`SECTIONS`" content without having to explicitly handle every
383 * section required by the compiler toolchain.
384 *
385 * The `sectionsTemplate` string names a package path relative path; e.g.,
386 * if the linker template you want to specify is
387 * `"templates/mySections.xdt"` in the package `myCompany.myPackage`,
388 * `sectionsTemplate` should be set to:
389 * @p(code) 390 * "myCompany/myPackage/templates/mySections.xdt"
391 * @p 392 * If `sectionsTemplate` begins with the string `"./"`, the file is NOT
393 * searched for along the package path; instead the file name is taken
394 * to specify a file relative to the current working directory.
395 *
396 * In any case, if `sectionsTemplate` is non-`null`, the file must exist;
397 * otherwise, the configuration step will fail.
398 *
399 * During expansion of this template, there are three "parameters"
400 * that can be referenced to generate new content.
401 * @p(dlist) 402 * - `this`
403 * reference to the `{@link Program}` object
404 * - `$args[0]`
405 * is the complete section map derived from
406 * `{@link Program#sectMap}`; some special sections relavent to
407 * XDCtools are added to the map defined by `Program.sectMap`.
408 * - `$args[1]`
409 * is a string that contains the content that would have been
410 * placed in the `SECTIONS` portion of the generated linker
411 * command file. This allows templates to easily modify this
412 * content or simply add statements before or after it.
413 * @p 414 * @a(Example) 415 * The following template, specific to TI compiler tools, adds start
416 * and size symbols for the `.stack` section and ensures that the stack
417 * is the first section to be allocated in its designated memory segment.
418 * @p(code) 419 * %// first output allocation for the .stack section
420 * %var sectMap = $args[0];
421 * %var stack = sectMap[".stack"];
422 * .stack: >`stack.loadSegment` START(_stack_start) SIZE(_stack_size)
423 * %
424 * %// now append the normally generated content
425 * `$args[1]`
426 * @p 427 * Note: this example requires that the `.stack` section be excluded
428 * from the normal generation via `{@link sectionsExclude}`; otherwise
429 * this section will be specified twice by the template shown above.
430 * @p(code) 431 * Program.sectionsExclude = "^\.stack$";
432 * @p 433 */
434 config String sectionsTemplate = null;
435
436 /*!
437 * ======== system ========
438 * @_nodoc 439 * A facade for the {@link xdc.runtime.System#SupportProxy} parameter
440 *
441 * The program configuration script may select an implementation of
442 * the `xdc.runtime.ISystemSupport` interface and "bind" it by setting
443 * this parameter. If the module assigned to this parameter does not
444 * inherit from `xdc.runtime.ISystemSupport`, the configuration will fail.
445 *
446 * If this parameter is not set (or set to `undefined`), then a default
447 * implementation is used: `xdc.runtime.SysStd` or, if
448 * `Program.build.target.os` is `null`, `xdc.runtime.SysMin`. Recall that
449 * `Program.build.target.os` is specified in the Build Object Model;
450 * `Program.build.target` is the target specified when the executable was
451 * added to the package.
452 *
453 * If this parameter is set to `null`, then the `System` module is not
454 * linked into the application (unless 'Memory' is used); any references
455 * to `System`'s methods will result in a linker error. By setting this
456 * parameter to `null`, one is asserting that `System`'s methods will not
457 * be used.
458 */
459 config Any system;
460
461 /*!
462 * ======== name ========
463 * The name of the executable file
464 *
465 * This is the full file name (relative to the package's base) of the
466 * executable that results from this configuration.
467 *
468 * @a(readonly) 469 * This parameter is set by the generated program configuration script
470 * and must not be modified.
471 */
472 config String name;
473
474 /*!
475 * ======== cfgBase ========
476 * UNDER CONSTRUCTION
477 * @_nodoc 478 */
479 config String cfgBase;
480
481 /*!
482 * ======== buildPackage ========
483 * The name of the executable's package
484 *
485 * This is the full package name (relative to the package's repository)
486 * of the package that contains the executable being configured.
487 *
488 * @a(readonly) 489 * This parameter is set by the generated program configuration script
490 * and must not be modified.
491 */
492 config String buildPackage;
493
494 /*!
495 * ======== endian ========
496 * The endianess of the executable
497 *
498 * This parameter is an alias for `build.target.model.dataModel` and is
499 * set to one of the following values: `"big"`, `"little"`, or `null`.
500 *
501 * @a(readonly) 502 * This parameter is set by the generated program configuration script
503 * and must not be modified.
504 */
505 config String endian = null;
506
507 /*!
508 * ======== codeModel ========
509 * The memory model for code
510 *
511 * This parameter is an alias for `build.target.model.codeModel` and is
512 * set to one of the following target-specific values: `"near"`, `"far"`,
513 * `"large"`, or `null`.
514 *
515 * @a(readonly) 516 * This parameter is set by the generated program configuration script
517 * and must not be modified.
518 */
519 config String codeModel = null;
520
521 /*!
522 * ======== dataModel ========
523 * The memory model for data
524 *
525 * This parameter is an alias for `build.target.model.dataModel` and is
526 * set to one of the following target-specific values: `"near"`, `"far"`,
527 * `"large"`, or `null`.
528 *
529 * @a(readonly) 530 * This parameter is set by the generated program configuration script
531 * and must not be modified.
532 */
533 config String dataModel = null;
534
535 /*!
536 * ======== build ========
537 * This program's build attributes
538 *
539 * This parameter allows arbitrary build attributes to be carried
540 * forward from the Build Object Model (BOM) into the configuration
541 * model for program configuration scripts to read.
542 *
543 * Conceptually, this config parameter should be declared as follows:
544 * @p(code) 545 * struct BuildAttrs inherits xdc.bld.Executable.Attrs {
546 * config xdc.bld.ITarget.Module target;
547 * };
548 * @p 549 * All parameters of the target associated with the executable being
550 * configured are available through '`Program.build.target`'. Any config
551 * parameter set in the BOM's `{@link xdc.bld.Executable#attrs}` is also
552 * available through `{@link #build}`. For example, the name of the
553 * target is `Program.build.target.name` and the name of the
554 * executable's configuration script is `Program.build.cfgScript`.
555 *
556 * @a(readonly) 557 * This parameter is set by the generated program configuration script
558 * and must not be modified.
559 */
560 config Any build; /* BuildAttrs */
561
562 /*!
563 * ======== cpu ========
564 * The execution context "seen" by the executable.
565 *
566 * Since the execution context is largely determined by the CPU that
567 * runs the executable, this configuration parameter allows scripts with
568 * access to the program object to conditionally configure based on CPU
569 * characteristics (e.g., ISA or revision of a chip).
570 *
571 * @a(readonly) 572 * This parameter is set by the platform's implementation of
573 * `xdc.IPackage` (i.e., `package.xs`).
574 */
575 config xdc.platform.IExeContext.Instance cpu;
576
577 /*!
578 * ======== platformName ========
579 * The name of the executable's platform
580 *
581 * This field is the name of the platform instance used to create the
582 * executable; e.g., `"ti.platforms.sim55xx"`, or
583 * `"ti.platforms.sim6xxx:TMS320C6416"`.
584 *
585 * Platform instance names have the form:
586 * @p(code) 587 * <platform_pkg>:<instance_id>
588 * @p 589 * where `<platform_pkg>` is the name of the platform package
590 * responsible for creating the platform instance and the optional
591 * "`:<instance_id>`" is a suffix that uniquely identifies the creation
592 * parameters for this instance.
593 *
594 * The creation parameters are the values specified by the map
595 * `{@link xdc.bld.BuildEnvironment#platformTable}`;
596 * if this map does not contain the platform instance name, the
597 * instance is created with default values that are specific to the
598 * platform.
599 *
600 * @a(readonly) 601 * This parameter is set by the generated program configuration script
602 * and must not be modified.
603 */
604 config String platformName;
605
606 /*!
607 * ======== platform ========
608 * The executable's platform instance object
609 *
610 * The platform instance that provided an execution context for the
611 * executable being configured.
612 *
613 * @a(readonly) 614 * This parameter is set by the generated program configuration script
615 * and must not be modified.
616 */
617 config xdc.platform.IPlatform.Instance platform;
618
619 /*!
620 * ======== global ========
621 * Global variable declarations
622 *
623 * Assignments to this hash table become global symbols that can be
624 * used to directly reference objects. These objects are declared
625 * in a generated header that is indirectly included by the header
626 * `xdc/cfg/global.h`.
627 *
628 * Configuration scripts define symbols by adding new properties to
629 * `global`.
630 * @p(code) 631 * Program.global.myInstance = Mod.create();
632 * Program.global.myString = "hello world";
633 * @p 634 *
635 * Programs can reference the symbols defined in `global` by including
636 * the C/C++ header `xdc/cfg/global.h` as follows:
637 * @p(code) 638 * #include <pkg/Mod.h>
639 * #include <xdc/cfg/global.h>
640 * :
641 * Mod_fxn(myInstance, ...);
642 * printf("greetings: %s\n", myString);
643 * @p 644 *
645 * To compile sources that include `xdc/cfg/global.h`, one symbol must be
646 * defined before including this header:
647 * @p(dlist) 648 * - `xdc_cfg__header__`
649 * the package qualified name of the executable-specific C/C++
650 * header generated by the program configuration tool; e.g.,
651 * `local/examples/package/cfg/mycfg_x62.h`.
652 * @p 653 * For example, to compile sources that reference the values declared in
654 * `{@link #global}` for a TI C6x target with a generated
655 * configuration header named `package/cfg/mycfg_x62.h` in a package
656 * named `local.examples` the following command line is sufficient:
657 * @p(code) 658 * cl6x -Dxdc_cfg__header__=local/examples/package/cfg/mycfg_x62.h ...
659 * @p 660 *
661 * The `xdc_cfg__header__` symbol is automatically defined when you use
662 * the the XDC Build Engine (`{@link xdc.bld}`) to create executables; see
663 * `{@link xdc.bld.Executable#addObjects}`
664 *
665 * @see xdc.bld.Executable#addObjects
666 */
667 config Any global[string];
668
669 /*!
670 * ======== symbol ========
671 * Global symbol specifications
672 *
673 * UNDER CONSTRUCTION
674 * @_nodoc 675 *
676 * This map contains symbol definitions that are used to define alises
677 * or constants. Symbol names are the C symbol names; i.e., compiler name
678 * mangling, such as the addition of a leading "_", is performed
679 * automatically.
680 *
681 * @a(Examples) 682 * To define a symbolic constant:
683 * @p(code) 684 * Program.symbol["ONE"] = 1;
685 * @p 686 * The line above causes the symbol "ONE" to be defined in the linker
687 * command file to be equal to 1. Note this in contrast to defining a
688 * variable whose value is 1; symbols do not occupy space, they are just
689 * symbolic constants defined in the symbol table of the executable.
690 *
691 * This is currently used by xdc.runtime.Startup to define symbols
692 * optionally referenced by boot files that support early startup
693 * "reset" functions.
694 *
695 * The only other use of this map is to define symbolic names for
696 * statically created instances as part of the support for legacy
697 * BIOS 5 instance names.
698 */
699 config Any symbol[string];
700
701 /*!
702 * ======== exportModule ========
703 * Force all the symbols of a module to be part of a configuration
704 *
705 * Although a call xdc.useModule() will force some of a module's methods
706 * to be part of a configuration, the linker is still free to omit any
707 * symbols that are not referenced. Use of exportModule will force all
708 * methods of the specified module to be available.
709 */
710 Void exportModule(String modName);
711
712 /*!
713 * ======== getSectMap ========
714 * Return the complete mapping of section names to `{@link #SectionSpec}`
715 * entries
716 *
717 * The returned map is assembled from `{@link xdc.bld.ITarget#sectMap}`,
718 * `{@link xdc.platform.IPlatform#sectMap}`,
719 * `{@link xdc.platform.IPlatform#codeMemory}`,
720 * `{@link xdc.platform.IPlatform#dataMemory}`,
721 * `{@link xdc.platform.IPlatform#stackMemory}` and `{@link #sectMap}`.
722 * The function can be called at any time during configuration, but if
723 * it is called before all packages had a chance to change `sectMap`,
724 * the returned map may not correspond to the actual section
725 * allocation as configured in the linker command file.
726 *
727 * @a(returns) 728 * `getSectMap` returns a map with section names as keys and
729 * `{@link #SectionSpec}` entries as values.
730 *
731 * @a(Note) 732 * If BIOS 5 configuration script (Tconf script) is executed, the
733 * section allocations configured in the Tconf script are also being
734 * returned.
735 */
736 function getSectMap();
737
738 /*!
739 * ======== importAssembly ========
740 * UNDER CONSTRUCTION
741 * @_nodoc 742 */
743 Void importAssembly(String asmName);
744
745 /*!
746 * ======== targetModules ========
747 * UNDER CONSTRUCTION
748 * @_nodoc 749 *
750 * This function returns a list of target modules. The list is completed
751 * only after all packages are closed, and runtime.finalized() is closed,
752 * so the only time when this function can be safely called is from
753 * within module$static$init and instance$static$init functions, package
754 * validate() functions, and templates.
755 */
756 function targetModules();
757
758 /*!
759 * ======== freezeRomConfig ========
760 * UNDER CONSTRUCTION
761 * @_nodoc 762 */
763 Void freezeRomConfig(String modName, String cfgName);
764
765 /*!
766 * ======== freezeRomConfig2 ========
767 * UNDER CONSTRUCTION
768 * @_nodoc 769 */
770 function freezeRomConfig2(mod, cfgName);
771
772 /*!
773 * ======== freezeRomParams ========
774 * UNDER CONSTRUCTION
775 * @_nodoc 776 */
777 function freezeRomParams(mod);
778
779 /*!
780 * ======== frozenRomConfig ========
781 * UNDER CONSTRUCTION
782 * @_nodoc 783 */
784 Bool frozenRomConfig(String modName, String cfgName);
785
786 /*!
787 * ======== frozenRomConfig2 ========
788 * UNDER CONSTRUCTION
789 * @_nodoc 790 */
791 function frozenRomConfig2(mod, cfgName);
792 }
793 /*
794 * @(#) xdc.cfg; 1, 0, 2, 0,360; 11-16-2011 10:59:52; /db/ztree/library/trees/xdc/xdc-y13x/src/packages/
795 */
796