1 /*
2 * Copyright (c) 2011 by Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12
13 /*
14 * ======== Platform.xdc ========
15 */
16 package ti.platforms.tms320x28;
17
18 /*!
19 * ======== Platform ========
20 * A generic platform that supports any TMS320x28 device
21 *
22 * The device to be used by this platform is passed as the platform instance
23 * name. On the `xdc.tools.configuro` command line, it is done in the
24 * following way:
25 * @p(code) 26 * xs xdc.tools.configuro ... -p "ti.platforms.tms320x28:TMS320C2812"
27 * @p 28 *
29 * In package.bld, the platform instance is selected as in:
30 * @p(code) 31 * Pkg.addExecutable("test", target, "ti.platforms.tms320x28:TMS320C2812");
32 * @p 33 */
34 metaonlymodule Platform inherits xdc.platform.IPlatform
35 {
36 config xdc.platform.IPlatform.Board BOARD = {
37 id: "0",
38 boardName: "tms320x28",
39 boardFamily: null,
40 boardRevision: null
41 };
42
43 /*!
44 * ======== nameFormat ========
45 * Encoding of instance creation parameters in the instance's name
46 *
47 * For this platform, the parameters `deviceName`, `includeLinkCmdFile`
48 * and `clockRate` can be encoded in the instance name supplied on
49 * `xdc.tools.configuro` command line, for example:
50 * @p(code) 51 * xs xdc.tools.configuro ... -p ti.platforms.tms320x28:TMS320F28035:1:60
52 * @p 53 * Optional parameters can be omitted:
54 * @p(code) 55 * xs xdc.tools.configuro ... -p ti.platforms.tms320x28:TMS320F28035:60
56 * @p 57 */
58 readonlyconfig string nameFormat
59 = "$(deviceName):$(includeLinkCmdFile):$(clockRate)";
60
61 instance:
62
63 config xdc.platform.IExeContext.Cpu CPU = {
64 id: "0",
65 clockRate: 0,
66 catalogName: "ti.catalog.c2800",
67 deviceName: "TMS320C2812",
68 revision: null,
69 };
70
71 /*!
72 * ======== deviceName ========
73 * The name of an `ICpuDataSheet` module for the device
74 *
75 * This parameter is required, but it does not have to be set explicitly;
76 * it can be encoded in the instance's name.
77 */
78 config string deviceName;
79
80 /*!
81 * ======== clockRate ========
82 * The clock rate for this device.
83 */
84 config Double clockRate = 0;
85
86 overrideconfig string codeMemory = null;
87
88 overrideconfig string dataMemory = null;
89
90 overrideconfig string stackMemory = null;
91
92 /*!
93 * ======== includeLinkCmdFile ========
94 * The flag that specifies if the platform should include a linker command
95 * file.
96 *
97 * By default, a user is responsible for adding a linker command file to
98 * the project, or to the linker command line. However, if this flag is
99 * set, this platform will include a default linker command file for the
100 * selected device.
101 */
102 config Bool includeLinkCmdFile = false;
103 };
104 /*
105 * @(#) ti.platforms.tms320x28; 1, 0, 0,45; 11-9-2011 12:05:55; /db/ztree/library/trees/platform/platform-n08x/src/
106 */
107