Texas Instruments Technology for Innovators(tm)

XDCtools 3.22.04.46 GA Release Notes

October 10, 2011

Introduction, Documentation, License, What's New, Upgrade & Compatibility Information, Host Support, Dependencies, Device Support, Validation Info, Known Issues, Version Information, Technical Support.


Introduction

RTSC / XDC (eXpanDed C) is a standard for reusable software components, optimized for real-time embedded systems. RTSC components have hardware-neutral formal interfaces, are configurable offline to optimize memory and performance, and support custom automation in the development environment via a scripting language.

The XDCtools product includes the following components:

back to top

Documentation

The product documentation for this release is available in two formats:

Both formats are delivered with the product in the docs subdirectory. The most up-to-date docs can also be viewed online in the RTSC-Pedia.

Release notes from previous product releases are available in the relnotes_archive directory. Note that  XDCtools 3.21 (which supports only the MSP430 device family) is shipped only with the Grace product. 

back to top


License

XDCtools contains elements released under the Eclipse Public License v1.0 and a number of other open-source licenses, detailed here.


What's New

The following significant changes are included in XDCtools 3.22 :

XGCONF Enhancements

New Host and Target Platform Support

Eclipse Integration Enhancements


Defect history and changes in 3.22.04.46 (This Release)

ID Headline
351983 dependencies between executables and imported libraries is broken
291686 multiple imports of the same named module do not trigger error
344740 Error when SourceDir.outputDir is set to a relative path within a directory with spaces
355425 configuro output directory names can't end with a slash
347085 configuro syntax error in generated config.bld
354063 Concerto 28x memory map needs to reserve FLASH/password section


Upgrade and Compatibility Information

 The following section describes compatibility breaks, and workarounds where available.

Package Compatibility Keys

The packages comprising the XDCtools release are uniquely identified by a compatibility key defined in the package.xdc file of a package. Please note that the package compatibility keys are independent of XDC product release numbers.

Package compatibility keys are intended to:

  1. Enable tooling to identify incompatibilities between components, and
  2. Convey a level of compatibility between different releases to set end user expectations.

Package compatibility keys are composed of 4 comma-delimited numbers - M, S, R, P - where:

back to top

Host Support

This release supports the following hosts:

back to top

Dependencies

This release requires the following other software components and tools versions to successfully function:

back to top

Device Support

This release supports the following device families:

back to top

Validation Information

This release was built and validated against using the following components:

The code generation tools used for the various RTSC targets shipped with the product are shown below:


RTSC TargetCode Generation Tools
ti.targets.[C64P,C64P_big_endian,C67P,C674,C674_big_endian,C64T,C64T_big_endian,C66,C66_big_endian]7.0.3 (TMS320C6x, COFF)
ti.targets.[C28,C28_large,C28_float]5.2.3 (TMS320C2000)
ti.targets.elf.[C64P,C64P_big_endian,C64T,C64T_big_endian,C66,C66_big_endian,C674,C674_big_endian,C67P]7.2.0 (TMS320C6x, ELF)
ti.targets.arm.elf.[TMS470,Arm7,Arm9,Arm9t,A8Ft,M3,M3_big_endian,R4,R4_big_endian,R4t,R4t_big_endian,R4F,R4F_big_endian,R4Ft_big_endian]4.9.0 (ARM/TMS470)
gnu.targets.MVArm9,gnu.targets.arm.GCArmv5T3.4.3 (GCC Montavista)
gnu.targets.UCArm94.2.1 (GCC Opensource)
gnu.targets.arm.GCArmv6,GCArmv7A4.3.2 (GCC Codesourcery)
gnu.targets.[Linux86,Sparc]4.1.0 (GCC Opensource)
gnu.targets.Mingw4.4.0 (GCC MingW)
microsoft.targets.Net3213.10.3052 (Microsoft .NET C/C++)
microsoft.targets.Win3214.00.50727.42 (Microsoft Visual C/C++)
microsoft.targets.VC9812.00.8168 (Microsoft Visual C/C++)
microsoft.targets.arm.WinCE14.01.60511 (Microsoft WinCE 6.00)
ti.targets.msp430.[MSP430,MSP430X,MSP430X_small]3.3.0 (MSP430)


back to top


Known Issues

ID Headline
280863 xgconf: If instances have required args, should force user to enter something
280869 xgconf: Can create two instances with the same name
305948
xgconf does not respond to config file rename
321074 xgconf and XDCtools error parser add duplicate errors to Problems view

Editing .cfg files with XGCONF while using ROV can cause Java out of memory error

The graphical editor for .cfg files (XGCONF) and the Runtime Object Viewer debug window (ROV) both consume a lot of Java heap memory. Using both at the same time, or editing multiple .cfg files at the same time, can cause CCS (v4 or v5) to run out of Java heap memory and crash during heavy use. Workaround is to edit only one .cfg file at a time, and close XGCONF while using ROV.

back to top


Version Information

All releases have 4 digits (M.mm.pp.bb). This includes GA and pre-releases (engineering, EA  etc.). Pre-releases are denoted with a suffix (e.g. 3.15.01.51-eng).

This product's version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. xdctools_3_15_00_50.

Subsequent releases of patch upgrades will be identified by the patch number, ex. XDCtools 3.15.01.67 with directory xdctools_3_15_01_67. Typically, these patches only include critical bug fixes.

Please note that version numbers and compatibility keys are NOT the same. For an explanation of compatibility keys, please refer to the 'Upgrade and Compatibility Information' section.

back to top


Technical Support

Support questions on the product should be posted to the RTSC newsgroup. Check the XDCtools download site for the latest releases and RTSC-Pedia (http://rtsc.eclipse.org/docs) for the latest documentation.

back to top


Last updated: October 10, 2011 Build Ver: 3.22.04.46 Rev: