1 /*
2 * Copyright 2011 by Texas Instruments Incorporated.
3 *
4 */
5
6 /*!
7 * ======== Main ========
8 * Command-line tool for generating eclipse plugins for RTSC content
9 *
10 * The `plugingen` tool allows RTSC content producers to
11 * create eclipse plugins that allows their content to be
12 * integrated in the CCS4 environment. As input, the tool requires
13 * @p(blist) 14 * - a RTSC module implementing {@link xdc.tools.product.IProduct}
15 * @p 16 * Refer to {@link ./doc-files/ExampleProduct.xdc ExampleProduct}
17 * for an implementation of {@link xdc.tools.product.IProduct IProduct}.
18 *
19 * The tool may also be used to generate starter examples that will showup
20 * in the new project wizard. This is accomplished by implementing
21 * {@link xdc.tools.product.IProductTemplate IProductTemplate} and setting
22 * the {@link xdc.tools.product.IProduct#templateModule templateModule}
23 * configuration parameter of the {@link xdc.tools.product.IProduct IProduct}
24 * implementation to the name of the implementation module.
25 * Refer to {@link ./doc-files/Examples.xdc Examples}
26 * for a sample implementation of {@link 27 * xdc.tools.product.IProductTemplate IProductTemplate}.
28 *
29 * The XGCONF product view maybe developed by implementing
30 * {@link xdc.tools.product.IProductView IProductView} and setting
31 * the {@link xdc.tools.product.IProduct#productViewModule productViewModule}
32 * configuration parameter of the {@link xdc.tools.product.IProduct IProduct}
33 * implementation to the name of the implementation module.
34 * Refer to {@link ./doc-files/ProductView.xdc ProductView.xdc} and
35 * {@link ./doc-files/ProductView.xs ProductView.xs}
36 * for a sample implementation of {@link 37 * xdc.tools.product.IProductView IProductView}.
38 *
39 * The tool operates on a product that is either specified by the `-p`
40 * option or is present in the folder from which the tool is executed.
41 * The tool will create the plugin in a sub-folder named `eclipse`
42 * in the output directory specified with `-o` option. If the `-o`
43 * option is not specified the plugin is created in the product root
44 * directory.
45 * The tool will search the repositories specified in the module
46 * implementing {@link xdc.tools.product.IProduct} for RTSC platforms.
47 * This search can be disabled by specifying the`--disable_repo_search`
48 * option. The user needs to ensure that the repositories are installed
49 * in the product root directory before using the tool.
50 *
51 * @a(Example) 52 * @p(code) 53 * xs xdc.tools.product.plugingen
54 * -p exampleprod_1_0_0_00
55 * -m xdc.tools.product.plugingen.examples.ExampleProduct
56 * @p 57 */
58 metaonlymodule Main inherits xdc.tools.ICmd
59 {
60 overrideconfig String usage[] = [
61 '[-p product_root_directory]',
62 ' -m module',
63 '[-o outdir]',
64 '[-f pluginFragment]',
65 '[--suppress_product_type_info]',
66 '[--disable_repo_search]'
67 ];
68
69 instance:
70
71 /*!
72 * ======== productDir ========
73 * Product root directory
74 *
75 * This option names the product root directory that is used by the
76 * tool to generate the plugin. If the '-o' option is not
77 * specified the tool generates the plugin in a sub-directory
78 * called `eclipse` in the product root directory.
79 *
80 * If this option is not specified, the product root directory is
81 * assumed to be `./`.
82 *
83 */
84 @CommandOption("p")
85 config String productDir = "./";
86
87 /*!
88 * ======== productModule ========
89 * Input description of the plug-in to be specified
90 *
91 * This required option names a module that implements
92 * `{@link xdc.tools.product.IProduct}`.
93 *
94 */
95 @CommandOption("m")
96 config String productModule;
97
98 /*!
99 * ======== outputDir ========
100 * Output directory in which the plugin will be generated.
101 *
102 * This option names the directory in which the plugin
103 * will be generated in a sub-directory named `eclipse`.
104 * If this option is not specified the tool will generate
105 * the plugin in the product root directory specified with
106 * the '-p' option.
107 *
108 */
109 @CommandOption("o")
110 config String outputDir = null;
111
112 /*!
113 * ======== pluginFragment ========
114 * Text file containing plugin fragment
115 *
116 * This option names the text file containing a plugin fragment.
117 * This allows users to contribute extensions to the UI plugins
118 * generated by the tool.
119 *
120 * The tool does not perform syntax checking of the contributed
121 * fragment. Users need to ensure the correctness of the
122 * contributed fragment. Note that syntactically incorrect
123 * fragments can disable the plugin completely in the eclipse
124 * platform.
125 */
126 @CommandOption("f")
127 config String pluginFragment = null;
128
129 /*!
130 * ======== generationFormat ========
131 * Plugin generation format
132 */
133 @CommandOption("generation_format")
134 config String generationFormat = null;
135
136 /*!
137 * ======== suppress_product_type_info ========
138 * Suppress generation of product type information in the
139 * generated plugin
140 *
141 * This option generates eclipse plugin without the product
142 * type information. Should be invoked to generate plugins
143 * whose product type is declared elsewhere
144 */
145 @CommandOption("suppress_product_type_info")
146 config Bool suppressProductTypeInfo = false;
147
148 /*!
149 * ======== disable_repo_search ========
150 * Suppress search of product repositories
151 *
152 * If this option is specified the tool does not
153 * search the product repositories for RTSC platforms.
154 */
155 @CommandOption("disable_repo_search")
156 config Bool suppressSearch = false;
157
158 /*!
159 * ======== run ========
160 */
161 override Any run(xdc.tools.Cmdr.Instance cmdr, String args[]);
162 }
163 /*
164 * @(#) xdc.tools.product.plugingen; 1, 0, 0,61; 10-9-2011 16:34:52; /db/ztree/library/trees/xdctools/xdctools-f04x/src/
165 */
166