1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== BuildEnvironment.xdc ========
    14     */
    15    package xdc.bld;
    16    
    17    /*!
    18     *  ======== BuildEnvironment ========
    19     *  Global build environment
    20     *
    21     *  This module defines a global object (aliased as '`Build`' in build scripts)
    22     *  which is configured by a build "startup" script and read by package build
    23     *  scripts.
    24     *
    25     *  This module's configuration parameters are initialized by
    26     *  a "startup" script that is run prior to running a package's build
    27     *  script (`package.bld`).  This script (often named "`config.bld`") is
    28     *  responsible for specifying the the `{@link xdc.bld.ITarget#rootDir}`
    29     *  configuration parameter of all targets that appear in the
    30     *  `{@link #targets}` array; the `rootDir` configuration parameter specifies 
    31     *  the absolute path to the installation directory of the compiler used to 
    32     *  build for the specified target.  Typically one startup script is used to
    33     *  establish an environment for multiple packages.
    34     *
    35     *  Note: it does not matter if you do not have tools for all the targets 
    36     *  mentioned in the startup script; if you do not build for a target,
    37     *  its setting in the startup script is irrelevant.
    38     *
    39     *  The startup script may configure this module as a function of the
    40     *  following global variables that exist before this script runs:
    41     *  @p(dlist)
    42     *    - `environment`
    43     *          a hash table of environment strings
    44     *    - `arguments`
    45     *          an array of string arguments to the `config.bld` script
    46     *          initialized as follows:
    47     *              `arguments[0]` - the file name of the `config.bld` script;
    48     *              `arguments[1]` - the first argument specified in `XDCARGS`;
    49     *                  ...;
    50     *              `arguments[n]` - the nth argument in `XDCARGS`.
    51     *    - `Build`
    52     *          an alias for this module (`xdc.bld.BuildEnvironment`).
    53     *          The following parameters of this object are initialized
    54     *          before the startup script runs:
    55     *              `hostOS`     - `{@link #HostOS}` enumeration identifier;
    56     *              `hostOSName` - "Windows", "Linux", or "Solaris"
    57     *    - `Pkg`
    58     *          an alias for this module (`xdc.bld.PackageContents`).
    59     *          The following parameters of this object are initialized
    60     *          before the startup script runs:
    61     *              `{@link PackageContents#name}` - the name of the current
    62     *              package;
    63     *              `{@link PackageContents#modules}` - array of module names
    64     *              supplied by this package; and
    65     *              `{@link PackageContents#interfaces}` - array of interface
    66     *              names supplied by this package
    67     *  @p
    68     *  When you build a package, the `xdc` command looks for the startup file
    69     *  using the following algorithm: 
    70     *  @p(nlist)
    71     *      -   if `XDCBUILDCFG` is defined on the `xdc` command line, its value is
    72     *          used;
    73     *      -   if `config.bld` exists in the current directory, this file is used;
    74     *      -   if `XDCBUILDCFG` is defined as an environment variable, its value
    75     *          is used;
    76     *      -   if `config.bld` exists along the package path (i.e. in `$XDCPATH`
    77     *          followed by the current package's repository), the first such
    78     *          file is used;
    79     *      -   if `$XDCROOT/config.bld` exists this file is used;
    80     *      -   if `$XDCROOT/etc/config.bld` exists, this file is used; and
    81     *          finally
    82     *      -   if no "startup file" can be found above, a fatal error is 
    83     *          reported and the `xdc` command terminates with a non-zero exit
    84     *          status.
    85     */
    86    metaonly module BuildEnvironment {
    87    
    88        /*!
    89         *  ======== HostOS ========
    90         *  An enumeration of all supported development hosts
    91         *
    92         *  @see #hostOS
    93         */
    94        enum HostOS {
    95            WINDOWS,    /*! Win32 Intel development host */
    96            SOLARIS,    /*! SUN OS 5.x development host */
    97            LINUX       /*! Linux development host */
    98        };
    99        
   100        /*!
   101         *  ======== hostOS ========
   102         *  Enumerated constant that identifies the host OS that is executing
   103         *  the build script
   104         *
   105         *  Note that host OS at the time the makefiles are created may be
   106         *  different from the host OS at the time sources are compiled!
   107         */
   108        readonly config HostOS hostOS;
   109    
   110        /*!
   111         *  ======== hostOSName ========
   112         *  The name of the development host
   113         *
   114         *  One of the strings: "Windows", "Solaris", "Linux".  This name is
   115         *  name of the host OS that is executing the package's build script.
   116         */
   117        readonly config String hostOSName;
   118    
   119        /*!
   120         *  ======== useTargets ========
   121         *  The set of targets to use if the `{@link #targets}` array
   122         *  is empty
   123         *
   124         *  `useTargets` is a string of white space separated target names 
   125         *  (i.e., names of modules that implement `{@link xdc.bld.ITarget}`) or
   126         *  regular expression patterns matching target names.
   127         *
   128         *  If the `Build.{@link #targets}` array is empty at the end of the
   129         *  build model's configuration script, targets specified by this string
   130         *  are added to the build model's `{@link #targets}` array.
   131         *
   132         *  In addition to module names, the distinguished string
   133         *  `"native"` is interpreted as an alias for the target
   134         *  specified by the `{@link #nativeTarget}` configuration
   135         *  parameter.
   136         *
   137         *  Special values:
   138         *  @p(dlist)
   139         *     -`undefined`
   140         *          use the environment variable `XDCTARGETS`;
   141         *     -`null`
   142         *          initialize the `{@link #targets}` array to be empty; and
   143         *     -`""`
   144         *          use all TI targets (i.e., "`ti.targets\..*`").
   145         *
   146         *  @see #excludeTargets
   147         *  @see #nativeTarget
   148         */
   149        config String useTargets;
   150    
   151        /*!
   152         *  ======== excludeTargets ========
   153         *  A set of targets to exclude from the set specified by
   154         *  `{@link #useTargets}`
   155         *
   156         *  This string parameter is a single regular expression used to exclude
   157         *  targets from the set specified by `useTargets` (or `XDCTARGETS`).
   158         *
   159         *  If `{@link #targets}` is initialized by the build model's
   160         *  configuration script (i.e., has length > 0) this parameter is
   161         *  ignored.
   162         *
   163         *  If this string is `null` or `undefined`, nothing is excluded from 
   164         *  list specified by `{@link #useTargets}` or the environment variable
   165         *  `XDCTARGETS`.
   166         *
   167         *  @see #useTargets
   168         *  @see #nativeTarget
   169         */
   170        config String excludeTargets;
   171        
   172        /*!
   173         *  ======== targets ========
   174         *  Array of all targets that are supported for the current build
   175         *
   176         *  This array may be explicitly initialized by the build model's
   177         *  initial configuration script (by default, "`config.bld`").  For
   178         *  example, the following fragment specifies that just the
   179         *  `ti.targets.C64` target should be used:
   180         *  @p(code)
   181         *      // get the ti.targets.C64 module
   182         *      var C64 = xdc.module('ti.targets.C64');
   183         *
   184         *      // add the ti.target.C64 module to BuildEnvironment.targets array
   185         *      Build.targets[Build.targets.length++] = C64;
   186         *  @p
   187         *  Alternatively, this array can be implicitly initialized via the
   188         *  `XDCTARGETS` environment variable or the `{@link #useTargets}`
   189         *  and `{@link #excludeTargets}` strings.  The `{@link #targets}` array
   190         *  is implicitly initialized if and only if the length of this array is
   191         *  0 after the build model's configuration script completes.
   192         *
   193         *  All targets that are in this array *must* have their
   194         *  `{@link xdc.bld.ITarget#rootDir}` property set.
   195         *
   196         *  @see #excludeTargets
   197         *  @see #useTargets
   198         */
   199        config ITarget.Module targets[];
   200    
   201        /*!
   202         *  ======== nativeTarget ========
   203         *  A target that defines the "native" target
   204         *
   205         *  This parameter allows build scripts to refer to the "native"
   206         *  target without explicitly naming the target.
   207         *
   208         *  For example, a `package.bld` script may add a library via:
   209         *  @p(code)
   210         *      Pkg.addLibrary("lib", Build.nativeTarget);
   211         *  @p
   212         *  In addition, it is possible to use `"native"` in `XDCTARGETS` or
   213         *  `{@link #useTargets}` to specify that
   214         *  `{@link #nativeTarget}` be added to the `{@link #targets}` array.
   215         *  Thus, it is possible to use the following command on *any* host to
   216         *  build for that host:
   217         *  @p(code)
   218         *      xdc XDCTARGETS=native
   219         *  @p
   220         *
   221         *  If this parameter is not set by the build model's configuration
   222         *  script, it is initialized to an appropriate default native target:
   223         *  @p(blist)
   224         *      - `{@link microsoft.targets.Win32}` for Windows hosts;
   225         *      - `{@link gnu.targets.Sparc}` for Solaris hosts; and
   226         *      - `{@link gnu.targets.Linux86}` for Linux hosts.
   227         *  @p
   228         */
   229        config ITarget.Module nativeTarget = null;
   230    
   231        /*!
   232         *  ======== platformTable ========
   233         *  A map of platform instance names to the parameters used to
   234         *  create them
   235         *
   236         *  This map allows one to define platform instances that require
   237         *  non-default parameter settings.  It also provides a way to
   238         *  publish a set of platforms to be shared among multiple build
   239         *  scripts.
   240         *
   241         *  @a(EXAMPLES)
   242         *  The following fragment defines a platform instance named
   243         *  `"ti.platforms.sim6xxx:big"` that corresponds to a platform instance
   244         *  created by the `ti.platforms.sim6xxx.Platform` module with the
   245         *  parameters `{endian: "big"}`:
   246         *  @p(code)
   247         *    Build.platformTable["ti.platforms.sim6xxx:big"] = {endian: "big"};
   248         *  @p
   249         *
   250         *  The following fragment redefines the default platform instance for
   251         *  the platform package `ti.platforms.sim6xxx` by specifying alternative
   252         *  instance creation parameters.
   253         *  @p(code)
   254         *    Build.platformTable["ti.platforms.sim6xxx"] = {
   255         *        endian: "little", verbose: false, ftpath: "c:/ftsuite_1_5",
   256         *    };
   257         *  @p
   258         *  Some platforms are "software abastractions" that can emulate a large
   259         *  number different physical platforms.  In the example below, the
   260         *  `ti.platforms.sim6xxx` platform package is capable of simulating
   261         *  any TMS320C6xxx device.  This particular platform package uses the
   262         *  name of the instance to determine the specific device that it should
   263         *  emulate.  So, the fragment below specifies a platform instance named
   264         *  `"ti.platforms.sim6xxx:TMS320C6416"` that emulates the `TMS320C6416`
   265         *  device, in little endian mode.
   266         *  @p(code)
   267         *    Build.platformTable["ti.platforms.sim6xxx:TMS320C6416"] = {
   268         *        endian: "little"
   269         *    };
   270         *  @p
   271         *  Software platform packages, such as the `ti.platforms.generic`, can
   272         *  even go as far as emulating any device from any "catalog" of
   273         *  devices.  In this example, we use the `ti.platforms.generic`
   274         *  platform package to define an instance named
   275         *  `ti.platforms.generic:c6416` that corresponds to a platform
   276         *  containing the TMS320C6416 device specified in the `ti.catalog.c6000`
   277         *  package of devices.
   278         *  @p(code)
   279         *    Build.platformTable["ti.platforms.generic:c6416"] = {
   280         *        deviceName: "TMS320C6416",
   281         *        catalogName: "ti.catalog.c6000",
   282         *    };
   283         *  @p
   284         *  @see ti.catalog.c6000
   285         *  @see ti.platforms.generic
   286         *  @see ti.platforms.sim6xxx
   287         */
   288        config any platformTable[string] = [];
   289        
   290        /*!
   291         *  ======== platforms ========
   292         *  Cache of all platform objects added via `{@link #usePlatform}`
   293         *  @_nodoc
   294         */
   295        config any platforms[string];
   296    
   297        /*!
   298         *  ======== usePlatform ========
   299         *  Instantiate the specified platform
   300         *
   301         *  @_nodoc
   302         *
   303         *  @param(name)  name of platform to create
   304         *
   305         *  @a(returns)
   306         *  `usePlatform()` returns the platform instance object
   307         *  (`xdc.platform.IPlatform.Instance`) specified by `name`.
   308         *
   309         *  @a(throws)
   310         *  `XDCException` exceptions are thrown for fatal errors. The following
   311         *  error codes are reported in the exception message:
   312         *  @p(dlist)
   313         *      -  `xdc.bld.PARAMETER_MISMATCH`
   314         *      This error is reported whenever parameters with the wrong type
   315         *      are passed to the method. Ensure that the parameters passed have
   316         *      the right type.
   317         */
   318        function usePlatform(name);
   319        
   320        /*!
   321         *  ======== isInTargetsArray ========
   322         *  Test whether a target is in of the `targets` array
   323         *
   324         *  @_nodoc
   325         *
   326         *  @param(target)  `xdc.bld.ITarget` target object to test
   327         */
   328        Bool isInTargetsArray(ITarget.Module target);
   329        
   330        /*!
   331         *  ======== printBuildTargets ========
   332         *  @_nodoc
   333         */
   334        String printBuildTargets();
   335    
   336        /*!
   337         *  ======== onInit ========
   338         *  @_nodoc this function is called from the `xdc.bld` package's 
   339         *          initialization function to initialize this module.
   340         */
   341        function onInit();
   342    
   343        /*!
   344         *  ======== getReleaseDescs ========
   345         *  Return a description of all releases for the specified package
   346         *
   347         *  This function allows a "package of packages" to select appropriate
   348         *  releases from another package based on information provided by that
   349         *  package.
   350         *
   351         *  @param(pname)   name of the package to get the release 
   352         *                  information from
   353         *
   354         *  @a(returns)     array of `{@link xdc.bld.Release#Desc}`
   355         *                  structures that describe the releases specified
   356         *                  by `pname`'s build script
   357         *
   358         *  @a(throws)      `XDCException` exceptions are thrown for fatal
   359         *                   errors. The following error codes are
   360         *                   reported in the exception message:
   361         *                   @p(dlist)
   362         *                   - `xdc.bld.PACKAGE_NOT_BUILT`
   363         *                      This error is reported when a consumer tries to
   364         *                      use a package that has not been built. Ensure that
   365         *                      the required package has been built by `XDCtools`.
   366         *                   -  `xdc.bld.INVALID_PACKAGE`
   367         *                      This error is reported when a consumer tries to
   368         *                      use a corrupted package. Try rebuilding the
   369         *                      package causing the problem.
   370         *
   371         *  @see xdc.bld.Release#Desc
   372         */
   373        Release.DescArray getReleaseDescs(String pname);
   374    
   375        /*!
   376         *  ======== initializeModel ========
   377         *  @_nodoc
   378         *  Initialize the build model
   379         *
   380         *  @param(args)    - an array of arguments whose first element is
   381         *                    the path to a config.bld script and subsequent
   382         *                    arguments are the argument (usually) specified
   383         *                    by `XDCARGS`.
   384         */
   385        function initializeModel(args);
   386    }
   387    /*
   388     *  @(#) xdc.bld; 1, 0, 2,347; 9-14-2011 15:36:09; /db/ztree/library/trees/xdc/xdc-x20x/src/packages/
   389     */
   390