1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ========= Text.xdc ========
    15     */
    16    
    17    package xdc.runtime;
    18    
    19    /*!
    20     *  ======== Text ========
    21     *  Runtime text handling services
    22     *
    23     *  This module efficiently manages a collection of strings that have
    24     *  common substrings.  Collections with a high degree of commonality
    25     *  are stored in much less space than as ordinary table of independent
    26     *  C strings.  
    27     *
    28     *  To further save space, the "compressed" representation need not even
    29     *  be loaded in the target's memory; see `{@link #isLoaded}`.
    30     *
    31     *  The total space available for the compressed representation of text
    32     *  strings is limited to 64K characters; each string is represented by
    33     *  a 16-bit "rope id".
    34     */
    35    @Template("./Text.xdt")
    36    module Text {
    37    
    38        /*!
    39         *  ======== CordAddr ========
    40         *  @_nodoc
    41         */
    42        typedef Types.CordAddr CordAddr;
    43    
    44        /*!
    45         *  ======== Label ========
    46         */
    47        typedef Types.Label Label;
    48    
    49        /*!
    50         *  ======== RopeId ========
    51         *  @_nodoc
    52         *
    53         *  A rope id is a 16-bit value whose most-significant bit indicates
    54         *  whether the lower 15-bits are an offset into the string table
    55         *  `charTab` or an offset into the "node" table `nodeTab`.
    56         *
    57         *  The node id 0 represents the empty string "".  
    58         */
    59        typedef Types.RopeId RopeId;
    60        
    61        /*!
    62         *  ======== Module_View ========
    63         *  @_nodoc
    64         */
    65        @XmlDtd
    66        metaonly struct Module_View {
    67            Ptr charBase;
    68            Ptr nodeBase;
    69        };
    70        
    71        /*!
    72         *  ======== nameUnknown ========
    73         *  Default unknowable instance name
    74         *
    75         *  The name of an instance if the module's instances are configured to
    76         *  not have names.
    77         */
    78        config String nameUnknown = "{unknown-instance-name}";
    79    
    80        /*!
    81         *  ======== nameEmpty ========
    82         *  Default `NULL` instance name
    83         *
    84         *  The name used if the instance's name has been set to `NULL`.
    85         */
    86        config String nameEmpty = "{empty-instance-name}";
    87    
    88        /*!
    89         *  ======== nameStatic ========
    90         *  Default static instance name
    91         *
    92         *  The name of an instance if the name exists but it's not loaded
    93         *  on the target.
    94         */
    95        config String nameStatic = "{static-instance-name}";
    96    
    97        /*!
    98         *  ======== isLoaded ========
    99         *  Ensure character-strings are loaded in target memory
   100         *
   101         *  Character strings managed by this module are allocated together
   102         *  with other character strings, and loaded to the target, when this
   103         *  parameter is set to its default value `true`. If this parameter is
   104         *  set to `false`, the character strings managed by Text are separated 
   105         *  in their own section `xdc.noload`, which is not loaded to the target.
   106         *
   107         *  @a(Note)
   108         *  For TI and GNU targets, the section `xdc.noload` is not loaded to
   109         *  the target, but it can overlay other output sections. If the linker
   110         *  allocates `xdc.noload` so that it overlaps the section that contains
   111         *  character strings when `isLoaded` is `false`, ROV/RTA functionality
   112         *  can be affected. In such a case, an error message is displayed that
   113         *  indicates the overlap between `xdc.noload` and another section, whose
   114         *  name depends on the target (.`const` on TI targets, `.rodata` on 
   115         *  GNU targets).
   116         *  The user can solve that problem by specifying an address for
   117         *  `xdc.noload` to unconfigured memory, and ensure that `.const` and
   118         *  `xdc.noload` do not overlap.
   119         *  @p(code)
   120         *      Program.sectMap["xdc.noload"] = new prog.SectionSpec();
   121         *      Program.sectMap["xdc.noload"].loadAddress = 0x50000000;
   122         *  @p 
   123         */
   124        config Bool isLoaded = true;
   125    
   126        /*!
   127         *  ======== cordText ========
   128         *  Return `NULL` if cord is in `charTab` and `isLoaded` is `FALSE`
   129         *  @_nodoc
   130         */
   131        String cordText(CordAddr cord);
   132    
   133        /*!
   134         *  ======== ropeText ========
   135         *  Convert rope to an ordinary C string
   136         *
   137         *  Convert rope to an ordinary C string or to NULL if rope refers
   138         *  to a node in nodeTab
   139         *
   140         *  @_nodoc
   141         */
   142        String ropeText(RopeId rope);
   143    
   144        /*!
   145         *  ======== matchRope ========
   146         *  Compare pattern string `pat` to String identified by `rope`.
   147         *  @_nodoc
   148         *
   149         *  @a(pre-conditions)
   150         *  @p(blist)
   151         *      - lenp must be less than or equal to the length of pat
   152         *  @p
   153         
   154         *  @a(post-conditions)
   155         *  @p(blist)
   156         *      - lenp is decreased by the length of any matching prefix
   157         *  @p
   158         *
   159         *  Returns:
   160         *  @p(blist)
   161         *      - -1  `pat` does not match string
   162         *      - 0   string is a prefix of pattern
   163         *      - 1   wildcard match
   164         *  @p
   165         */
   166        Int matchRope(RopeId rope, String pat, Int *lenp);
   167    
   168        /*!
   169         *  ======== putLab ========
   170         *  Convert label to an ASCII character sequence
   171         *
   172         *  This function converts a `{@link Types#Label}` to a sequence of
   173         *  ASCII characters, writes the characters to the supplied buffer,
   174         *  updates the buffer pointer to point to the location after the last
   175         *  output character, and returns the number of characters output.
   176         *
   177         *  No more than `len` characters will be output.  If the label would
   178         *  otherwise be longer, the output is truncated at the point where a
   179         *  potential overflow is detected. The return value always reflects the
   180         *  number of characters output, but it may be less than `len`.
   181         *
   182         *  Label structures can be initialized from any module's instance handle
   183         *  using the module's `Mod_Handle_label()` method.  See
   184         *  `{@link Types#Label}` for more information.
   185         *
   186         *  @param(lab)    address of the label to interpret
   187         *  @param(bufp)   address of the output buffer pointer or `NULL`
   188         *
   189         *                 If `bufp` is `NULL`, the label's characters are
   190         *                 output via `{@link System#putch()}`.
   191         *
   192         *  @param(len)    maximum number of characters to generate
   193         *
   194         *                 If `len` is negative, the number of characters to be
   195         *                 generated is not limited.
   196         *
   197         *  @a(returns)
   198         *  The return value always reflects the number of characters output,
   199         *  but it may be less than `len`.
   200         *
   201         *  @see Types#Label
   202         */
   203        Int putLab(Types.Label *lab, Char **bufp, Int len);
   204    
   205        /*!
   206         *  ======== putMod ========
   207         *  Convert module ID to its ASCII name
   208         *
   209         *  This function converts a `{@link Types#ModuleId}` to a sequence of
   210         *  ASCII characters, writes the characters to the supplied buffer,
   211         *  updates the buffer pointer to point to the location after the last
   212         *  output character, and returns the number of characters output.
   213         *
   214         *  No more than `len` characters will be output.  If the module name would
   215         *  otherwise be longer, the output is truncated at the point where a
   216         *  potential overflow is detected. The return value always reflects the
   217         *  number of characters output, but it may be less than `len`.
   218         *
   219         *  @param(mid)    ID of the module
   220         *  @param(bufp)   address of the output buffer pointer or `NULL`
   221         *
   222         *                 If `bufp` is `NULL`, the module's name characters are
   223         *                 output via `{@link System#putch()}`.
   224         *
   225         *  @param(len)    maximum number of characters to generate
   226         *
   227         *                 If `len` is negative, the number of characters to be
   228         *                 generated is not limited.
   229         *
   230         *  @a(returns)
   231         *  The return value always reflects the number of characters output,
   232         *  but it may be less than `len`.
   233         */
   234        Int putMod(Types.ModuleId mid, Char **bufp, Int len);
   235    
   236        /*!
   237         *  ======== putSite ========
   238         *  Convert call site structure to an ASCII character sequence
   239         *
   240         *  This function converts a `{@link Types#Site}` to a sequence of
   241         *  ASCII characters, writes the characters to the supplied buffer,
   242         *  updates the buffer pointer to point to the location after the last
   243         *  output character, and returns the number of characters output.
   244         *
   245         *  No more than `len` characters will be output.  If the sequence would
   246         *  otherwise be longer, the output is truncated at the point where a
   247         *  potential overflow is detected. 
   248         *
   249         *  @param(site)   address of the call site structure to interpret
   250         *  @param(bufp)   address of the output buffer pointer or `NULL`
   251         *
   252         *                 If `bufp` is `NULL`, the site's name characters are
   253         *                 output via `{@link System#putch()}`.
   254         *
   255         *  @param(len)    maximum number of characters to generate
   256         *
   257         *                 If `len` is negative, the number of characters to be
   258         *                 generated is not limited.
   259         *
   260         *  @a(returns)
   261         *  The return value always reflects the number of characters output,
   262         *  but it may be less than `len`.
   263         */
   264        Int putSite(Types.Site *site, Char **bufp, Int len);
   265    
   266    internal:
   267    
   268        struct Node {
   269            Types.RopeId left;
   270            Types.RopeId right;
   271        };
   272    
   273        typedef Bool (*RopeVisitor)(Ptr, String);
   274    
   275        struct MatchVisState {
   276            String pat;
   277            Int *lenp;
   278            Int res;
   279        };
   280    
   281        struct PrintVisState {
   282            Char **bufp;
   283            Int len;
   284            Int res;
   285        };
   286    
   287        /* charTab[] and nodeTab[] are the "compressed" representation of
   288         * target strings used to name instances, modules, packages, ...
   289         *
   290         * The predefined node id 0 represents the empty string.
   291         */
   292        config Char charTab[] = [0];
   293        config Node nodeTab[] = [{left: 0, right: 0}];
   294        
   295        config Int16 charCnt = 1;
   296        config Int16 nodeCnt = 1;
   297    
   298        /* 
   299         * The module ids are allocated as follows:
   300         * 0x1 - 0x4000     unnamed modules
   301         * 0x4001 - 0x7FFF  registry modules
   302         * 0x8000 - 0xFFFF  named modules
   303         *
   304         * See 'genModNames' in Text.xs
   305         *
   306         * TODO - We may be able to set unnamedModsLastId based on the config
   307         *        to give the Registry more room, but then the Registry id range
   308         *        would not be a constant.
   309         */
   310        config UInt16 unnamedModsLastId = 0x4000;
   311        config UInt16 registryModsLastId = 0x7FFF;
   312    
   313    /* unnamedModCnt can be used to define a constant that allows external 
   314     * modules to define their own module IDs that don't conflict with the 
   315     * statically configured modules; e.g., the dlog example could use this
   316     */
   317    //    config Int16 unnamedModCnt = 0;
   318    
   319        function defineRopeCord(text); 
   320        function defineRopeNode(left, right);
   321    
   322        function fetchAddr(raddr);
   323        function fetchCord(cid);
   324        function fetchId(rid);
   325        function fetchNode(nid);
   326    
   327        function genModNames();
   328        function genPkgName();
   329    
   330        Bool matchVisFxn(Ptr p, String s);
   331        Bool printVisFxn(Ptr p, String s);
   332    
   333        Void visitRope(RopeId rope, Fxn visFxn, Ptr visState);
   334        Void visitRope2(RopeId rope, Fxn visFxn, Ptr visState, String stack[]);
   335    
   336        typedef Void (*VisitRopeFxn)(RopeId, Fxn, Ptr);
   337        typedef Void (*VisitRopeFxn2)(RopeId, Fxn, Ptr, String[]);
   338    
   339        config VisitRopeFxn visitRopeFxn = visitRope;
   340    
   341        config VisitRopeFxn2 visitRopeFxn2 = visitRope2;
   342    
   343        Int xprintf(Char **bufp, String fmt, ...);
   344    
   345        struct Module_State {
   346            Ptr charBase;
   347            Ptr nodeBase;
   348        };
   349    }
   350    /*
   351     *  @(#) xdc.runtime; 2, 1, 0,344; 9-14-2011 15:36:27; /db/ztree/library/trees/xdc/xdc-x20x/src/packages/
   352     */
   353