1    /* 
     2     *  Copyright (c) 2008 Texas Instruments. All rights reserved. 
     3     *  This program and the accompanying materials are made available under the 
     4     *  terms of the Eclipse Public License v1.0 and Eclipse Distribution License
     5     *  v. 1.0 which accompanies this distribution. The Eclipse Public License is
     6     *  available at http://www.eclipse.org/legal/epl-v10.html and the Eclipse
     7     *  Distribution License is available at 
     8     *  http://www.eclipse.org/org/documents/edl-v10.php.
     9     *
    10     *  Contributors:
    11     *      Texas Instruments - initial implementation
    12     * */
    13    /*
    14     *  ======== Startup.xdc ========
    15     */
    16    
    17    package xdc.runtime;
    18    
    19    /*!
    20     *  ======== Startup ========
    21     *  The `xdc.runtime` startup bootstrap
    22     *
    23     *  Every module can optionally define a startup function which is called
    24     *  before `main()`.  Modules declare that they want to participate in this
    25     *  startup sequence via the `@ModuleStartup` attribute in the module's spec
    26     *  file.  Modules that use this attribute must also implement the following
    27     *  startup function:
    28     *  @p(code)
    29     *      Int Mod_Module_startup(Int state);
    30     *  @p
    31     *  where "Mod" is the name of the module requesting startup support.
    32     *
    33     *  The parameter to the startup function serves as "state variable" whose
    34     *  initial value will be `Startup_NOTDONE`. If `startup()` returns a value
    35     *  other than `Startup_DONE`, it will be called in a subsequent pass with this
    36     *  return value passed in as `state`.  To ensure this process terminates,
    37     *  no startup function is ever called more than `{@link #maxPasses}`
    38     *  times.
    39     *
    40     *  For situations in which the startup of one module depends upon another
    41     *  having completed its startup processing, the following function is
    42     *  automatically defined for all modules and proxies:
    43     *  @p(code)
    44     *      Bool Mod_Module_startupDone();
    45     *  @p
    46     *  where "Mod" is the name of some module or proxy.  These predicates can
    47     *  be used as guards inside of a startup function to probe whether a
    48     *  particular module has completed its own startup processing.  As a
    49     *  convenience, the function `Startup_rtsDone()` probes the necessary set of
    50     *  `xdc.runtime` modules required to support instance `create()` functions, and
    51     *  should be called before any startup-time instance creation and/or
    52     *  memory allocation is performed.
    53     *  @p(code)
    54     *      Int Mod_Module_startup(Int state)
    55     *      {
    56     *          if (!Startup_rtsDone()) {
    57     *              return (Startup_NOTDONE);
    58     *          }
    59     *              .
    60     *              .
    61     *              .
    62     *          return (Startup_DONE);
    63     *      }
    64     *  @p
    65     *
    66     *  @a(Startup Sequence)
    67     *  The following list defines when in the startup sequence the user provided
    68     *  startup functions are being invoked:
    69     *  @p(nlist)
    70     *   - CPU is initialized and C stack setup is performed.
    71     *   - Function specified by `Startup.resetFxn` is called.
    72     *     `Startup.resetFxn` is called only on platforms where reset is performed
    73     *     before running a program. For example, boot code for all TI targets
    74     *     invokes `Startup.resetFxn`, while that function is not invoked on
    75     *     Microsoft targets.
    76     *   - C runtime initialization is performed.
    77     *   - Functions from the array `Startup.firstFxns` are called.
    78     *   - All `Mod_Module_startup` functions are called in a loop until all such
    79     *     functions return `Startup_DONE` or `maxPasses` threshold is reached.
    80     *   - Functions from the array `Startup.lastFxns` are called.
    81     *   - The function `main` is called.
    82     *  @p
    83     *     The steps 4 - 6 occur during C++ static object initialization. Since
    84     *     the ANSI C++ Language Standard does not provide a means to control
    85     *     the order of C++ constructors, if a C++ constructor uses an XDC module,
    86     *     there is no guarantee that the module's startup function already ran.
    87     *     Therefore, any C++ constructor that needs XDC modules' services should
    88     *     call `Startup_exec` first to force all startup related functions from
    89     *     steps 4 - 6 to run, before the constructor uses any XDC module.
    90     *  @p
    91     *     Also, if a target does not support C++, the steps 4 - 6 will not run
    92     *     automatically. It is then up to a user's code to invoke `Startup_exec`,
    93     *     possibly as the first step in `main`.
    94     *  @p
    95     */
    96    @Template("./Startup.xdt")
    97    
    98    module Startup {
    99    
   100        /*!
   101         *  ======== DONE ========
   102         *  Returned from module startup functions no further calls are required
   103         */
   104        const Int DONE = -1;
   105    
   106        /*!
   107         *  ======== NOTDONE ========
   108         *  Initial value of state argument passed to module startup functions
   109         */
   110        const Int NOTDONE = 0;
   111    
   112        /*!
   113         *  ======== ModuleView ========
   114         *  @_nodoc
   115         */
   116        metaonly struct ModuleView {
   117            Bool    rtsStartupDone;
   118            Bool    startupBegun;
   119            String  resetFxn;
   120            String  firstFxns[];
   121            String  lastFxns[];
   122        }
   123        
   124        /*!
   125         *  ======== StartupStateView ========
   126         *  @_nodoc
   127         */
   128        metaonly struct StartupStateView {
   129            Int     order;
   130            String  moduleName;
   131            String  done;
   132        }
   133            
   134        /*!
   135         *  ======== rovViewInfo ========
   136         *  @_nodoc
   137         */
   138        @Facet
   139        metaonly config xdc.rov.ViewInfo.Instance rovViewInfo = 
   140            xdc.rov.ViewInfo.create({
   141                viewMap: [
   142                    ['Module', 
   143                        {
   144                            type: xdc.rov.ViewInfo.MODULE,
   145                            viewInitFxn: 'viewInitModule',
   146                            structName: 'ModuleView'
   147                        }
   148                    ],
   149                    ['Startup State', 
   150                        {
   151                            type: xdc.rov.ViewInfo.MODULE_DATA,
   152                            viewInitFxn: 'viewInitStartupState',
   153                            structName: 'StartupStateView'
   154                        }
   155                    ]
   156                ]
   157            });
   158        
   159        /*!
   160         *  ======== maxPasses ========
   161         *  Max number of iterations over the set of startup functions
   162         */
   163        config Int maxPasses = 32;
   164        
   165        /*!
   166         *  ======== InitFxn ========
   167         *  Type of function assignable to `firstFxns`, `lastFxns`, or `resetFxn`
   168         */
   169        typedef Void (*InitFxn)();
   170        
   171        /*!
   172         *  ======== firstFxns ========
   173         *  List of functions called before module startup
   174         *
   175         */
   176        config InitFxn firstFxns[length] = [];
   177    
   178        /*!
   179         *  ======== lastFxns ========
   180         *  List of functions called after module startup
   181         *
   182         */
   183        config InitFxn lastFxns[length] = [];
   184    
   185        /*!
   186         *  ======== resetFxn ========
   187         *  Function to be called by during initialization
   188         *
   189         *  This function is called only on platforms where reset is performed
   190         *  before running the program. The purpose of this function is to set up
   191         *  the hardware registers (cache, external memory interface, etc.) before
   192         *  any other code executes.
   193         *  
   194         */
   195        metaonly config InitFxn resetFxn = null;
   196    
   197        /*!
   198         *  ======== exec ========
   199         *  Execute the startup functions of all resident modules
   200         *
   201         *  Note that this function is idempotent, and can be called at any point
   202         *  in the platform/target startup sequence in which "ordinary" C functions
   203         *  can execute.  By default, this function is called as part of the
   204         *  standard C++ static initialization sequence.
   205         *
   206         *  If your target compiler does not support C++, this function must be
   207         *  called at least once prior to using any `xdc.runtime` modules.
   208         *  Simply call this function at the very beginning of `main()`.
   209         */
   210        Void exec();
   211    
   212        /*!
   213         *  ======== rtsDone ========
   214         *  Query the state of the `xdc.runtime` package
   215         *
   216         *  This function is used by module startup functions to determine
   217         *  when it is possible to use the `xdc.runtime` modules; e.g. to
   218         *  allocate memory, create instances managed by some module (even
   219         *  those outside the `xdc.runtime` package), call a `Log` function,
   220         *  etc.
   221         *
   222         *  @a(returns)     
   223         *  Returns `TRUE` when all `xdc.runtime` modules have completed
   224         *  initialization.
   225         */
   226        Bool rtsDone();
   227    
   228    internal:
   229    
   230        /*!
   231         *  ======== reset ========
   232         *  Application-specific reset function
   233         *
   234         *  This function is defined in `Startup.xdt`
   235         *  (`xdc_runtime_Startup_reset__I`) and is called as early as
   236         *  possible in the program initialization process; for many platforms,
   237         *  it is called prior the the initialization of the C runtime
   238         *  environment.
   239         */
   240        Void reset();
   241    
   242        Void startMods(Int state[], Int len);
   243        readonly config Void (*startModsFxn)(Int[], Int) = startMods;
   244    
   245        extern Void execImplFxn() = xdc_runtime_Startup_exec__I;
   246    
   247        readonly config Void (*execImpl)() = execImplFxn;
   248    
   249        typedef Int (*SFxn)(Int);
   250        config SFxn sfxnTab[];
   251        
   252        /*!
   253         *  ======== sfxnRts ========
   254         *  Array of runtime modules' startup functions 
   255         *
   256         *  This array also contains startup functions of the modules that inherit
   257         *  from interfaces in `xdc.runtime`. Functions added to this array are
   258         *  called only once before the startup procedure for all modules begins.
   259         */
   260        config Bool sfxnRts[];
   261    
   262        struct Module_State {
   263            Int *stateTab;      /* initially null */
   264            Bool execFlag;      /* if true, startup code processing started */
   265            Bool rtsDoneFlag;
   266        };
   267    
   268    }
   269    /*
   270     *  @(#) xdc.runtime; 2, 1, 0,344; 9-14-2011 15:36:27; /db/ztree/library/trees/xdc/xdc-x20x/src/packages/
   271     */
   272