1 /*
2 * Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*
13 * ======== IExeContext.xdc ========
14 */
15 package xdc.platform;
16
17 /*!
18 * ======== IExeContext ========
19 * Execution environment interface between a platform and an executable
20 *
21 * This interface describes the execution environment provided by a
22 * platform as seen by an executable on a particular CPU at the time
23 * it is loaded.
24 *
25 * Execution contexts are created by platforms via
26 * `{@link xdc.platform.IPlatform#getExeContext()}`. Execution contexts are
27 * created implicitly just prior to executing a program's configuration
28 * script. This execution context is made available to the configuration
29 * script as the global read-only `Program.cpu` configuration parameter;
30 * see `{@link xdc.cfg.Program}`.
31 */
32 metaonlyinterface IExeContext
33 {
34 /*!
35 * ======== Cpu ========
36 * CPU attributes necessary to create an execution context.
37 *
38 * Attributes that uniquely identify the CPU responsible for executing
39 * an executable image.
40 */
41 struct Cpu {
42 string id; /*! unique id within the platform */
43 string catalogName; /*! name of catalog package */
44 string deviceName; /*! module name within catalog package */
45 string revision; /*! revision of specified device */
46 float clockRate; /*! clock rate in MHz of CPU on board */
47 };
48
49 instance:
50 /*!
51 * ======== id ========
52 * The CPU's unique id within the platform
53 *
54 * This id is the string used to identify a specific CPU within
55 * the platform that provides this execution context.
56 *
57 * @a(readonly) This parameter is set by the platform and is readonly
58 * for configuration scripts.
59 */
60 config string id;
61
62 /*!
63 * ======== catalogName ========
64 * The name of the package containing the module named by deviceName
65 *
66 * This string names a package containing one or more modules that
67 * implements the `{@link xdc.platform.ICpuDataSheet}` interface.
68 *
69 * @a(readonly) This parameter is set by the platform and is readonly for
70 * configuration scripts.
71 */
72 config string catalogName;
73
74 /*!
75 * ======== deviceName ========
76 * The name of a CPU device within the catalog package catalogName
77 *
78 * This string names a module in the catalog package, specified by
79 * catalogName, that represents the CPU that runs the executable; i.e.,
80 * it implements the `{@link xdc.platform.ICpuDataSheet}` interface.
81 */
82 config string deviceName;
83
84 /*!
85 * ======== revision ========
86 * The revision of the CPU
87 *
88 * @a(readonly) This parameter is set by the platform and is readonly for
89 * configuration scripts.
90 */
91 config string revision = "";
92
93 /*!
94 * ======== clockRate ========
95 * The clock rate in MHz of the CPU
96 *
97 * @a(readonly) This parameter is set by the platform and is readonly for
98 * configuration scripts.
99 */
100 configfloat clockRate;
101
102 /*!
103 * ======== board ========
104 * The board-level attributes
105 *
106 * This parameter defines the static attributes of the board
107 * containing the CPU that runs the executable.
108 *
109 * @a(readonly) This parameter is set by the platform and is readonly for
110 * configuration scripts.
111 */
112 readonlyconfig IPlatform.Board board;
113
114 /*!
115 * ======== attrs ========
116 * The CPU "data-sheet" attributes
117 *
118 * This "data sheet" allows one to get information about the CPU that
119 * runs the run the executable associated with this execution context.
120 *
121 * Multi-CPU platforms provide multiple execution contexts; each
122 * context is associated with a single CPU on the platform.
123 *
124 * @a(readonly) This parameter is set by the platform and is readonly for
125 * configuration scripts.
126 */
127 config ICpuDataSheet.Instance attrs;
128
129 /*!
130 * ======== memoryMap ========
131 * The memory map seen by executables at the time they are loaded
132 *
133 * @a(readonly) This parameter is set by the platform and is readonly for
134 * configuration scripts.
135 */
136 config IPlatform.Memory memoryMap[string];
137 };
138 /*
139 * @(#) xdc.platform; 1, 0, 1, 0,344; 9-14-2011 15:36:12; /db/ztree/library/trees/xdc/xdc-x20x/src/packages/
140 */
141