1 /*
2 * Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*
13 * ======== Program.xdc ========
14 */
15 package xdc.cfg;
16
17 /*!
18 * ======== Program ========
19 * The Program object for the configuration object model.
20 *
21 * This module defines the "root" of the configuration object model; all
22 * configuration settings are for the executable represented by this
23 * object. Program configuration scripts reference this module via the
24 * global variable `Program`; i.e., `Program` implicitly initialized as
25 * follows:
26 * @p(code) 27 * var Program = xdc.useModule('xdc.cfg.Program');
28 * @p 29 *
30 * After a configuration script completes successfully, the XDC runtime
31 * generates the following files:
32 * @p(nlist) 33 * - package/cfg/<exe_name>.c
34 * - package/cfg/<exe_name>.xdl
35 * @p 36 * where `<exe_name>` is the name of the executable with the final '.'
37 * character replaced with an '_'.
38 *
39 * The generated C file contains code and data from each module used by the
40 * program and must be compiled and linked with the other sources to
41 * produce the final executable.
42 *
43 * The generated linker command file must also be used during this final
44 * link step. This linker command file is produced by expanding a template
45 * specified by `{@link xdc.cfg.Program#linkTemplate}`.
46 * Each template is responsible for expanding templates specified by each
47 * imported package's `getSects` method (see `{@link xdc.IPackage#getSects}`).
48 * This allows each package participating in the configuration of an
49 * executable to contribute a portion of the executable's linker command file.
50 */
51
52 @Template("./Program.xdt")
53
54 metaonlymodule Program {
55
56 /*!
57 * ======== GenerationOptions ========
58 * Options that control the files generated as part of program
59 * configuration.
60 *
61 * @field(debuggerFiles) If set to `true` in a configuration script,
62 * debugger project files will be generated as part of the
63 * configuration step. If set to `false`, these files will not
64 * be generated.
65 *
66 * If it is not set (or set to undefined) and the environment
67 * variable `environment["xdc.cfg.gen.debuggerFiles"]` is
68 * non-`null`, then the default value of this parameter is taken
69 * to be the value of the following expression:
70 * @p(code) 71 * environment["xdc.cfg.gen.debuggerFiles"] == "true"
72 * @p 73 * This makes it is possible to enable the generation of
74 * debugger project files from build scripts by passing
75 * the option `-Dxdc.cfg.gen.debuggerFiles=true` to the
76 * configuration tool (see
77 * `{@link xdc.bld.Executable#Attrs.xsopts}` or
78 * `{@link xdc.bld.PackageContents#Attrs.xsopts}`).
79 *
80 * Finally, if `debuggerFiles` is not set (or set to `undefined`)
81 * and the environment variable above is not defined,
82 * the generation of debugger project files occurs only if
83 * `{@link xdc.cfg.Program#build.profile}` contains
84 * the string `"debug"`. So, unless otherwise specified, debug
85 * profiles result in debugger project files being generated.
86 */
87 struct GenerationOptions {
88 Bool debuggerFiles; /*! if `true`, generate debugger "project" files */
89 };
90
91 /*!
92 * ======== SectionSpec ========
93 * Map that instructs the linker where to place output sections.
94 *
95 * This structure contains some fields that are specific to TI targets.
96 * On non-TI targets, such fields are ignored.
97 *
98 * @field(runSegment) Defines the memory segment where the section is
99 * to be run.
100 *
101 * @field(loadSegment) Defines the memory segment where the section is
102 * to be loaded. If 'runSegment' or 'loadSegment' is defined,
103 * but not both, the linker is instructed to use the defined
104 * field as the load and run allocation for the section.
105 *
106 * @field(runAddress) Defines the memory address where the section is
107 * to be run. It is an error if both 'runSegment' and 'runAddress'
108 * are specified.
109 *
110 * @field(loadAddress) Defines the memory address where the section is
111 * to be loaded. It is an error if both 'loadSegment' and
112 * 'loadAddress' are specified. If 'runAddress' or 'loadAddress'
113 * is defined, but not both, the linker is instructed to use the
114 * defined field as the load and run address for the section.
115 *
116 * @field(runAlign) If runSegment is specified, runAlign determines the
117 * alignment. It is an error if both 'runAlign' and 'runAddress'
118 * are specified.
119 *
120 * @field(loadAlign) If runSegment is specified, runAlign determins the
121 * alignment. It is an error if both 'loadAlign' and 'loadAddress'
122 * are specified.
123 *
124 * @field(type) Defines flags for special section types (COPY, DSECT,
125 * NOLOAD).
126 *
127 * @field(fill) Defines the value to initialize an uninitialized
128 * section.
129 */
130 struct SectionSpec {
131 String runSegment; /*! segment where section contents are run */
132 String loadSegment; /*! segment where section contents are loaded */
133 UInt runAddress; /*! start address of section when run */
134 UInt loadAddress; /*! start address of section when loaded */
135 UInt runAlign; /*! alignment of section within runSegment */
136 UInt loadAlign; /*! alignment of section within loadSegment */
137 String type; /*! target-specific flags */
138 UInt fill; /*! fill value */
139 };
140
141 /*!
142 * ======== gen ========
143 * Generation options for this executable
144 *
145 * This configuration parameter allows the program configuration script
146 * to control (to some extent) what files are generated as part of the
147 * configuration process.
148 */
149 config GenerationOptions gen;
150
151 /*!
152 * ======== globalSection ========
153 * UNDER CONSTRUCTION
154 * @_nodoc 155 *
156 * Section where `{@link #globals}` are placed.
157 *
158 * All globals specified in the application configuration file
159 * are placed into this section.
160 *
161 * The default is `null`, which means the `{@link #dataSection}` is used.
162 */
163 config String globalSection = null;
164
165 /*!
166 * ======== sysStack ========
167 * The size of the executable's initial system stack
168 *
169 * On architectures that maintain a separate "system stack" in addition
170 * to the normal `{@link #stack}`, this parameter sets its initial size
171 * (in units of chars). This parameter is ignored for those
172 * architectures for which there is just a single stack; in other
173 * words, almost all known architectures.
174 *
175 * This parameter is used on later generation TI/C55 16-bit DSPs where,
176 * in order to compatibly support 24-bit addresses, a separate
177 * system call/return stack that stores the upper address bits is
178 * employed.
179 */
180 config UInt sysStack = 0x1000;
181
182 /*!
183 * ======== stack ========
184 * The size of the executable's initial stack
185 *
186 * On platforms that enable control of the initial stack size (the
187 * stack that exists immediately after reset), this parameter specifies
188 * its initial size (in units of chars).
189 */
190 config UInt stack = 0x1000;
191
192 /*!
193 * ======== heap ========
194 * The size of the executable's initial heap
195 *
196 * On platforms that enable control of the size of the heap managed by
197 * the run-time support function malloc(), this parameter specifies
198 * its initial size (in units of chars).
199 */
200 config UInt heap = 0x1000;
201
202 /*!
203 * ======== argSize ========
204 * The size allocated for command line args to the executable
205 *
206 * On platforms that require static allocation of space to hold
207 * command line arguments, this parameter specifies its maximum size
208 * (in units of chars).
209 *
210 * Command line arguments are passed to C's `main` function when it's
211 * declared via the prototype: `int main(int argc, char *argv[])`. the
212 * `argv` array points to an array of strings allocated from the
213 * memory block whose size is controlled by `argSize`.
214 *
215 * Setting `argSize` to 0 means that no `argv` array will be allocated
216 * and the application `main()` function should be declared as
217 * `int main(void)`.
218 */
219 config UInt argSize = 0x200;
220
221 /*!
222 * ======== execCmd ========
223 * The command used to run this executable
224 *
225 * This string is used to create a command that runs the executable
226 * from the command line. If it is not set by the configuration script,
227 * it is set by the program's platform package (during program
228 * configuration).
229 *
230 * This command is run as follows:
231 * @p(code) 232 * execCmd <prog> <args>
233 * @p 234 * where, `<prog>` is the name of the executable and `<args>` are
235 * the arguments specified in the test (if any).
236 *
237 * @a(Note) 238 * This parameter is ignored if the exec command is specified as part
239 * of the test; see `{@link xdc.bld.Test#Attrs}`.
240 */
241 config String execCmd;
242
243 /*!
244 * ======== linkTemplate ========
245 * The template for the Program's linker command file
246 *
247 * A template is used to create the linker command file for each
248 * program. It can be optionally specified by setting this
249 * configuration parameter in the program's configuration script. If
250 * `linkTemplate` it is not set or set to `null`, the template is
251 * obtained from the platform associated with this program (i.e., the
252 * platform named by the `{@link #platform}` config in this module).
253 * See `{@link xdc.platform.IPlatform#getLinkTemplate IPlatform.getLinkTemplate}`.
254 *
255 * The `linkTemplate` string names a package path relative path; e.g.,
256 * if the linker template you want to specify is
257 * `"templates/big_n_hairy.xdt"` in the package `myCompany.myPackage`,
258 * `linkTemplate` should be set to:
259 * @p(code) 260 * "myCompany/myPackage/templates/big_n_hairy.xdt"
261 * @p 262 * If `linkTemplate` begins with the string `"./"`, the file is NOT
263 * searched for along the package path; instead the file name is taken
264 * to specify a file relative to the current working directory.
265 *
266 * In any case, if `linkTemplate` is non-`null`, the file must exist;
267 * otherwise, the configuration step will fail.
268 */
269 config String linkTemplate = null;
270
271 /*!
272 * ======== main ========
273 * The main entry point for the program
274 *
275 * This parameter is optionally set by the user's program
276 * configuration script. If it is not set, then a "legacy" `main()`
277 * function is assumed to be linked into the program; otherwise,
278 * the value of `main` is used as the "main" entry point to the
279 * program.
280 */
281 config Int (*main)(Int, Char*[]);
282
283 /*!
284 * ======== sectMap ========
285 * A section name to SectionSpec mapping
286 *
287 * This is a program specific mapping of output section names to
288 * {@link #SectionSpec} objects. The map supports mapping of section
289 * names to memory names; see {@link xdc.platform.IPlatform#sectMap}.
290 *
291 * This parameter enables program configurations to place named
292 * sections in platform specific memory regions. During generation of
293 * the linker command file, sections are mapped to named memories by
294 * first consulting this table; if the table does not contain a mapping,
295 * the target classifies each section as either "code", "data" or
296 * "stack" {@link xdc.bld.ITarget#sectMap} and the platform defines a
297 * memory region for each of these section types
298 * ({@link xdc.platform.IPlatform#codeMemory}/
299 * {@link xdc.platform.IPlatform#dataMemory}). If
300 * this does not produce a result, an error is generated.
301 * It is important to note that `sectMap` does not contain the complete
302 * section allocation for the program. It only contains the entries
303 * explicitly added to `sectMap`. To get the complete section
304 * allocation, a user should call {@link #getSectMap}.
305 *
306 * Suppose for example that the platform defines a memory segment
307 * named "DDR2". The following configuration statement places
308 * everything from the ".text" section into the "DDR2" segment.
309 *
310 * @p(code) 311 * Program.sectMap[".text"] = new Program.SectionSpec();
312 * Program.sectMap[".text"].loadSegment = "DDR2";
313 * @p 314 *
315 * @a(Note) 316 * If BIOS 5 configuration script (Tconf script) is executed, the
317 * section allocations configured in the Tconf script take precedence
318 * over any settings for the same sections in this parameter.
319 *
320 * @see #SectionSpec
321 * @see xdc.platform.IPlatform#sectMap
322 * @see xdc.bld.ITarget#sectMap
323 */
324 config Any sectMap[string]; /* section name => SectionSpec */
325
326 /*!
327 * ======== sectionsExclude ========
328 * Sections to exclude from linker command file generation
329 *
330 * The `sectionsExclude` string is a JavaScript regular expression
331 * that is used to identify names of sections that should NOT be
332 * be handled by the normal linker command file generation process.
333 *
334 * Sections whose name matches `sectionsExclude` must be handled
335 * using a custom linker command file or by specifying a custom template
336 * (see `{@link #sectionsTemplate}` or `{@link #linkTemplate}`).
337 * @a(Examples) 338 * To completely override the placement of all output sections you can
339 * define `sectionsExclude` to match any string.
340 * @p(code) 341 * // Note: the '.' below represents _any_ character, not just "."
342 * Program.sectionsExclude = ".*";
343 * @p 344 * To override output sections that begin with '.' you must specify
345 * the literal character '.' and use the '^' character to match the
346 * beginning of the string.
347 * @p(code) 348 * // the sequence '^\.' matches just "." at the start of the name
349 * Program.sectionsExclude = "^\.";
350 * @p 351 * To override a specific sections you should be careful to supply a
352 * regular expression that matches the entire section name. You can
353 * use '$' to match the end of the name.
354 * @p(code) 355 * // match only ".const" or ".text"
356 * Program.sectionsExclude = "^\.const$|^\.text$";
357 * @p 358 */
359 config String sectionsExclude = null;
360
361 /*!
362 * ======== sectionsTemplate ========
363 * Replace the sections portion of the generated linker command file
364 *
365 * The `sectionsTemplate` string names a template that is used to replace
366 * the "`SECTIONS`" content to the generated linker command file. This
367 * is useful especially when excluding specific sections via
368 * `{@link #sectionsExclude}` or when taking full control of the linker
369 * command file via `{@link #linkTemplate}` is unnecessary. The original
370 * "`SECTIONS`" content is computed and passed as an argument to this
371 * template, which makes it relatively simple to perform small changes to
372 * the "`SECTIONS`" content without having to explicitly handle every
373 * section required by the compiler toolchain.
374 *
375 * The `sectionsTemplate` string names a package path relative path; e.g.,
376 * if the linker template you want to specify is
377 * `"templates/mySections.xdt"` in the package `myCompany.myPackage`,
378 * `sectionsTemplate` should be set to:
379 * @p(code) 380 * "myCompany/myPackage/templates/mySections.xdt"
381 * @p 382 * If `sectionsTemplate` begins with the string `"./"`, the file is NOT
383 * searched for along the package path; instead the file name is taken
384 * to specify a file relative to the current working directory.
385 *
386 * In any case, if `sectionsTemplate` is non-`null`, the file must exist;
387 * otherwise, the configuration step will fail.
388 *
389 * During expansion of this template, there are three "parameters"
390 * that can be referenced to generate new content.
391 * @p(dlist) 392 * - `this`
393 * reference to the `{@link Program}` object
394 * - `$args[0]`
395 * is the complete section map derived from
396 * `{@link Program#sectMap}`; some special sections relavent to
397 * XDCtools are added to the map defined by `Program.sectMap`.
398 * - `$args[1]`
399 * is a string that contains the content that would have been
400 * placed in the `SECTIONS` portion of the generated linker
401 * command file. This allows templates to easily modify this
402 * content or simply add statements before or after it.
403 * @p 404 * @a(Example) 405 * The following template, specific to TI compiler tools, adds start
406 * and size symbols for the `.stack` section and ensures that the stack
407 * is the first section to be allocated in its designated memory segment.
408 * @p(code) 409 * %// first output allocation for the .stack section
410 * %var sectMap = $args[0];
411 * %var stack = sectMap[".stack"];
412 * .stack: >`stack.loadSegment` START(_stack_start) SIZE(_stack_size)
413 * %
414 * %// now append the normally generated content
415 * `$args[1]`
416 * @p 417 * Note: this example requires that the `.stack` section be excluded
418 * from the normal generation via `{@link sectionsExclude}`; otherwise
419 * this section will be specified twice by the template shown above.
420 * @p(code) 421 * Program.sectionsExclude = "^\.stack$";
422 * @p 423 */
424 config String sectionsTemplate = null;
425
426 /*!
427 * ======== system ========
428 * @_nodoc 429 * A facade for the {@link xdc.runtime.System#SupportProxy} parameter
430 *
431 * The program configuration script may select an implementation of
432 * the `xdc.runtime.ISystemSupport` interface and "bind" it by setting
433 * this parameter. If the module assigned to this parameter does not
434 * inherit from `xdc.runtime.ISystemSupport`, the configuration will fail.
435 *
436 * If this parameter is not set (or set to `undefined`), then a default
437 * implementation is used: `xdc.runtime.SysStd` or, if
438 * `Program.build.target.os` is `null`, `xdc.runtime.SysMin`. Recall that
439 * `Program.build.target.os` is specified in the Build Object Model;
440 * `Program.build.target` is the target specified when the executable was
441 * added to the package.
442 *
443 * If this parameter is set to `null`, then the `System` module is not
444 * linked into the application (unless 'Memory' is used); any references
445 * to `System`'s methods will result in a linker error. By setting this
446 * parameter to `null`, one is asserting that `System`'s methods will not
447 * be used.
448 */
449 config Any system;
450
451 /*!
452 * ======== name ========
453 * The name of the executable file
454 *
455 * This is the full file name (relative to the package's base) of the
456 * executable that results from this configuration.
457 *
458 * @a(readonly) 459 * This parameter is set by the generated program configuration script
460 * and must not be modified.
461 */
462 config String name;
463
464 /*!
465 * ======== cfgBase ========
466 * UNDER CONSTRUCTION
467 * @_nodoc 468 */
469 config String cfgBase;
470
471 /*!
472 * ======== buildPackage ========
473 * The name of the executable's package
474 *
475 * This is the full package name (relative to the package's repository)
476 * of the package that contains the executable being configured.
477 *
478 * @a(readonly) 479 * This parameter is set by the generated program configuration script
480 * and must not be modified.
481 */
482 config String buildPackage;
483
484 /*!
485 * ======== endian ========
486 * The endianess of the executable
487 *
488 * This parameter is an alias for `build.target.model.dataModel` and is
489 * set to one of the following values: `"big"`, `"little"`, or `null`.
490 *
491 * @a(readonly) 492 * This parameter is set by the generated program configuration script
493 * and must not be modified.
494 */
495 config String endian = null;
496
497 /*!
498 * ======== codeModel ========
499 * The memory model for code
500 *
501 * This parameter is an alias for `build.target.model.codeModel` and is
502 * set to one of the following target-specific values: `"near"`, `"far"`,
503 * `"large"`, or `null`.
504 *
505 * @a(readonly) 506 * This parameter is set by the generated program configuration script
507 * and must not be modified.
508 */
509 config String codeModel = null;
510
511 /*!
512 * ======== dataModel ========
513 * The memory model for data
514 *
515 * This parameter is an alias for `build.target.model.dataModel` and is
516 * set to one of the following target-specific values: `"near"`, `"far"`,
517 * `"large"`, or `null`.
518 *
519 * @a(readonly) 520 * This parameter is set by the generated program configuration script
521 * and must not be modified.
522 */
523 config String dataModel = null;
524
525 /*!
526 * ======== build ========
527 * This program's build attributes
528 *
529 * This parameter allows arbitrary build attributes to be carried
530 * forward from the Build Object Model (BOM) into the configuration
531 * model for program configuration scripts to read.
532 *
533 * Conceptually, this config parameter should be declared as follows:
534 * @p(code) 535 * struct BuildAttrs inherits xdc.bld.Executable.Attrs {
536 * config xdc.bld.ITarget.Module target;
537 * };
538 * @p 539 * All parameters of the target associated with the executable being
540 * configured are available through '`Program.build.target`'. Any config
541 * parameter set in the BOM's `{@link xdc.bld.Executable#attrs}` is also
542 * available through `{@link #build}`. For example, the name of the
543 * target is `Program.build.target.name` and the name of the
544 * executable's configuration script is `Program.build.cfgScript`.
545 *
546 * @a(readonly) 547 * This parameter is set by the generated program configuration script
548 * and must not be modified.
549 */
550 config Any build; /* BuildAttrs */
551
552 /*!
553 * ======== cpu ========
554 * The execution context "seen" by the executable.
555 *
556 * Since the execution context is largely determined by the CPU that
557 * runs the executable, this configuration parameter allows scripts with
558 * access to the program object to conditionally configure based on CPU
559 * characteristics (e.g., ISA or revision of a chip).
560 *
561 * @a(readonly) 562 * This parameter is set by the platform's implementation of
563 * `xdc.IPackage` (i.e., `package.xs`).
564 */
565 config xdc.platform.IExeContext.Instance cpu;
566
567 /*!
568 * ======== platformName ========
569 * The name of the executable's platform
570 *
571 * This field is the name of the platform instance used to create the
572 * executable; e.g., `"ti.platforms.sim55xx"`, or
573 * `"ti.platforms.sim6xxx:TMS320C6416"`.
574 *
575 * Platform instance names have the form:
576 * @p(code) 577 * <platform_pkg>:<instance_id>
578 * @p 579 * where `<platform_pkg>` is the name of the platform package
580 * responsible for creating the platform instance and the optional
581 * "`:<instance_id>`" is a suffix that uniquely identifies the creation
582 * parameters for this instance.
583 *
584 * The creation parameters are the values specified by the map
585 * `{@link xdc.bld.BuildEnvironment#platformTable}`;
586 * if this map does not contain the platform instance name, the
587 * instance is created with default values that are specific to the
588 * platform.
589 *
590 * @a(readonly) 591 * This parameter is set by the generated program configuration script
592 * and must not be modified.
593 */
594 config String platformName;
595
596 /*!
597 * ======== platform ========
598 * The executable's platform instance object
599 *
600 * The platform instance that provided an execution context for the
601 * executable being configured.
602 *
603 * @a(readonly) 604 * This parameter is set by the generated program configuration script
605 * and must not be modified.
606 */
607 config xdc.platform.IPlatform.Instance platform;
608
609 /*!
610 * ======== global ========
611 * Global variable declarations
612 *
613 * Assignments to this hash table become global symbols that can be
614 * used to directly reference objects. These objects are declared
615 * in a generated header that is indirectly included by the header
616 * `xdc/cfg/global.h`.
617 *
618 * Configuration scripts define symbols by adding new properties to
619 * `global`.
620 * @p(code) 621 * Program.global.myInstance = Mod.create();
622 * Program.global.myString = "hello world";
623 * @p 624 *
625 * Programs can reference the symbols defined in `global` by including
626 * the C/C++ header `xdc/cfg/global.h` as follows:
627 * @p(code) 628 * #include <pkg/Mod.h>
629 * #include <xdc/cfg/global.h>
630 * :
631 * Mod_fxn(myInstance, ...);
632 * printf("greetings: %s\n", myString);
633 * @p 634 *
635 * To compile sources that include `xdc/cfg/global.h`, one symbol must be
636 * defined before including this header:
637 * @p(dlist) 638 * - `xdc_cfg__header__`
639 * the package qualified name of the executable-specific C/C++
640 * header generated by the program configuration tool; e.g.,
641 * `local/examples/package/cfg/mycfg_x62.h`.
642 * @p 643 * For example, to compile sources that reference the values declared in
644 * `{@link #global}` for a TI C6x target with a generated
645 * configuration header named `package/cfg/mycfg_x62.h` in a package
646 * named `local.examples` the following command line is sufficient:
647 * @p(code) 648 * cl6x -Dxdc_cfg__header__=local/examples/package/cfg/mycfg_x62.h ...
649 * @p 650 *
651 * The `xdc_cfg__header__` symbol is automatically defined when you use
652 * the the XDC Build Engine (`{@link xdc.bld}`) to create executables; see
653 * `{@link xdc.bld.Executable#addObjects}`
654 *
655 * @see xdc.bld.Executable#addObjects
656 */
657 config Any global[string];
658
659 /*!
660 * ======== symbol ========
661 * Global symbol specifications
662 *
663 * UNDER CONSTRUCTION
664 * @_nodoc 665 *
666 * This map contains symbol definitions that are used to define alises
667 * or constants. Symbol names are the C symbol names; i.e., compiler name
668 * mangling, such as the addition of a leading "_", is performed
669 * automatically.
670 *
671 * @a(Examples) 672 * To define a symbolic constant:
673 * @p(code) 674 * Program.symbol["ONE"] = 1;
675 * @p 676 * The line above causes the symbol "ONE" to be defined in the linker
677 * command file to be equal to 1. Note this in contrast to defining a
678 * variable whose value is 1; symbols do not occupy space, they are just
679 * symbolic constants defined in the symbol table of the executable.
680 *
681 * This is currently used by xdc.runtime.Startup to define symbols
682 * optionally referenced by boot files that support early startup
683 * "reset" functions.
684 *
685 * The only other use of this map is to define symbolic names for
686 * statically created instances as part of the support for legacy
687 * BIOS 5 instance names.
688 */
689 config Any symbol[string];
690
691 /*!
692 * ======== exportModule ========
693 * Force all the symbols of a module to be part of a configuration
694 *
695 * Although a call xdc.useModule() will force some of a module's methods
696 * to be part of a configuration, the linker is still free to omit any
697 * symbols that are not referenced. Use of exportModule will force all
698 * methods of the specified module to be available.
699 */
700 Void exportModule(String modName);
701
702 /*!
703 * ======== getSectMap ========
704 * Return the complete mapping of section names to `{@link #SectionSpec}`
705 * entries
706 *
707 * The returned map is assembled from `{@link xdc.bld.ITarget#sectMap}`,
708 * `{@link xdc.platform.IPlatform#sectMap}`,
709 * `{@link xdc.platform.IPlatform#codeMemory}`,
710 * `{@link xdc.platform.IPlatform#dataMemory}`,
711 * `{@link xdc.platform.IPlatform#stackMemory}` and `{@link #sectMap}`.
712 * The function can be called at any time during configuration, but if
713 * it is called before all packages had a chance to change `sectMap`,
714 * the returned map may not correspond to the actual section
715 * allocation as configured in the linker command file.
716 *
717 * @a(returns) 718 * `getSectMap` returns a map with section names as keys and
719 * `{@link #SectionSpec}` entries as values.
720 *
721 * @a(Note) 722 * If BIOS 5 configuration script (Tconf script) is executed, the
723 * section allocations configured in the Tconf script are also being
724 * returned.
725 */
726 function getSectMap();
727
728 /*!
729 * ======== importAssembly ========
730 * UNDER CONSTRUCTION
731 * @_nodoc 732 */
733 Void importAssembly(String asmName);
734
735 /*!
736 * ======== targetModules ========
737 * UNDER CONSTRUCTION
738 * @_nodoc 739 *
740 * This function returns a list of target modules. The list is completed
741 * only after all packages are closed, and runtime.finalized() is closed,
742 * so the only time when this function can be safely called is from
743 * within module$static$init and instance$static$init functions, package
744 * validate() functions, and templates.
745 */
746 function targetModules();
747
748 /*!
749 * ======== freezeRomConfig ========
750 * UNDER CONSTRUCTION
751 * @_nodoc 752 */
753 Void freezeRomConfig(String modName, String cfgName);
754
755 /*!
756 * ======== freezeRomConfig2 ========
757 * UNDER CONSTRUCTION
758 * @_nodoc 759 */
760 function freezeRomConfig2(mod, cfgName);
761
762 /*!
763 * ======== freezeRomParams ========
764 * UNDER CONSTRUCTION
765 * @_nodoc 766 */
767 function freezeRomParams(mod);
768
769 /*!
770 * ======== frozenRomConfig ========
771 * UNDER CONSTRUCTION
772 * @_nodoc 773 */
774 Bool frozenRomConfig(String modName, String cfgName);
775
776 /*!
777 * ======== frozenRomConfig2 ========
778 * UNDER CONSTRUCTION
779 * @_nodoc 780 */
781 function frozenRomConfig2(mod, cfgName);
782 }
783 /*
784 * @(#) xdc.cfg; 1, 0, 2, 0,344; 9-14-2011 15:36:07; /db/ztree/library/trees/xdc/xdc-x20x/src/packages/
785 */
786