1    /* 
     2     *  Copyright (c) 2008 Texas Instruments and others.
     3     *  All rights reserved. This program and the accompanying materials
     4     *  are made available under the terms of the Eclipse Public License v1.0
     5     *  which accompanies this distribution, and is available at
     6     *  http://www.eclipse.org/legal/epl-v10.html
     7     * 
     8     *  Contributors:
     9     *      Texas Instruments - initial implementation
    10     * 
    11     * */
    12    /*
    13     *  ======== Repository.xdc ========
    14     */
    15    package xdc.bld;
    16    
    17    /*!
    18     *  ======== Repository ========
    19     *  Model of a package repository
    20     */
    21    metaonly module Repository {
    22    
    23        /*!
    24         *  ======== Attrs ========
    25         *  Optional attributes for a repository
    26         *
    27         *  @field(releases)  This array contains releases that will contain the
    28         *          repository.  Thus, a single repository can be part of any set 
    29         *          of releases.  Each repository is always added to the 
    30         *          package's "default release" in addition to any releases
    31         *          specified in the releases array.
    32         *
    33         *  @see #attrs
    34         */
    35        struct Attrs {
    36            Release.Instance releases[]; /*! releases that this rep is a part of */
    37        };
    38    
    39    instance:
    40        /*!
    41         *  ======== create ========
    42         *  @_nodoc
    43         *  Instances should only be created via PackageContents.addRepository()
    44         */
    45        create();
    46    
    47        /*!
    48         *  ======== name ========
    49         *  The repository's directory name
    50         */
    51        config String name;
    52    
    53        /*!
    54         *  ======== attrs ========
    55         *  The repository's attributes
    56         */
    57        config Attrs attrs;
    58    
    59        /*!
    60         *  ======== addPackages ========
    61         *  Add specified package releases to this repository
    62         *
    63         *  @param(names) An array of strings naming package releases to be added
    64         *          to the repository.  Package releases are named as follows:
    65         *          @p(code)
    66         *              <pkgName>:<releaseName>
    67         *          @p
    68         *          where `<pkgName>` is the name of the package to add to the
    69         *          repository and `<releaseName>` is the name of one of that
    70         *          package's releases.  A package release name may be either the
    71         *          archive file name (relative to the package's base directory)
    72         *          of the release archive or the name used create the release in
    73         *          package named `<pkgName>`.
    74         *
    75         *          For example, if the package `ti.bios` had a release named
    76         *          `exports/ti_bios,src`, the following statements would add
    77         *          this release to the repository named `packages`:
    78         *          @p(code)
    79         *              var r = Pkg.addRepository("packages");
    80         *              r.addPackages(["ti.bios:exports/ti_bios,src"]);
    81         *          @p
    82         *
    83         *          Alternatively, one can specify the archive file name:
    84         *          @p(code)
    85         *              var r = Pkg.addRepository("packages");
    86         *              r.addPackages(["ti.bios:exports/ti_bios,src.tar"]);
    87         *          @p
    88         *
    89         *          It is possible to get a list of release archive names from a
    90         *          package via the
    91         *          `{@link xdc.bld.BuildEnvironment#getReleaseDescs()}`
    92         *          method.  For example, to get the physical archive name of the
    93         *          default release of the `ti.bios` package, the following loop
    94         *          can be added to a build script:
    95         *          @p(code)
    96         *              var archiveName;
    97         *              var rels = Build.getReleaseDescs('ti.bios');
    98         *              for (var j = 0; j < rels.length; j++) {
    99         *                  if (rels[j].label == "default") {
   100         *                      archiveName = rels[j].aname;
   101         *                      break;
   102         *                  }
   103         *              }
   104         *              // archiveName is now set to the file name of the ti.bios
   105         *              // default release archive (or undefined)
   106         *          @p
   107         *
   108         *  @see xdc.bld.BuildEnvironment#getReleaseDescs()
   109         */
   110        Void addPackages(String names[]);
   111    }
   112    /*
   113     *  @(#) xdc.bld; 1, 0, 2,347; 9-14-2011 15:36:09; /db/ztree/library/trees/xdc/xdc-x20x/src/packages/
   114     */
   115