1 /*
2 * Copyright (c) 2008 Texas Instruments and others.
3 * All rights reserved. This program and the accompanying materials
4 * are made available under the terms of the Eclipse Public License v1.0
5 * which accompanies this distribution, and is available at
6 * http://www.eclipse.org/legal/epl-v10.html
7 *
8 * Contributors:
9 * Texas Instruments - initial implementation
10 *
11 * */
12 /*
13 * ======== ITarget.xdc ========
14 */
15 package microsoft.targets;
16
17 /*!
18 * ======== ITarget ========
19 * A Microsoft-specific extension to the base xdc.bld.ITarget2 interface.
20 */
21 @TargetHeader("xdc/bld/stddefs.xdt")
22 metaonlyinterface ITarget inherits xdc.bld.ITarget2 {
23
24 overridereadonlyconfig string stdInclude = "microsoft/targets/std.h";
25 overrideconfig string dllExt = ".dll";
26
27 /*!
28 * ======== debugGen ========
29 * Debugger/IDE project file generation support.
30 *
31 * The settings below generate VC project files that enable one
32 * to debug (and even rebuild) Executables from within the VC GUI.
33 *
34 * To avoid unnecessary build time overhead, these files are not always
35 * generated; by default, they are only generated for "debug" profiles.
36 * The generation of these files is controlled by the
37 * `{@link xdc.cfg.Program#gen}` configuration parameter. To force these
38 * files to be generated for a particular executable, add the following
39 * line to the executable's program configuration script:
40 * @p(code) 41 * Program.gen.debuggerFiles = true;
42 * @p 43 * It is also possible to control the generation via build options; see
44 * `{@link xdc.bld.ITarget#DebugGen}`.
45 *
46 * To debug an executable: double click on the generated *.vcproj file,
47 * when the debugger comes up, type F11 (step into).
48 *
49 * The first time you debug an executable, the VC debugger may prompt
50 * you for a "solution file" to save. Click OK (accepting the solution
51 * file name), and you will be at the first statement of your
52 * executable.
53 *
54 * To set command line arguments prior to debugging: open the
55 * executable's "Project Properties" dialog (select the
56 * executable in the "Solution Explorer" window and pull-down
57 * View->"Property Pages" or type shift-F4), select "Debugging"
58 * in the left-most pane of the executable's "Property Pages", and
59 * enter command line arguments in the "Command Arguments" text box.
60 *
61 * @see http://msdn.microsoft.com/library/default.asp?url=/library/en-us/vsdebug/html/vxtskdebugginganexecreatedwithoutvisualstudioproject.asp
62 */
63 overrideconfig xdc.bld.ITarget.DebugGen debugGen = {
64 execTemplate: "microsoft/targets/vc_exec.xdt",
65 execPattern: "$(cfgName).vcproj"
66 };
67
68 /*!
69 * ======== profiles ========
70 * Standard options profiles for the microsoft tool-chain.
71 */
72 overrideconfig xdc.bld.ITarget.OptionSet profiles[string] = [
73 ["debug", {
74 compileOpts: {
75 copts: "-Z7 -Odi -MTd",
76 defs: "-D_DEBUG=1",
77 },
78 linkOpts: "-debug msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib",
79 }],
80
81 ["release", {
82 compileOpts: {
83 copts: "-O2 -MT",
84 defs: "",
85 },
86 linkOpts: "msvcrt.lib setargv.obj oldnames.lib ole32.lib oleaut32.lib olepro32.lib uuid.lib kernel32.lib user32.lib gdi32.lib advapi32.lib shell32.lib comctl32.lib",
87 }],
88 ];
89
90 /*!
91 * ======== setPath ========
92 * Return path needed to find necessary DLLS
93 *
94 * The microsoft compilers often require one or more directories to
95 * be in the PATH; this allows the compiler to find necessary DLLs.
96 * A target implementing this function returns a string with path
97 * components separated by ";".
98 */
99 function setPath();
100
101 /*!
102 * ======== cmdPrefix ========
103 * Prefix to put in front of each command
104 *
105 * This string is put in front of every Command before being passed to
106 * the shell for execution. This string can be used to run the compiler
107 * in emulation environments.
108 */
109 config String cmdPrefix = "";
110
111 /*!
112 * ======== strictANSI ========
113 * Disable Microsoft C/C++ language extensions
114 *
115 * Set to true if you plan to port your program to other environments.
116 * The compiler treats extended keywords as simple identifiers, disables
117 * the other Microsoft extensions, and automatically defines the
118 * `__STDC__` predefined macro for C programs. This option shows up
119 * as `"-Za"` on the command line when strictANSI is set to `true`.
120 */
121 configbool strictANSI = true;
122
123 /*!
124 * ======== version ========
125 * The Compatibility Key associated with this target.
126 *
127 * The first two components of this target Compatibility Key are '1,0'.
128 * The rest of the Key represents the compiler version. The third
129 * component combines the major and the minor version number in the format
130 * Major.Minor. The fourth component is the build number.
131 *
132 * @a(Example) 133 * If this target's `rootDir` points to the Visual C++ 2005 Express
134 * Edition, the output of the command `cl` may contains the compiler
135 * version string 14.00.50727.42. The Compatibility Key is
136 * [1,0,14.00,50727].
137 *
138 */
139 overridemetaonlyconfig String version;
140
141 /*!
142 * ======== stdTypes ========
143 * @_nodoc 144 */
145 overridereadonlyconfig xdc.bld.ITarget.StdTypes stdTypes = {
146 t_IArg : { size: 4, align: 1 },
147 t_Char : { size: 1, align: 1 },
148 t_Double : { size: 8, align: 1 },
149 t_Float : { size: 4, align: 1 },
150 t_Fxn : { size: 4, align: 1 },
151 t_Int : { size: 4, align: 1 },
152 t_Int8 : { size: 1, align: 1 },
153 t_Int16 : { size: 2, align: 1 },
154 t_Int32 : { size: 4, align: 1 },
155 t_Int64 : { size: 8, align: 1 },
156 t_Long : { size: 4, align: 1 },
157 t_LDouble : { size: 8, align: 1 },
158 t_Ptr : { size: 4, align: 1 },
159 t_Short : { size: 2, align: 1 },
160 };
161 }
162 /*
163 * @(#) microsoft.targets; 1, 0, 2, 0,469; 9-16-2011 17:13:17; /db/ztree/library/trees/xdctargets/xdctargets-e09x/src/ xlibrary
164 165 */
166